Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Vivado's forgotten feature: The Dashboard
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 10 Nov 2018 4:46 AM Date Created
  • Views 1514 views
  • Likes 3 likes
  • Comments 2 comments
  • xilinx
  • fpga
  • vivado
  • arty
  • arty s7
  • spartan-7
  • dashboard
  • xadc
Related
Recommended

Vivado's forgotten feature: The Dashboard

wolfgangfriedrich
wolfgangfriedrich
10 Nov 2018

The roadtest about my adventures in Vivado together with the Digilent ARTY S7 board continues.

 

I just re-found a feature that might help during very low level debugging and system testing: the dashboard.

 

It is accessed through the hardware manager, when connected to a board.

  1. Open the 'Hardware Manager' from the Flow Navigator panel and connect to your board. I am not sure which devices support this feature, but the Spartan7 and all Zync do.
  2. Connect to your device to establish communication between Vivado and the target.
  3. Double click the XADC to open the dashboard window.

    image

  4. From the '+' icon you can select the temperatures and voltage rails to be monitored.

image

 

This opens the dashboard window and gives a nice graph. The displayed information is helpful during debug to see if any voltage rail drops during high chip activity (e.g. a RAM stress test) or any over-temperature condition that might cause instabilities.

 

Next time I am going to talk about J9 or how to implement the SDRAM interface in VHDL on the ARTY S7.

 

Cheers,

- Wolfgang.

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 8 years ago +2
    Thanks Wolfgang, I'll keep a look out for that function when I get back to working with my Digilent Arty S7 board. Might be useful also for the Path to Programmable students who are also using Vivado.…
  • wolfgangfriedrich
    wolfgangfriedrich over 8 years ago in reply to 14rhb +2
    Cheers. Thanks for spreading the word. - W.
Parents
  • 14rhb
    14rhb over 8 years ago

    Thanks Wolfgang,

     

    I'll keep a look out for that function when I get back to working with my Digilent Arty S7 board. Might be useful also for the Path to Programmable students who are also using Vivado.

     

    Rod

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 8 years ago

    Thanks Wolfgang,

     

    I'll keep a look out for that function when I get back to working with my Digilent Arty S7 board. Might be useful also for the Path to Programmable students who are also using Vivado.

     

    Rod

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • wolfgangfriedrich
    wolfgangfriedrich over 8 years ago in reply to 14rhb

    Cheers.

    Thanks for spreading the word.

    - W.