Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Wemos d1 Battery Shield - charging 18650 Li-on Battery
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: neilk
  • Date Created: 24 Mar 2019 6:11 PM Date Created
  • Views 3209 views
  • Likes 5 likes
  • Comments 3 comments
  • li-ion
  • 18650
  • esp8266
  • wemos
Related
Recommended

Wemos d1 Battery Shield - charging 18650 Li-on Battery

neilk
neilk
24 Mar 2019

When the final long term test of power consumption of my Wemos d1 mini temperature monitoring system was complete:

 

Power Consumption of a Wemos D1 mini ESP8266 - Long Term Test 3

 

I decided to try recharging the battery - from a mobile phone charger - whilst the Wemos d1 mini was still connected, so that I could monitor the charging process.

 

image

After charging the battery for just over 2 hours I had to go out, leaving the house empty, except for #sadiethecat1409 (Instagram). I disconnected the charger because I felt uneasy about leaving it charging unattended.

 

While I was out I had the idea of charging the battery from the mobile phone power bank that failed to run the Wemos d1 mini in my first blog in this series, here is the result:

 

image

 

After about 2.5 hours on the power bank, the battery voltage, as measured by the A/D on the Wemos d1 mini, has reached 4.31V. By this time, I would have hoped that the blue LED on the battery shield would have come on to indicate that the battery was fully charged. Alas it didn't!

 

The series of blips which follow the plateau are:

  1. Disconnecting the power bank and reconnecting the mobile phone charger, to see if the charger delivered a higher voltage - it didn't
  2. Re-connecting the power bank
  3. Disconnecting the power bank and leaving the Wemos d1 mini to run for a while.

 

Conclusion

 

Using a mobile phone power bank provides an ideal method of recharging the battery of a system designed to run in an environment where there is no mains power.

 

I think this is a better approach than one in which the battery is replaced, because replacing the battery could cause disturbance to the system and will result in a (hopefully brief) interruption to the system function - this may or may not matter.

  • Sign in to reply

Top Comments

  • neilk
    neilk over 7 years ago +3
    The prototype Temperature monitor ran in the greenhouse for just over 17 days before the battery ran out so I recharged, again from the mobile phone power bank When I saw that the voltage had stabilised…
  • DAB
    DAB over 7 years ago +2
    Nice post. DAB
  • neilk
    neilk over 7 years ago in reply to DAB +1
    Thanks, DAB
  • neilk
    neilk over 7 years ago

    The prototype Temperature monitor ran in the greenhouse for just over 17 days before the battery ran out so I recharged, again from the mobile phone power bank

     

    image

     

    When I saw that the voltage had stabilised at 4.32V, I went out to the greenhouse to see if the blue light on the battery shield had come on - no!

     

    Next time I checked the graph, I saw that the voltage had suddenly fallen and was now around 4.23 to 4.25. Out to the greenhouse again, where I saw that the charging indicator on the power bank had gone out - it had shut down because insufficient current was being drawn. I disconnected and closed up the plastic sandwich box!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 7 years ago in reply to DAB

    Thanks, DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 7 years ago

    Nice post.

     

    DAB