Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Wireless ECG
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kk99
  • Date Created: 23 Jun 2018 6:13 PM Date Created
  • Views 1115 views
  • Likes 6 likes
  • Comments 3 comments
Related
Recommended

Wireless ECG

kk99
kk99
23 Jun 2018

I would like to present my project which I made four years ago. It was wireless electrocardiograph which work with mobile device.
Main presumptions of project:
- simple analog front-end working with ARM device and responsible for data collection and transferring,
- mobile device with android system as receiver which was responsible of data presentation,
- Bluetooth connection via BTM-222 module.

 

As device responsible for data collection and pre-processing I had choose STM32F0Discovery board with custom ECG module

image

Analog front-end had simple instrumentation amplifier with low-pass amplifier as second stage. Additionally it contained also boost-converter which was responsible to provide 5V supply for board from 3,3V battery. Here is schematic of ECG amplifier:
image

At input we have high-pass filter with cutoff frequency set to 0.15 Hz  INA126PINA126P it is instrumentation amplifier with gain set to 13 Second stage it is non-inverting amplifier with gain set to 69 This amplifier is also low-pass filter with cutoff frequency set to 106 Hz This analog-front end have band 0.16 Hz 106 Hz and total gain equal to 59 dB Here is photo of this ECG amplifier
image

This board contains also BTM-222 Bluetooth module and it was connected to STM32F0Discovery board Here is photo where this board is connected to STM32F0Disocvery

image

STM32F0Discovery was responsible for following things
- conversion of ECG signal from analog-front end to digital data,

- digital processing of data: averaging, normalization, digital filtering (50 Hz notch filter and down-pass filter),

- connection and transferring data to mobile device.

Program was written in C language. Here is diagram with flow of application:

image

Mobile device with Android system was responsible for receiving and data presentation. Application was written for Android in version 2.3.5 and used graphic library called: achartengine. Here were responsibilities of mobile application:
manage connection to STM32F0Discovery board via Bluetooth
- presentation of received data: (ECG wave and heart rate variability),
- data collection to file.
Here is example screen-shoot of application:
image

In attachments there are source code for both applications. It was really nice project where I learned a lot of about analog and digital electronic.

Attachments:
wireless-ecg.zip
wireless-ecg-app.zip
  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    Nice build. DAB
  • kk99
    kk99 over 8 years ago in reply to DAB +1
    Thanks.
  • genebren
    genebren over 8 years ago +1
    Very nice project. Gene
Parents
  • genebren
    genebren over 8 years ago

    Very nice project.

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Very nice project.

    Gene