Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Wireless RS485 Remote Annunciator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: s-fly
  • Date Created: 11 Mar 2015 2:08 PM Date Created
  • Views 2196 views
  • Likes 0 likes
  • Comments 4 comments
  • wifi
  • rs485
  • wireless
  • remote
Related
Recommended

Wireless RS485 Remote Annunciator

s-fly
s-fly
11 Mar 2015

I install, test, and inspect a lot of fire alarm systems, mostly notifier, and have been thinking of a way to wirelessly control one of these panels using the rs485 annunciator port on the panel. After working in N.D. the last few months and constantly adding onto strip malls and having to run back and forth for Marshal Inspections it got old fast. I was originally thinking about using a raspberry pie with a usb to rs485 cable, then connecting to it remotely with my cell phone while tethering to pie to my tablet, but I think the data will burn out the data plan way too fast. I've been thinking that hospitals and hotels won't be too much of an issue because they usually have wifi set up.

Last night as I was checking my facebook I got an ad about spark io's new electron with 2g/3g

After reading it a bit I was thinking about maybe using it if I can get it to talk with the panel via rs485.

If all I need is to send commands to the eletron that will acknowledge, silence, & reset the panel as well as send panel events back then 3g should be all I need, not sure how much 2g can do.

 

Right now when I perform large inspections I'll connect my laptop to the sr232 printer port and use terra term to capture panel events, then use logmein on my phone to watch what comes in.

 

I doupt anyone will comment on this but if anyone can give me some advice I will appreciate it

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago +1
    Hi Christopher, A 3G/4G connection is probably the way to go, it shouldn't cost a lot monthly per site since you won't be sending/receiving much data. However, for your use-case security is a concern …
  • gadget.iom
    gadget.iom over 11 years ago +1
    I think your first step would be to see if you can find a data sheet for the 485 communications.
Parents
  • clem57
    clem57 over 11 years ago

    Can I suggest an alternative that is low cost and may handle the task? PSOC CY8CKIT-042-BLE.

    These are good if the data transferred is bursty with a distance of 100 meters or less (about the same as wireless). They are small as well. Otherwise the solution you mentioned is good for distance. Would suggest some encryption if not SSL like shabaz said.

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 11 years ago

    Can I suggest an alternative that is low cost and may handle the task? PSOC CY8CKIT-042-BLE.

    These are good if the data transferred is bursty with a distance of 100 meters or less (about the same as wireless). They are small as well. Otherwise the solution you mentioned is good for distance. Would suggest some encryption if not SSL like shabaz said.

    Cheers,

    Clem