Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Working with Modest Equipment
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 5 Feb 2016 10:45 PM Date Created
  • Views 2077 views
  • Likes 7 likes
  • Comments 15 comments
  • test
  • gear
  • lab
Related
Recommended

Working with Modest Equipment

Jan Cumps
Jan Cumps
5 Feb 2016

You'll see in my blogs that I don't use state-of-the art lab equipment.

That may point out that I'm a cheapskate. And yes, that's part of the story.

But the real reason is that I believe in modest means. I've learned that during my electronics studies.

 

I learned electronics in the 1st half of the 80's, when two things were different from now. Lab equipment was much more expensive. And there was a big crisis.

These days, I can afford to purchase a +100MHz, 4 channel oscilloscope, even mixed signal if I stress my budget a little. But I don't do that. I use a second hand DS1052E.

And I believe that my education learned me a great thing: learn to design and work with tolerance, fault margins and uncertainty.

 

Tolerance

I like to think that that is the best thing I got out of my education. Try to design with the worst component possible. Make a stable design with 10% tolerance. Use transistors with high Hfe range.

Deal with the real world at its worst.

 

These things force you to get a deep understanding of the problem domain. Almost an organic understanding.

 

The same with meters and other lab gear. When you have high-end material, it's easy to replicate tests.
When you deal with modest means, the brain has to jump in. You learn.

If you find yourself in a situation where your test gear isn't optimal, you have several choices.
The two most popular ones are:

  • give up or
  • think further.

When you choose #2, you learn. You understand and grow.

 

 

You'll often see articles from me where I use a mediocre meter, or where the signal on my oscilloscope shows significant ringing. That's my own choise. I like to go for the core of the problem.

I'm not looking for perfect images. I want to see that my design works. Or I want to see what happens in a circuit.

If precision is not part of the problem domain - I ignore it and don't take measures to avoid it. If the integrity of the signal does interest me, I use better measurement methods.

Or I visit a friend with better gear - something I plan to do again soon. I will keep you posted on that image.

  • Sign in to reply

Top Comments

  • D_Hersey
    D_Hersey over 10 years ago +4
    There is a distinction to be drawn between precision and accuracy. The DVM did not completely supplant the analog meter, for example. In critical safety situations, glancing at a needle has been found…
  • shabaz
    shabaz over 10 years ago +3
    I also like that most of us have very sensitive or very high performance equipment for helping with our projects, yet some people don't realise it! For example a radio makes an incredible test tool, possibly…
  • jw0752
    jw0752 over 10 years ago +1
    Hi Jan, I totally agree with your approach. When I started into electronics marginal equipment was all I could afford. I was a technician involved in repairing the equipment that was designed by others…
  • shabaz
    shabaz over 10 years ago in reply to Workshopshed

    Hi Andy,

     

    I think you might have a narrow browser currently? The site tries to 'gracefully' optimise page layout, so with a certain width browser the side pane with the 'Like' button disappears.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to clem57

    Not getting that myself

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Workshopshed

    Workshopshed

    Like is available when you click on article name

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago

    Great points, I could not find a like or helpful button for the main post although they are there for the comments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago

    I also like that most of us have very sensitive or very high performance equipment for helping with our projects, yet some people don't realise it!

    For example a radio makes an incredible test tool, possibly one of the most sensitive bits of kit and we all have it. And the cheap SDR dongles too.

    The PC sound card and powerful free software allows for audio related projects.

    And like Don mentions we can use high performing op-amps easily. Dev-boards are cheap, so pulling up signals and then processing them with (say) a PC is possible.

    I needed a test signal, and I'm using a frequency synthesizer dev-board from TI for it, saving 4 figure expenditure on new gear and providing a signal better than the ancient test gear from ebay that might sell for $1000+. Basically individuals can now do more.

    There was a time where if a microcontroller was needed inside a project then it also needed expensive equipment to program it in, and

    equipment to test the code. Now none of this is needed, there are cheap dev-boards for that too (and no need to even build and test the

    microcontroller portion of the project if an off-the-shelf board is used for the prototype). The bedroom lab is a real option, no need for stacks of test equipment on shelves to get a lot done. Also, there are simulation tools so testing can be virtual too. I love that many manufacturers have online tools to create circuits based on specifications, like TI has on their front page. More chance to get it right first time.

    The low-cost logic analyzers like OBLS will handle logic signals up to 100MHz I think from memory (provided there is no issue with the signals! - it is no substitute for a scope).

    Also the BeagleBone Black (or other SBCs) can sample and generate signals at 100MHz, supporting close to a Gbps of sustained capture too. I managed about 14Msps of 8-bit ADC capture with little effort (so more than enough to trigger on and capture 1MHz analogue signals), and there is a project by someone that managed 100Msps for use as a logic analyzer.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>