Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs XMUTIL ... understanding platformstats
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: albertabeef
  • Date Created: 1 May 2021 7:43 PM Date Created
  • Views 2667 views
  • Likes 4 likes
  • Comments 0 comments
  • platformstats
  • xilinx
  • xilinx-linux
  • xilinx fpga
  • xmutil
Related
Recommended

XMUTIL ... understanding platformstats

albertabeef
albertabeef
1 May 2021

In this blog series, I dive into Xilinx's new platform management utility called xmutil.

 

Introduction

In my last blog, I gave a high level overview of the xmutil utility.

XMUTIL ... a new platform and app management utility from Xilinx

 

We already saw that xmutil is a shell script, that calls the following utilities as sub-commands:

 

sub-commandsutilityreference
boardidfru_print.py?

bootfw_status

bootfw_update

image_updatehttps://github.com/Xilinx/linux-image_update

listapps

unloadapp

loadapp

dfx-mgr-clienthttps://github.com/Xilinx/dfx-mgr
platformstatsplatformstatshttps://github.com/Xilinx/platformstats
ddrqosddr-qoshttps://github.com/Xilinx/ddr-qos
axiqosaxi-qoshttps://github.com/Xilinx/axi-qos
pwrctlsom-pwr-ctlhttps://github.com/Xilinx/xmutil/blob/release-2020.2.2_k26/som-pwrctl

 

 

In this blog, I start investigating how to port this utility to a custom platform (in this case, Ultra96-V2), starting with the platformstats sub-command / utility.

 

Installing xmutil on Ultra96-V2

In order to understand how the xmutil works, lets install the xmutil and platformstats components to the Ultra96-V2 board.

 

Note that I am using my Vitis-AI 1.3 image for Ultra96-V2 for this exercise :
http://avnet.me/vitis-ai-1.3-project

 

On our embedded Ultra06-V2 platform, let's start by creating a xmutil directory to work with:

 

mkdir xmutil

cd xmutil

 

Next, let's clone the xmutil repository, and install the shell script to the /usr/bin directory:

 

git clone https://github.com/Xilinx/xmutil

cd xmutil

cp xmutil /usr/bin/.

cd ..

 

Finally, let's clone the platformstats repository, build the utility, and install to the expected location (I figured this out with trial and error):

 

git clone -b avnet-2020.2 https://github.com/Xilinx/platformstats

cd platformstats

./build.sh

cp src/libplatformstats.so.1.0 /usr/lib/.

ln -s /usr/lib/libplatformstats.so.1.0 /usr/lib/libplatformstats.so.1

ln -s /usr/lib/libplatformstats.so.1 /usr/lib/libplatformstats.so

cp platformstats /usr/bin/.

cd ..

 

If we run the platformstats sub-command via xmutil, with the "-a" argument, we get the following output:

 

root@u96v2-sbc-base-2020-2:~/xmutil/platformstats# xmutil platformstats -a

 

CPU Utilization

CPU0    :     6.222449%

CPU1    :     0.100000%

CPU2    :     0.100000%

CPU3    :     0.100000%

 

RAM Utilization

MemTotal      :     2036740 kB

MemFree       :     1513088 kB

MemAvailable  :     1717784 kB

 

Swap Mem Utilization

SwapTotal    :    0 kB

SwapFree     :    0 kB

 

Power Utilization

no hwmon device found for ina260_u14 under /sys/class/hwmon

no hwmon device found for ams under /sys/class/hwmon

 

CMA Mem Utilization

CmaTotal   :     0 kB

CmaFree    :     0 kB

 

CPU Frequency

match not foundCPU0     :    0.000000 MHz

match not foundCPU1     :    0.000000 MHz

 

Most of the code seems to be generic, making use of the standard linux file system.

 

platformstats optiondescriptionreference
-cCPU Utilization/proc/stat
-rRAM Utilization/proc/meminfo (lines 1-3)
-sSwap Mem UItilization/proc/meminfo (lines 15-16)
-pPower Utilization/sys/class/hwmon/hwmon*/*
-mCMA Memory Utilization/proc/meminfo (lines 38-39)
-fCPU Frequency/proc/cpuinfo

 

The "CPU Frequency" hangs, and I don't know why.  I noticed that is also hangs on the KV260.

 

The "Power Utilization" is not working on Ultra96-V2, and is looking for "ina260", "ams" devices specific to the KV260.

 

root@u96v2-sbc-base-2020-2:~/xmutil/platformstats# xmutil platformstats -p

 

Power Utilization

no hwmon device found for ina260_u14 under /sys/class/hwmon

no hwmon device found for ams under /sys/class/hwmon

 

For a custom board, therefore, this option needs to be modified.

 

 

Modifying platformstats for Ultra96-V2

I modified the code for the avnet platforms.  These modifications were based on the work I had previously done with the python based project:
https://www.hackster.io/AlbertaBeef/monitoring-power-on-the-avnet-platforms-e52a23

For the Ultra96-V2, I specified the power monitoring devices available on the pmbus as a data structure.

Note that I also included a few temperature values, which should probably be included with a new option ( -t => Temperature ).


struct pmbus_info pmbus_ultra96v2[] =

{

   //    device   address           name    label         alias  unit  division

   //  ir38060-i2c-6-45

   {  "ir38060", "6-0045",            "", "pout1", "         5V", "mW", 1000 },

   {  "ir38060", "6-0045",            "", "iout1", "         5V", "mA",    1 },

   {  "ir38060", "6-0045",            "", "iout1", "         5V", "mV",    1 },

   {  "ir38060", "6-0045", "temp1_input", "temp1", "Temperature",  "C", 1000 },

   // irps5401-i2c-6-43

   { "irps5401", "6-0043",            "", "pout1", "     VCCAUX", "mW", 1000 },

   { "irps5401", "6-0043",            "", "pout2", "  VCCO 1.2V", "mW", 1000 },

   { "irps5401", "6-0043",            "", "pout3", "  VCCO 1.1V", "mW", 1000 },

   { "irps5401", "6-0043",            "", "pout4", "     VCCINT", "mW", 1000 },

   { "irps5401", "6-0043",            "", "pout5", "    3.3V DP", "mW", 1000 },

   { "irps5401", "6-0043", "temp1_input", "temp1", "Temperature",  "C", 1000 },

   // irps5401-i2c-6-44

   { "irps5401", "6-0044",            "", "pout1", "   VCCPSAUX", "mW", 1000 },

   { "irps5401", "6-0044",            "", "pout2", "   PSINT_LP", "mW", 1000 },

   { "irps5401", "6-0044",            "", "pout3", "  VCCO 3.3V", "mW", 1000 },

   { "irps5401", "6-0044",            "", "pout4", "   PSINT_FP", "mW", 1000 },

   { "irps5401", "6-0044",            "", "pout5", " PSPLL 1.2V", "mW", 1000 },

   { "irps5401", "6-0044", "temp1_input", "temp1", "Temperature",  "C", 1000 },

   //

   { "", "", "", "", "", 1 }

};

 

I did the same for the UltraZed-EVCC:

 

struct pmbus_info pmbus_uz7ev_evcc[] =

{

   //    device   address           name    label                        alias  unit  division

   //  ir38063-i2c-3-4c

   {  "ir38063", "3-004c",            "", "pout1", "              Carrier 3V3", "mW", 1000 },

   //  ir38063-i2c-3-4b

   {  "ir38063", "3-004b",            "", "pout1", "              Carrier 1V8", "mW", 1000 },

   // irps5401-i2c-3-4a

   { "irps5401", "3-004a",            "", "pout1", "      Carrier 0V9 MGTAVCC", "mW", 1000 },

   { "irps5401", "3-004a",            "", "pout2", "      Carrier 1V2 MGTAVTT", "mW", 1000 },

   { "irps5401", "3-004a",            "", "pout3", "         Carrier 1V1 HDMI", "mW", 1000 },

//{ "irps5401", "3-004a",            "", "pout4", "                   Unused", "mW", 1000 },

   { "irps5401", "3-004a",            "", "pout5", "Carrier 1V8 MGTVCCAUX LDO", "mW", 1000 },

   // irps5401-i2c-3-49

   { "irps5401", "3-0049",            "", "pout1", "    Carrier 0V85 MGTRAVCC", "mW", 1000 },

   { "irps5401", "3-0049",            "", "pout2", "         Carrier 1V8 VCCO", "mW", 1000 },

   { "irps5401", "3-0049",            "", "pout3", "         Carrier 3V3 VCCO", "mW", 1000 },

   { "irps5401", "3-0049",            "", "pout4", "          Carrier 5V MAIN", "mW", 1000 },

   { "irps5401", "3-0049",            "", "pout5", " Carrier 1V8 MGTRAVTT LDO", "mW", 1000 },

   { "irps5401", "3-0049", "temp1_input", "temp1", "              Temperature",  "C", 1000 },

   //  ir38063-i2c-3-48

   {  "ir38063", "3-0048",            "", "pout1", "          SOM 0V85 VCCINT", "mW", 1000 },

   // irps5401-i2c-3-47

   { "irps5401", "3-0047",            "", "pout1", "           SOM 1V8 VCCAUX", "mW", 1000 },

   { "irps5401", "3-0047",            "", "pout2", "                  SOM 3V3", "mW", 1000 },

   { "irps5401", "3-0047",            "", "pout3", "           SOM 0V9 VCUINT", "mW", 1000 },

   { "irps5401", "3-0047",            "", "pout4", "       SOM 1V2 VCCO_HP_66", "mW", 1000 },

   { "irps5401", "3-0047",            "", "pout5", "    SOM 1V8 PSDDR_PLL LDO", "mW", 1000 },

   { "irps5401", "3-0047", "temp1_input", "temp1", "              Temperature",  "C", 1000 },

   // irps5401-i2c-3-46

   { "irps5401", "3-0046",            "", "pout1", "        SOM 1V2 VCCO_PSIO", "mW", 1000 },

   { "irps5401", "3-0046",            "", "pout2", "     SOM 0V85 VCC_PSINTLP", "mW", 1000 },

   { "irps5401", "3-0046",            "", "pout3", "  SOM 1V2 VCCO_PSDDR4_504", "mW", 1000 },

   { "irps5401", "3-0046",            "", "pout4", "     SOM 0V85 VCC_PSINTFP", "mW", 1000 },

   { "irps5401", "3-0046",            "", "pout5", "    SOM 1V2 VCC_PSPLL LDO", "mW", 1000 },

   { "irps5401", "3-0046", "temp1_input", "temp1", "              Temperature",  "C", 1000 },

   //

   { "", "", "", "", "", 1 }

};

 

And the same for the UltraZed-EG IOCC and PCIE carrier cards:

 

struct pmbus_info pmbus_uz3eg_xxx[] =

{

   //    device   address           name    label         alias  unit  division

   // irps5401-i2c-3-43

   { "irps5401", "3-0043",            "", "pout1", "       PSIO", "mW", 1000 },

   { "irps5401", "3-0043",            "", "pout2", "     VCCAUX", "mW", 1000 },

   { "irps5401", "3-0043",            "", "pout3", "    PSINTLP", "mW", 1000 },

   { "irps5401", "3-0043",            "", "pout4", "    PSINTFP", "mW", 1000 },

   { "irps5401", "3-0043",            "", "pout5", "      PSPLL", "mW", 1000 },

   { "irps5401", "3-0043", "temp1_input", "temp1", "Temperature",  "C", 1000 },

   // irps5401-i2c-3-44

   { "irps5401", "3-0044",            "", "pout1", "     PSDDR4", "mW", 1000 },

   { "irps5401", "3-0044",            "", "pout2", "     INT_IO", "mW", 1000 },

   { "irps5401", "3-0044",            "", "pout3", "       3.3V", "mW", 1000 },

   { "irps5401", "3-0044",            "", "pout4", "        INT", "mW", 1000 },

   { "irps5401", "3-0044",            "", "pout5", "   PSDDRPLL", "mW", 1000 },

   { "irps5401", "3-0044", "temp1_input", "temp1", "Temperature",  "C", 1000 },

   // irps5401-i2c-3-45

   { "irps5401", "3-0045",            "", "pout1", "    MGTAVCC", "mW", 1000 },

   { "irps5401", "3-0045",            "", "pout2", "         5V", "mW", 1000 },

   { "irps5401", "3-0045",            "", "pout3", "       3.3V", "mW", 1000 },

   { "irps5401", "3-0045",            "", "pout4", "  VCCO 1.8V", "mW", 1000 },

   { "irps5401", "3-0045",            "", "pout5", "    MGTAVTT", "mW", 1000 },

   { "irps5401", "3-0045", "temp1_input", "temp1", "Temperature",  "C", 1000 },

   //

   { "", "", "", "", "", 1 }

};

 

The print_pmbus_info function scans the /sys/class/hwmon to find the matching pmbus device, address, and label, then displays the value.  I admit the code is not very clean, but gets the job done.

 

Finally, I use the hostname command to determine which Avnet board we are running on:

 

int print_power_utilization(int verbose_flag)

{

  FILE *fp;

  char hostname[128] = "";

 

  fp = popen("hostname", "r");

  if (fp != NULL) {

    if ( fgets(hostname, sizeof(hostname), fp) != NULL ) {

      if (verbose_flag)

      {

        printf("hostname=%s\n", hostname);

      }

    }

    pclose(fp);

  }

 

  if ( strstr(hostname,"u96v2") )

  {

    if (verbose_flag)

    {

      printf("Ultra96-V2\n");

    }

    print_pmbus_info(verbose_flag,pmbus_ultra96v2);

  }

  if ( strstr(hostname,"uz7ev") )

  {

    if (verbose_flag)

    {

      printf("UltraZed-7EV-EVCC\n");

    }

    print_pmbus_info(verbose_flag,pmbus_uz7ev_evcc);

  }

  if ( strstr(hostname,"uz3eg") )

  {

    if (verbose_flag)

    {

      printf("UltraZed-3EG\n");

    }

    print_pmbus_info(verbose_flag,pmbus_uz3eg_xxx);

  }

 

 

return(0);

}

 

Let's clone this version of the platformstats repository, re-build, and re-install:

 

git clone -b avnet-2020.2 https://github.com/AlbertaBeef/platformstats platformstats_avnet

cd platformstats_avnet

./build.sh

cp src/libplatformstats.so.1.0 /usr/lib/.

ln -s /usr/lib/libplatformstats.so.1.0 /usr/lib/libplatformstats.so.1

ln -s /usr/lib/libplatformstats.so.1 /usr/lib/libplatformstats.so

cp platformstats /usr/bin/.

cd ..

 

Now if we run the platformstats sub-command via xmutil on the Ultra96-V2 board, we get the following:

 

root@u96v2-sbc-base-2020-2:~/xmutil/platformstats_avnet# xmutil platformstats -p

 

Power Utilization:

        ir38060@6-0045-pout1 (         5V) = 5062 mW

        ir38060@6-0045-iout1 (         5V) = 1187 mA

        ir38060@6-0045-iout1 (         5V) = 1187 mV

        ir38060@6-0045-temp1 (Temperature) = 61 C

        irps5401@6-0043-pout1 (     VCCAUX) = 156 mW

        irps5401@6-0043-pout2 (  VCCO 1.2V) = 0 mW

        irps5401@6-0043-pout3 (  VCCO 1.1V) = 125 mW

        irps5401@6-0043-pout4 (     VCCINT) = 1218 mW

        irps5401@6-0043-pout5 (    3.3V DP) = 0 mW

        irps5401@6-0043-temp1 (Temperature) = 54 C

        irps5401@6-0044-pout1 (   VCCPSAUX) = 281 mW

        irps5401@6-0044-pout2 (   PSINT_LP) = 250 mW

        irps5401@6-0044-pout3 (  VCCO 3.3V) = 500 mW

        irps5401@6-0044-pout4 (   PSINT_FP) = 656 mW

        irps5401@6-0044-pout5 ( PSPLL 1.2V) = 46 mW

        irps5401@6-0044-temp1 (Temperature) = 56 C

 

What Next ?

Which sub-command should we investigate next ?