Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs You Are Here
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 13 Jan 2019 9:43 PM Date Created
  • Views 1836 views
  • Likes 15 likes
  • Comments 7 comments
  • jlcpcb
  • seeed studios
  • seeed
  • pcb
  • led
  • reverse
  • cool led display
  • artistic
  • not_a_badge
Related
Recommended

You Are Here

wolfgangfriedrich
wolfgangfriedrich
13 Jan 2019

I decided to explore the artistic PCB realm and the map location pin became the theme.

A reverse mounted red LED, powered by a CR2032 coin cell, is shining through the PCB to provide a bright homing beacon.

 

Soon also available in blue.

 

The 1st installment is the classic maps pin inspired by your favorite 'show me the way' tool.  The 2nd version has the outline of the more modern icon that can be found everywhere by now, even on my milk carton.

image

The reverse mounted LED is driven by a 3V coin cell through a simple 200 Ohm current limiting resistor. This provides ~5mA for the LED to balance brightness against battery life. A micro-switch can turn the LED on and off without the need to remove the battery,easily accessible on the top of the pin.

The batteries I have tested lasted more than 6 hours at reasonable brightness with a measured current of >2mA. And then it is running for another 24 hours at 2 to 1mA and still the LED is shining considerably bright through the PCB.

imageimage

 

A circuit for a quasi-constant current supply is also designed onto the board, to run the LED from 5-20V without a battery. Here the LED can also be controlled by an additional external signal.  This requires wires soldered to the pin and makes not as mobile but would be a good option for a more permanent wearable installation. Details about this circuit are documented here.

 

The boards were manufactured by Seed Studio (Classic version) and JLCPCB (Modern).

 

They are not_a_badge and if you really like them, they are available for sale in my Tindie shop image.

 

I sell on Tindie

 

- W.

 

PS:  Don't get lost. image

  • Sign in to reply

Top Comments

  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago in reply to genebren +3
    They are red LEDs, the forward voltage for white ones would be too high to be run off a coin cell. No, nothing is 3D printed, just a PCB and components. I make a little bit of money, if I don't think about…
  • Fred27
    Fred27 over 7 years ago +3
    That's a great fun project. Do you have any specific plans for them? I used a reverse mount RGB LED shining through the PCB substrate on a recent project. Great for a nice diffuse light. You can also define…
  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago in reply to Fred27 +3
    Thanks for the kind words. Yes, big plans. I will sell thousands of them and people will not be lost any more because they know where they are and I become super rich . The real thing looks even better…
Parents
  • dubbie
    dubbie over 7 years ago

    Wolfgang,

     

    A really neat and inspiring project. It spins off all sorts of possibilities.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 7 years ago

    Wolfgang,

     

    A really neat and inspiring project. It spins off all sorts of possibilities.

     

    Dubbie