Personal Blogs
  • Community Hub
  • More
Personal Blogs
Bruce Prewit's Blog Embedded Pi - Part 1
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bprewit
  • Date Created: 5 Aug 2013 6:53 PM Date Created
  • Views 1353 views
  • Likes 1 like
  • Comments 0 comments
  • st_micro
  • rasperry_pi
  • embedded_pi
Related
Recommended

Embedded Pi - Part 1

bprewit
bprewit
5 Aug 2013

After anxiously awaiting arrival of the Embedded Pi board, I was (unfortunately) not able to take a look at it for quite some time. The description of the board piqued my interest -- I can see all sorts of possibilities for it.  My initial task was to use the examples provided to exercise the ePi and get a feel for the development flow required.

 

The Embedded Pi has three modes of operation:

     - The STM32 Standalone Mode, where the ePi is configured strictly as an STM32 board.  In this configuration, the STM32 is mapped to the pinout for Arduino shields.

     - The RasPi mode, where the ePi serves as a bridge between the RasPi and the Arduino shield;

     - The ST/Adapter Mode with the RasPi communicating to the STM32 via UART, and the STM32 is mapped to the Arduino shield.

 

I will be evaluating the ePi in all three modes, but first I need to set up the environment required to program it ..

 

Unboxing the Embedded Pi, the package contained

          - The Embedded Pi board

          - A USB Cable for linking it to a PC

          - A CDROM with the CooCox tools.

 

I opted to download the CooCox software from there website (here) using their CoCenter tool.  By using CoCenter, all that I had to do was click on "Install" and the product was downloaded and installed automatically.  Hard to beat that for easy installation.

 

However, there are a couple of "gotchas" in their software:  First, it's Windows-only.  This was somewhat disappointing as most of the larger semiconductor companies - TI, Microchip, and NXP to name a few -- are offering Linux and Mac versions of there development tools. Yes, there is plenty of literature available regarding developing for the STM32 on Linux or Mac -- but I have never been able to get anything to work correctly yet. The second issue, and it's a minor one, is that CoIDE requires a separate installation of GCC/Arm to function. Embest did provide an appropriate link, and I was able to get the CoIDE tool setup and configured fairly quickly.

 

The next hurdle was to actually get a program into the board.  I initially followed the directions here to program the ePi via the RasPi serial port. Note that the article says towards the end:

"If a prompt of “None” always appears, redo step 1 (press BOOT0 to reset the STM32)."; this is incorrect .. it should be "Hold BOOT0 while resetting the board" or words to that effect.

 

Unfortunately, no matter what I tried (different baud rates, attaching a ground, etc) I could not get the ePi to reliably program. In fact, the board had to be repeatedly reset to get it to program at all.Once I got frustrated with that approach, I re-read the User Guide, which very clearly states: "Since Embedded Pi has no debugger onboard, an external JTAG/SWD debugger is needed to

program Embedded Pi in the External Debugger Mode, like J-Link and CoLinkEx.".  It would have been nice to have included the SWD on-board (not uncommon) but Oh, well.

 

So, I ordered the CoLinkEx from Newark (here); the product arrived and functioned as designed and I was able to get a test program onto the board fairly quickly.

 

With that done, I was ready to try the CooCox examples; Part 2 will cover programming the ePi in STM32 Standalone Mode.

 

Note:  In the interest of completeness, I attempted to examine the CD-ROM that was included with the ePi; nothing I had (Windows, Linux, or Mac) would read it ... my conclusion is that the CD-ROM was defective.