Personal Blogs
  • Community Hub
  • More
Personal Blogs
Clem Martins's Blog AMD laptop CPU
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: clem57
  • Date Created: 29 Oct 2019 1:17 PM Date Created
  • Views 1576 views
  • Likes 2 likes
  • Comments 6 comments
  • amd
Related
Recommended

AMD laptop CPU

clem57
clem57
29 Oct 2019
General information
TypeCPU / Microprocessor
Market segmentMobile
Family
AMD A12-Series for Notebooks
Model number ? A12-9720P
CPU part number
  • AM972PADY44AB is an OEM/tray microprocessor [1]
Frequency ? 2700 MHz
Maximum turbo frequency3600 MHz
Packagemicro-BGA
SocketBGA (FP4)
Architecture / Microarchitecture
MicroarchitectureExcavator
Processor core ? Bristol Ridge
CPUID660F51
Manufacturing process0.028 micron
Data width64 bit
The number of CPU cores4
The number of threads4
Floating Point UnitIntegrated
Level 1 cache size ? 2 x 96 KB 3-way set associative shared instruction caches
4 x 32 KB 8-way set associative data caches
Level 2 cache size ? 2 x 1 MB 16-way set associative shared caches
Level 3 cache sizeNone
MultiprocessingUniprocessor
Extensions and Technologies
  • MMX instructions
  • Extensions to MMX
  • SSE / Streaming SIMD Extensions
  • SSE2 / Streaming SIMD Extensions 2
  • SSE3 / Streaming SIMD Extensions 3
  • SSSE3 / Supplemental Streaming SIMD Extensions 3
  • SSE4 / SSE4.1 + SSE4.2 / Streaming SIMD Extensions 4 ?
  • SSE4a ?
  • AES / Advanced Encryption Standard instructions
  • AVX / Advanced Vector Extensions
  • AVX2 / Advanced Vector Extensions 2.0
  • BMI / BMI1 + BMI2 / Bit Manipulation instructions
  • F16C / 16-bit Floating-Point conversion instructions
  • FMA3 / 3-operand Fused Multiply-Add instructions
  • FMA4 / 4-operand Fused Multiply-Add instructions
  • TBM / Trailing Bit Manipulation instructions
  • XOP / eXtended Operations instructions
  • AMD64 / AMD 64-bit technology ?
  • Turbo Core technology
  • AMD-V / AMD Virtualization technology
Security Features
  • EVP / Enhanced Virus Protection ?
  • SMEP / Secure Mode Execution Protection
Low power featuresPowerNow!
Integrated peripherals / components
Integrated graphicsGPU Type: Radeon R7 series
Shader cores: 512
Base frequency (MHz): 758
Memory controllerThe number of controllers: 1
Memory channels: 2
Supported memory: DDR4-1866
Maximum memory bandwidth (GB/s): 29.9
Other peripherals
  • PCI-Express 3.0 interface
  • Unified Video Decoder ?
  • Video Coding Engine ?
  • Secure processor
Electrical / Thermal parameters
Thermal Design Power ? 15 Watt
Notes on AMD A12-9720P
  • The processor supports configurable TDP of 12 Watt
  • The processor has the following security, data protection and/or software features: AMD StartNow technology and FreeSync.
  • The graphics unit has the following software features enabled: AMD Radeon Dual Graphics, Perfect Picture, Steady Video, Virtual Super Resolution, Eyefinity technology and Frame Rate Target Control.

 

[1] - Information is not confirmed

 

My laptop died a couple of days ago and I am considering this as a purchase. I am looking for good value and not necessary fast or big. I use this day to day and for going to meetings.

Thanks for any comments to help me decide.

  • Sign in to reply

Top Comments

  • dougw
    dougw over 6 years ago +1
    Something to compare to: https://www.intel.ca/content/www/ca/en/products/processors/core/i5-processors/i5-10210u.html (uses 14 nm lithography)
  • clem57
    clem57 over 6 years ago in reply to dougw +1
    That one looks very good... I have another one to compare with in the AMD line: https://www.notebookcheck.net/A12-9720P-vs-3200U_9192_11191.247596.0.html The Ryzen 3 can be found in thie one from HP at…
  • e14 Contributor
    e14 Contributor over 6 years ago +1
    Which laptop are you considering buying that has this APU? A review of that APU: https://www.notebookcheck.net/AMD-A12-9720P-SoC-Benchmarks-and-Specs.234448.0.html
Parents
  • clem57
    clem57 over 6 years ago

    After looking at the dead laptop, I decided to try to replace the hard drive with a SSD. It took a few YouTube video's and much patience, but after three times taking it apart, it now works with Linux Mint distribution. But I need to recover the missing data from the old hard drive if I can. Looks like another weekend or so for this task.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 6 years ago

    After looking at the dead laptop, I decided to try to replace the hard drive with a SSD. It took a few YouTube video's and much patience, but after three times taking it apart, it now works with Linux Mint distribution. But I need to recover the missing data from the old hard drive if I can. Looks like another weekend or so for this task.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 6 years ago in reply to clem57

    Been there too.  Going to make it a secondary SATA?  Maybe the HDD has a USB option?  In any case, good luck with data recovery.

     

    You might want to look at this list of recovery tools: https://www.ubuntupit.com/top-15-linux-data-recovery-tools-the-professionals-choice/

    I've used the Knoppix distro in the past with some success.  Essentially, you boot from the CD/DVD/stick with Knoppix on it and use one of its current tools which might be on the referenced list.