Personal Blogs
  • Community Hub
  • More
Personal Blogs
Clem Martins's Blog Do you hate to soldier?
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: clem57
  • Date Created: 16 Apr 2015 1:08 PM Date Created
  • Views 1343 views
  • Likes 2 likes
  • Comments 13 comments
Related
Recommended

Do you hate to soldier?

clem57
clem57
16 Apr 2015

     I seem have have a phobia or mental block when it comes to soldiering. First there is the iron heating up and waiting. Later I have to be careful not to burn me or the table. Ouch!imageimage So now to check was it a good joint. Oops!image Try again until it is correct. So what am I to do? Here is a new tool that I am going to use:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

     Well to jog my memory... Oh where is that pen? Oh well next I need that string around the finger. LOLimage

 

Clem

  • Sign in to reply

Top Comments

  • johnbeetem
    johnbeetem over 11 years ago +4
    I hate soldiering too. But I don't mind solder ing You've got to have the right power, temperature, and flux to make soldering a pleasure instead of a frustration. I haven't used lead-free solder, so maybe…
  • e14 Contributor
    e14 Contributor over 11 years ago +4
    I find soldering quite relaxing just sit back, put on some music or a youtube video, get a coffee (or glass of wine if you're feeling adventurous about the future!) and take your time to enjoy it.
  • jw0752
    jw0752 over 11 years ago in reply to johnbeetem +3
    Hi John, I agree with you 100% on the intoxicating quality of the solder from the kit building era. Once in a while I will be taking apart an old piece of equipment and I will catch a whiff of that smell…
Parents
  • 4ringfan
    4ringfan over 11 years ago

    As a kid, I de-soldered literally thousands of components.  All with an inexpensive weller corded soldering iron.  I probably gave myself my asthma condition considering how much solder smoke I inhaled. image

     

    For the last 20+ years when I'm out in the field working on dental equipment that needed to be soldered, I would whip out my butane powered portable soldering iron.  https://www.masterappliance.com/heat-tool-products/butane-powered/ultratorches/ultratorch-ut-100si I think that many of my skills suffered with the use of the Butane powered soldering iron.  It always seems to be either too hot or not hot enough.  Still can't quite beat the portability of it though, and it is still a good iron.

     

    Recently I picked up a new temperature controlled bench hot air and soldering iron and I'm very much enjoying it and I am realizing what I've been missing all these years.  Nice to be able to accurately control the solder flow.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to 4ringfan

    I like the butane one but also the exhaust has burned up things before.  really nice in a pinch but yes, either too hot or too cold seems to be the story.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 4ringfan
    4ringfan over 11 years ago in reply to screamingtiger

    Ah yes, the "waste gate" image  It has caused some damage for me before as well.  Usually rotating the iron 180 degrees solved that problem though.  The heat waste does have some use however!  It works wonderfully to shrink heat shrink tubing!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 4ringfan
    4ringfan over 11 years ago in reply to screamingtiger

    Ah yes, the "waste gate" image  It has caused some damage for me before as well.  Usually rotating the iron 180 degrees solved that problem though.  The heat waste does have some use however!  It works wonderfully to shrink heat shrink tubing!