Personal Blogs
  • Community Hub
  • More
Personal Blogs
Clem Martins's Blog Maix Bit Risc V
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: clem57
  • Date Created: 25 Sep 2019 1:11 AM Date Created
  • Views 2432 views
  • Likes 5 likes
  • Comments 10 comments
  • kpu
  • risc-v
Related
Recommended

Maix Bit Risc V

clem57
clem57
25 Sep 2019

I recently came across an interesting AIoT device called Maix Risc V device. It was originally a crowd sourced campaign from Shenzhen, China. Being interested in exploring this architecture as well as neural  network processing, I decided to take the byte (Ha ha) and get one. Here is the package unopened.

 

image

 

 

Overview

 

 

Sipeed MAIX is the first RV64 AI board for Edge Computing, it makes AI embedded to any IoT device possible. MAIX have tons of excited features: Dual Core RV64 IMAFDC, 8 MB SRAM, Neural Network Processor(0.25~0.5 TOPS, support Tensor Flow Lite), APU, hardcore FFT... All this is in Square Inch, 0.3 W! Also we have made it breadboard friendly with micro python available. MAIX is open mind, everyone can contribute code/document, trade network module. MAIX can Maximize AI's power.

 

 

Sipeed MAIX: AI at the edge

 

 

AI is pervasive today, from consumer to enterprise applications.

With the explosive growth of connected devices, combined with a demand for privacy/confidentiality, low latency and bandwidth constraints, AI models trained in the cloud increasingly need to be run at the edge.

MAIX is Sipeed’s purpose-built module designed to run AI at the edge, we called it AIoT. Add to that a KPU(Neural Network Processor) inside.  This 64 KPU which is 576 bit width, supports convolution kernels and any form of activation function.

 

Without any more ado, here are the parts for the kit opened up:

 

image

 

I hope to expand more as I uncover and learn about this board. Drop a comment or two to let me know what do you think and maybe what uses you can come up with.

  • Sign in to reply

Top Comments

  • ralphjy
    ralphjy over 6 years ago in reply to clem57 +2
    These development boards come in several different variations. I've decided to try the "Maixduino" which is quite a bit larger because of the Arduino form factor but it includes an ESP32 for WiFI and Bluetooth…
  • clem57
    clem57 over 6 years ago +2
    In browsing the internet about Maix Risc V, I came across this: https://www.hackster.io/news/a-new-risc-v-based-ai-hat-for-the-raspberry-pi-from-seeed-studio-6ca6ac5af7ce Seems like a prototype is done…
  • ralphjy
    ralphjy over 6 years ago +1
    I've seen those from Seeed but haven't got around to trying one. I'll be interested in seeing how you do with it. Did you get a new version or old version? The new version has the MEMS microphone.
Parents
  • clem57
    clem57 over 6 years ago

    Over the weekend, I continued to used my Maix Bit and was successful using the video to the LCD. It was very clear and had nice colours to boot. When I get time, I intend to do a separate write up...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 6 years ago

    Over the weekend, I continued to used my Maix Bit and was successful using the video to the LCD. It was very clear and had nice colours to boot. When I get time, I intend to do a separate write up...