Personal Blogs
  • Community Hub
  • More
Personal Blogs
Douglas Wong's Blog Miracle Batteries
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 12 Dec 2020 3:58 AM Date Created
  • Views 3501 views
  • Likes 11 likes
  • Comments 12 comments
  • doug wong
  • micronta
  • enercell
  • radio shack
Related
Recommended

Miracle Batteries

dougw
dougw
12 Dec 2020

My first digital multimeter was a Micronta....here it is, fresh from my museum archives:

imageimage

I remember being very impressed with its long battery life when I was using it decades ago, probably because it didn't use LEDs. But now I just turned it on and it powered right up, so I checked the batteries and they look pristine. The absolutely astounding thing is I believe these are the original Radio Shack Enercell Extra Life batteries bought when the meter was new! More than 3 decades ago! I did hang out at Radio Shack in the 70's and 80's but I definitely haven't bought batteries at Radio Shack for decades. I just measured the voltages at 1.54 V and 1.539 V.

Count me astonished, gobsmacked, flabergasted and totally blown away at how they can still be in this pristine condition. On the batteries it says they have a "miracle seal" - that is obviously not just hype. I have never seen any AA batteries sit on a shelf for a decade without dying and spewing their guts all over the battery compartment. I am going to have to see if these batteries are still in production - they are truly spectacular.

  • Sign in to reply

Top Comments

  • Andrew J
    Andrew J over 5 years ago +7
    That is impressive. I was sat by the computer a week or so ago and could hear this curious ticking sound. Using the power of cross-triangulation - i.e. moving my head around to pick up the direction of…
  • koudelad
    koudelad over 5 years ago +6
    That is really an impressive find, dougw . My colleague recommended me these Energizer Industrial cells , which have a shelf life of 10 years. I bought a few of them to supply power to my IR thermometer…
  • ntewinkel
    ntewinkel over 5 years ago +5
    It's impressive how long they lasted and how little power the tester uses, but most impressive might be the fact that the batteries didn't leak! I'd pay a lot extra for batteries that don't leak, especially…
Parents
  • ralphjy
    ralphjy over 5 years ago

    Wow!  That really is impressive.  I remember being part of Radio Shack's "battery club".  I guess I was only affording the cheaper batteries because I was always replacing them.

     

    I wish all batteries would perform this well.  There are so many forgotten places where batteries hide and unfortunately usually end up in a corroded mess.  Of course, nowadays it's more frightening with the failure modes of Lithium batteries image.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago in reply to ralphjy

    Lithium batteries need to come with a built-in pressure sensor.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 5 years ago in reply to ralphjy

    Lithium batteries need to come with a built-in pressure sensor.

    • Cancel
    • Vote Up +3 Vote Down