Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog A Beginning Journey in TensorFlow #2: Simple Image Recognition
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 1 Oct 2019 6:12 AM Date Created
  • Views 1827 views
  • Likes 9 likes
  • Comments 7 comments
  • tensorflow
  • image classification
  • colab
  • vision thing
  • keras
  • image recognition
  • raspberry pi
  • deep learining
Related
Recommended

A Beginning Journey in TensorFlow #2: Simple Image Recognition

fmilburn
fmilburn
1 Oct 2019

This is the second of a series exploring TensorFlow.  Since I have no training in machine learning it does not consist of tutorials but has links to the material that I am using.  I use my Windows PC to train models and plan to use a Raspberry Pi to do object classification.  The main purpose will be to document the things I learn along the way and perhaps interest you in a similar journey.

 

Recap

 

TensorFlow can do two types of deep learning:  Regression and Classification.  In the last post Regression was described.  In the model diagrammed below (taken from Udacity training material) input data feeds one or more dense hidden layers and gives a single output number.

image

In this post the model is extended to recognize classifications of images, in this case clothing.  The output for an image after training is the probability that it is one of the classes that have been was in the training dataset.

 

Flattening the Image

 

The model takes in a vector as input.  Accordingly, the pixels in the two dimensional image are converted to a one dimensional array as shown in the very simple example below.

image

The training dataset in this example used here has 28 x 28 pixel gray scale images.  The grey scale values  for each pixel will be normalized to floating point numbers between 0 and 1.

 

NMIST Fashion Dataset

 

The NMIST Fashion Dataset is easily imported into Colab which is the Jupyter notebook in the cloud that is used in conjunction with the Udacity training.  It consists of low resolution 28 x 28 pixel gray scale images for 10 different types of clothing.  There are 70,000 images in total with a sample shown below.

image

As noted above the resolution of the images is quite low.

image

One of my observations from facial recognition was that it also was able to do classification with low resolution images which was a surprise to me.

 

Developing a Model

 

The dataset is split into two parts:

  • Training Dataset:  60,000 representative images that will be used to train the model
  • Test Dataset:  10,000 images used to test the model after training - must be images the model has not seen before

 

The images are flattened as described above and pixels normalized to values between 0 and 1.  The model itself is very similar to a Regression model with exceptions as outlined in the diagram below taken from the Udacity training material.

image

  • A single dense layer of arbitrary 128 units is selected
  • The activation function ReLU is added to the layer which allows it to solve non-linear equations
  • The output layer has 10 units corresponding to the items of clothing in the input dataset and uses SoftMax for the activation function

 

The model is compiled using the optimizer 'adam' as used before but a new loss function 'sparse_categorical_crossentropy' is introduced without much discussion.  It is said to be used normally for these type models.  Training is  done for 5 epochs.

 

In Colab, which runs in the cloud, the training completes in about 2 minutes with 89% accuracy.

image

The test dataset has 87% accuracy and all 10,000 images are analyzed in 3 seconds.

image

 

Conclusion and Looking Ahead

 

The 87% accuracy may or may not be acceptable for a given application but I have looked ahead to the next lesson and know that it provides information that will improve accuracy.  Accordingly, I will wait until then to develop my own dataset for training.

 

Useful Links

 

A Beginning Journey in TensorFlow #1: Regression

A Beginning Journey in TensorFlow #3: ReLU Activation

A Beginning Journey in TensorFlow #4: Convolutional Neural Networks

A Beginning Journey in TensorFlow #5: Color Images

A Beginning Journey in TensorFlow #6: Image Augmentation and Dropout

RoadTest with OpenCV

Picasso Art Deluxe with OpenCV

Udacity Into to TensorFlow for DeepLearning

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 6 years ago in reply to 14rhb +3
    Thanks! The basic concept is simple although the details not so much. But it seems that it is now where practical application is within grasp. I really recommend the Google course on Udacity that is linked…
  • 14rhb
    14rhb over 6 years ago +1
    Hi fmilburn , This is great work and just the sort of introduction someone like me needs - I knew nothing about how image recognition worked until I read your blog(s), so thank you. I use the plural because…
  • 14rhb
    14rhb over 6 years ago in reply to fmilburn +1
    It also made more sense when I realised this was blog #2 (although you do say so) and read your posts in the right order
Parents
  • 14rhb
    14rhb over 6 years ago

    Hi fmilburn ,

     

    This is great work and just the sort of introduction someone like me needs - I knew nothing about how image recognition worked until I read your blog(s), so thank you. I use the plural because I noticed you have another blog as well which I need to read through image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to 14rhb

    Thanks!

     

    The basic concept is simple although the details not so much.  But it seems that it is now where practical application is within grasp.  I really recommend the Google course on Udacity that is linked above.  They explain the basics well and the online notebook Colab makes it easy to get started.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 6 years ago in reply to fmilburn

    It also made more sense when I realised this was blog #2 (although you do say so) and read your posts in the right order image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to 14rhb

    True, it is there but easy to miss.  I'll make that a bit clearer when I make the next post :-).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 6 years ago in reply to fmilburn

    It really was just me, eager to get your great content without reading the intro as carefully as I should !

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 6 years ago in reply to fmilburn

    It really was just me, eager to get your great content without reading the intro as carefully as I should !