Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog A Beginning Journey in TensorFlow #6: Image Augmentation and Dropout
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 20 Oct 2019 3:56 AM Date Created
  • Views 3881 views
  • Likes 7 likes
  • Comments 8 comments
  • neural network
  • tensorflow
  • image classification
  • colab
  • cnn
  • vision thing
  • keras
  • image recognition
  • raspberry pi
  • machine learning
  • deep learning
  • regression
Related
Recommended

A Beginning Journey in TensorFlow #6: Image Augmentation and Dropout

fmilburn
fmilburn
20 Oct 2019

This is the 6th post of a series exploring TensorFlow.  The primary source of material used is the Udacity course "Intro to TensorFlow for Deep Learning" by TensorFlow.  My objective is to document some of the things I learn along the way and perhaps interest you in a similar journey.  In a follow-on series I intend to cover TensorFlow Lite using a Raspberry Pi.

 

Recap

 

In the last post complex color image categorization and the concept of validation was introduced.  The issues associated with overfitting and underfitting the model were presented.  In this post Dropout, a method for reducing overtraining will be covered as well as Augmentation, a method for increasing the training dataset size and quality.

 

Dropout

 

During training the neural network adjusts weights and biases to minimize the loss function.  This can result in certain neurons obtaining large weights relative to other neurons which causes them to dominate the network.  As a result the neurons with smaller weights don't get trained much.  Dropout is a way to avoid this by randomly turning off some neurons in the network during training.  This allows the other neurons to receive more training.  For example, in the example below taken from the Udacity training two neurons (shown filled with black) are randomly turned off, one in each row during an epoch.  In subsequent epochs this random selection is continued.

 

image

Feed forward and back propagation continues without using the neurons that have been turned off.  This helps avoid overfitting and the network utilizes all the neurons more efficiently.

 

Augmentation

 

It is desirable for the model to recognize the subject no matter the size, position or where it is in the image.  In a large enough dataset all of this information may be included in the training dataset and it will be less likely to overfit.  If not, augmentation is a way to add examples with different angles, size, orientation, etc. which allows it to generalize better.

 

For example, TensorFlow can modify or transform an image as shown in the example below.

image

Example snippets of code and the results are shown below.

 

Flipping Images

image_gen = ImageDataGenerator(rescale=1./255, horizontal_flip=True)


train_data_gen = image_gen.flow_from_directory(batch_size=BATCH_SIZE,
                                               directory=train_dir,
                                               shuffle=True,
                                               target_size=(IMG_SHAPE,IMG_SHAPE))

image

 

 

Rotating Images

image_gen = ImageDataGenerator(rescale=1./255, rotation_range=45)


train_data_gen = image_gen.flow_from_directory(batch_size=BATCH_SIZE,
                                               directory=train_dir,
                                               shuffle=True,
                                               target_size=(IMG_SHAPE, IMG_SHAPE))

image

 

Zoomed images

image_gen = ImageDataGenerator(rescale=1./255, zoom_range=0.5)


train_data_gen = image_gen.flow_from_directory(batch_size=BATCH_SIZE,
                                               directory=train_dir,
                                               shuffle=True,
                                               target_size=(IMG_SHAPE, IMG_SHAPE))

image

 

Building a Model

 

It is possible to apply all the augmentation transformations as shown in the code snippet that follows:

image_gen_train = ImageDataGenerator(

      rescale=1./255,
      rotation_range=40,
      width_shift_range=0.2,
      height_shift_range=0.2,
      shear_range=0.2,
      zoom_range=0.2,
      horizontal_flip=True,
      fill_mode='nearest')

train_data_gen = image_gen_train.flow_from_directory(batch_size=BATCH_SIZE,
                                                     directory=train_dir,
                                                     shuffle=True,
                                                     target_size=(IMG_SHAPE,IMG_SHAPE),
                                                     class_mode='binary')

image

 

Validation data is generally scaled but not augmented.

image_gen_val = ImageDataGenerator(rescale=1./255)


val_data_gen = image_gen_val.flow_from_directory(batch_size=BATCH_SIZE,
                                                 directory=validation_dir,
                                                 target_size=(IMG_SHAPE, IMG_SHAPE),
                                                 class_mode='binary')

 

The convolution and compiling of the model remains the same as the previous example.  The model definition remains the same as the previous example except that a dropout of 0.5 (50% of the values coming into the dropout layer are zeroed) is specificied just before flattening and the dense layers.

model = tf.keras.models.Sequential([

    tf.keras.layers.Conv2D(32, (3,3), activation='relu', input_shape=(150, 150, 3)),
    tf.keras.layers.MaxPooling2D(2, 2),

    tf.keras.layers.Conv2D(64, (3,3), activation='relu'),
    tf.keras.layers.MaxPooling2D(2,2),

    tf.keras.layers.Conv2D(128, (3,3), activation='relu'),
    tf.keras.layers.MaxPooling2D(2,2),

    tf.keras.layers.Conv2D(128, (3,3), activation='relu'),
    tf.keras.layers.MaxPooling2D(2,2),

    tf.keras.layers.Dropout(0.5),
    tf.keras.layers.Flatten(),
    tf.keras.layers.Dense(512, activation='relu'),
    tf.keras.layers.Dense(2, activation='softmax')
])

 

Below is the model summary.

image

Remember that previously, without augmentation or dropout, the training accuracy was 100%  (overfit) at 100 epochs and the validation accuracy of 75% was achieved in less than 20 epochs.  Adding augmentation and dropout results in the following.

 

image

Training accuracy is now about 88% (Vs. 100% before) due to the use of image augmentation.  But the image validation has improved to 84% (Vs. 75% before), a significant improvement.  According to the course training video, training should probably cease around 60 epochs which is where the curves for the training and validation start to diverge.

 

More Useful Stuff

 

The following site gives more information on overfitting:  Memorization is not learning!

 

There is some additional material in the course that I recommend but which will not be covered here::

  • Transfer Leaning, a way to use existing networks created by experts for your own models.
  • Housekeeping such as how to save and load models
  • Time Series Forecasting
  • Introduction to TensorFlow Lite

 

I plan to cover TensorFlow Lite in more detail in future posts.

 

Conclusions and Look Ahead

 

This brings us to the end of how image classification works in TensorFlow.  At the start of the journey my knowledge was limited to following a recipe without much understanding of the underlying model.  My objective was to gain understanding without going too deeply into the math.  Conceptually, it is fairly easy but as they say the devil is in the details.  As is often the case, XKCD is able to convey this in one frame:

XKCD Machine Learning

My knowledge has now been extended to following recipes with a somewhat improved understanding of the underlying model.

 

In future posts I plan to develop my own model from scratch and move it to a Raspberry Pi running TensorFlow Lite.  Hopefully I will be able to stir the pile until something useful comes out.

 

Useful Links

 

RoadTest of Raspberry Pi 4 doing Facial Recognition with OpenCV

Picasso Art Deluxe OpenCV Face Detection

Udacity Intro to TensorFlow for Deep Learning

A Beginning Journey in TensorFlow #1: Regression

A Beginning Journey in TensorFlow #2: Simple Image Recognition

A Beginning Journey in TensorFlow #3: ReLU Activation

A Beginning Journey in TensorFlow #4: Convolutional Neural Networks

A Beginning Journey in TensorFlow #5: Color Images

  • Sign in to reply

Top Comments

  • Sean_Miller
    Sean_Miller over 6 years ago +2
    Great blog series! Hope to see more. My big question is, after I run code to train a model, how to I use it with my BBAI classification.cpp code? The classification example has close to a 1000 objects…
  • Sean_Miller
    Sean_Miller over 6 years ago in reply to fmilburn +2
    I just binged the TIDL API. Unfortunately, the page I was after, training and converting for TIDL use is temporarily down. This is the time of year I get my personal deep learning on, so I hope they get…
  • genebren
    genebren over 7 years ago +1
    Frank, The augmentation concepts seem very powerful. Covering a range of angles and sizes seems like a great way to stretch your images to improve your model. Images that are going to be recognized will…
  • genebren
    genebren over 7 years ago in reply to fmilburn

    Frank,

     

    The skinny/fat aspect might be addressed via augmentation, using stretched/squished images, creating a somewhat variable ratio within the training set of images.

     

    Just a thought.

     

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to genebren

    Hi Gene,

     

    I agree...  I am playing around with that right now.  Something that bothers me about the TensorFlow method taught in the course is that it allows scale distortion.  Dogs and cats may come in skinny and fat versions but some objects have fixed ratios. There may be ways to control this In TensorFlow but I am trying to devise a simple test to see how it might impact accuracy.  Perspective is also something I wonder about...  I am preprocessing in Photoshop for my tests. 

     

    Frank

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    Frank,

     

    The augmentation concepts seem very powerful.  Covering a range of angles and sizes seems like a great way to stretch your images to improve your model.  Images that are going to be recognized will not always be oriented straight up and down or at a given size, so I can see how this might improve accuracy.

     

    Well done!

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<