Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog AIS Alarm - PCB Version 0.1 Arrived
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 25 Jan 2018 4:02 AM Date Created
  • Views 1329 views
  • Likes 7 likes
  • Comments 7 comments
  • daisy
  • smd
  • ais
  • pcb
  • msp430
Related
Recommended

AIS Alarm - PCB Version 0.1 Arrived

fmilburn
fmilburn
25 Jan 2018

Project Objective: Develop an open source AIS Alarm that alerts sailors that a new marine vessel with AIS is within range

 

The PCBs arrived today but unfortunately I was slow in ordering the more obscure parts for the design and they have not yet arrived.  This blog post will describe populating the board with the parts I have on hand and first impressions of what will be needed for the next revision.

 

Here is a photo of the board as it currently stands:

image

It looks pretty sparse now that it is off the breadboard and onto a PCB.  I am soldering by hand using an inexpensive reflow station for the SMD components.  The parts that remain to be placed are the buzzer, dual MOSFET, and the bright 5 mm right angle LED.  I've been able to test the switches and LED indicators and they are OK.  All the traces look OK.  The board is programmed using the header on the far left.  The inside header will connect to the dAISy radio via ribbon cable.  Here are the observations so far that will need to be addressed before the next revision:

  • The boards were attached in the original panel by tabs with mouse bites that had to be taken off with a dremel tool for it to fit in the enclosure.  I will look at V-cuts  or possibly making the board slightly less wide in the final design to avoid this.
  • The board is going to slide in over the radio in the enclosure.  There is very little room between the indicator LEDs on the right and the board with the radio below it.   This prevents the use of a connector and will require hand soldering of the ribbon cable between the radio and the Alarm PCB.  I knew this was going to be a problem and am still looking for a way around it.
  • The MOSFET footprint is pretty small and will be difficult to hand solder.
  • Should add some test points.
  • The button switch on the left needs to be moved to better clear the enclosure.

 

A funny thing is that most of the issues are mechanical in nature and I am a mechanical engineer.  I find that the mechanical issues are the ones I usually iterate on the most when it comes to the PCB.

 

The remaining parts are expected by Friday but I am expecting guests for the weekend so probably won't get back to this until early next week.  But it looks like this will be good enough to iron out most of the hardware issues as well as make the next upgrade to the firmware.

 

Past Posts from this Project:

AIS Alarm

AIS Alarm - The Process

AIS Alarm - Prototype Hardware

AIS Alarm - Timers and GPIO

AIS Alarm - Prototype Code Outline

AIS Alarm - UART

AIS Alarm - First AIS Messages

AIS Alarm - First FRAM Storage

AIS Alarm - Debouncing Momentary Button Switches

AIS Alarm - FRAM Ring Buffer

AIS Alarm - Schematic

AIS Alarm - PCB Version 0.1

 

References and Links:

WEGMATT LLC - dAISy AIS Receiver - low cost AIS receiver

Texas Instruments MSP430FR2xx FRAM Microcontrollers - Post No. 4

TI MSP430FR2111

Maximize the Sound from a Buzzer

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 8 years ago in reply to genebren +3
    Hi Gene, Thanks for the feedback! Below is a photo that will give you a better idea of what I am up against by trying to use the existing dAISy aluminum enclosure: As you can see, the new PCB slides (almost…
  • genebren
    genebren over 8 years ago +2
    Frank, Nice clean looking board. To bad about the outstanding issues. Those tiny MOSFET packages are tough, but with a little practice I was able to hand solder those. Good luck there. One the issue of…
  • genebren
    genebren over 8 years ago in reply to fmilburn +2
    Frank, That is a very tight and very clean little package there. On the LEDs, you might free up some space with some bright, surface mount LEDs (side view). You could do small cut-out windows with plastic…
Parents
  • DAB
    DAB over 8 years ago

    Nice looking board.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 8 years ago

    Nice looking board.

     

    DAB