Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog AIS Alarm - PCB Version 0.2 Populated
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 20 Feb 2018 5:16 AM Date Created
  • Views 1559 views
  • Likes 7 likes
  • Comments 6 comments
  • daisy
  • ais
  • buzzer
  • msp430
Related
Recommended

AIS Alarm - PCB Version 0.2 Populated

fmilburn
fmilburn
20 Feb 2018

Project Objective: Develop an open source AIS Alarm that alerts sailors that a new marine vessel with AIS is within range

 

I worked most of last week to complete my RoadTest of the TPSM84A21EVM DC-DC Converter but on Friday the revised PCBs for the AIS Alarm arrived and today I populated two of the boards.  This is an update on how things are coming along.

 

image

The revised board is shown fully populated on the right.  If you have a look back at the first version it is clear how much cleaner the board is now and I much prefer this connection over a ribbon cable.  The interferences have also been taken care of.

 

The microcontroller is programmed over the open header on the far left of the board with pogo pins.  The buzzer is just above it.  I have two buzzers from different manufacturers and haven't decided which I prefer.  Just above the buzzer is the female header that allows connection with the dAISy radio board.  The simplified user interface consists of a LED and two buttons and are aligned along the top edge.  The tiny SOT363 MOSFET is just visible in the middle of the board with the TSSOP 16 pin microcontroller below it.  Everything else is 0805 resistors and capacitors to support.

 

 

For some reason I was having trouble soldering the TSSOP microcontrollers today.  One had a bridge I didn't think I would ever be able to remove.  The next order will include a stencil and my solder paste is getting old so need that too.  In the end both boards I put together are working and all hardware seems OK.

 

The photograph on the left shows the second board fitted into the case.  I like the aesthetics of it.  Everything fits nicely although snug.

 

I haven't made any progress on the firmware due to the RoadTest so I need to get back on that.  I also need to design the end panel for the case which will fit over the LED and switches.

 

Past Posts from this Project:

AIS Alarm

AIS Alarm - The Process

AIS Alarm - Prototype Hardware

AIS Alarm - Timers and GPIO

AIS Alarm - Prototype Code Outline

AIS Alarm - UART

AIS Alarm - First AIS Messages

AIS Alarm - First FRAM Storage

AIS Alarm - Debouncing Momentary Button Switches

AIS Alarm - FRAM Ring Buffer

AIS Alarm - Schematic

AIS Alarm - PCB Version 0.1

AIS Alarm - PCB Version 0.1 Arrived

AIS Alarm - PCB Version 0.2

 

References and Links:

WEGMATT LLC - dAISy AIS Receiver - low cost AIS receiver

Texas Instruments MSP430FR2xx FRAM Microcontrollers - Post No. 4

TI MSP430FR2111

Maximize the Sound from a Buzzer

  • Sign in to reply

Top Comments

  • gecoz
    gecoz over 8 years ago +3
    Hi Frank, Excellent work. I think your choices paid off, as the board looks very well laid out, and I believe this might well be your AIS v1.0 board candidate . Looking forward to your next update. Fa…
  • genebren
    genebren over 8 years ago +3
    Hi Frank, Everything looks very clean. Your redesign appears to have addressed all of your major issues. Good luck with all the firmware changes and additions. Looks like smooth sailing from here. Gen…
  • three-phase
    three-phase over 8 years ago +2
    This has turned out to be an elegant professional looking design. Well done.
Parents
  • three-phase
    three-phase over 8 years ago

    This has turned out to be an elegant professional looking design. Well done.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 8 years ago

    This has turned out to be an elegant professional looking design. Well done.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fmilburn
    fmilburn over 8 years ago in reply to three-phase

    Thanks Donald.  Making things more polished is my New Years resolution.