Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog Even More on Current Sources and a Kelvin (4-Wire) Milliohm Meter
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 3 Oct 2018 6:27 AM Date Created
  • Views 7673 views
  • Likes 9 likes
  • Comments 51 comments
  • current source
  • milliohm measurement
  • op amps
Related
Recommended

Even More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

fmilburn
fmilburn
3 Oct 2018

Introduction

This is the third post on the development of an inexpensive but reasonably accurate meter for measuring resistance in the milliohm range. In the first post a simple current source was described that created a 10 mA current  across a resistor that allowed the voltage drop to be measured using a multimeter and the resistance calculated.  A number of helpful suggestions were received and I ordered additional components based on that feedback.  In the second post a block diagram for the instrument was introduced and initial measurements were made with a microcontroller using the built-in ADC.  Some, but not all of the ordered parts have been received now and this post will update progress as I don't want John's popcorn to get stale.

 

A Change to the Design Objectives

I originally specified that the current to the DUT would not be greater than 10 mA.  Testing to date has indicated that meeting the desired accuracy will be difficult without amplification of the voltage difference across the DUT which adds some complexity and cost.  Accordingly, the specification is being changed to 100 mA across the DUT.

 

Component Status

First, I have to admit to making a mistake in the orders.  The MCP6N16 instrument amp comes in three versions with different minimum gain.  I wanted the version with minimum gain of 1 and ordered the version that has a minimum gain of 100.  Doh!  Always read the datasheet carefully.  For now I am substituting the MAX9619.  I also ordered a precision LDO voltage source from the TI store which has not been shipped yet.  Usually they are pretty quick. The volt meter I plan to use is still in shipment from China.

 

100 mA Current Source

This is the revised circuit, the only real changes being the addition of a MOSFET to handle the increased current and a new precision 0.1% 10 ohm resistor to set the current.  I am using an inexpensive ANENG multimeter to measure voltage but it does agree well with my bench meter.

image

And here are the results:

image

The tests are being performed the same way as previously using a coil of wire that has been center tapped.  The measured resistance of the full length of wire is 0.092 ohms as seen on top while the measured resistance of half the length is 0.046 ohms - exactly half.

 

Next Steps

The inexpensive voltmeter needs at least 4.5 V to operate so I will probably use either 4 x 1.5 V AAA batteries or USB power and a precision voltage source to set the current.  If I decide to use a microcontroller instead of a voltmeter then a 3V3 LDO will be used to power that.  The parts for Kelvin probes are on order.  Progress depends on the postal service now...

 

Past Posts on this Topic

More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

Testing Current Sources for a Kelvin (4-Wire) Milliohm Meter

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago in reply to shabaz +5
    Hi Shabaz, An update... I read the datasheet thoroughly and set up the LM334 as a temperature compensated current source as described in the datasheet. A IN4148 was substituted for the diode they used…
  • shabaz
    shabaz over 7 years ago in reply to fmilburn +5
    Hi Frank, That's very interesting! Is it figure 15 in the datasheet? There is a modification suggested here: https://www.electronicdesign.com/analog/what-s-all-lm334-stuff-anyhow that looks like it could…
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz +5
    Shabaz,, Yes, using the circuit in Figure 15 with 1% resistors and the diode noted above. I am at the limit of the resolution of my multimeter and there was some bouncing back and forth so am not sure…
Parents
  • fmilburn
    fmilburn over 7 years ago

    This is a summary of experiments with the LM334 Adjustable Current Source as the comments are getting pretty long and possibly difficult to follow.  See the running dialog above for greater detail.  Shabaz has provided links to interesting information on an improved variation of the LM344 circuit and the advantages of using BJT transistors as a PN junction for temperature compensation.  He also ran a very interesting series of experiments to better determine the temperature coefficient of various common transistors as well as the diode recommended in the LM344 datasheet.  The forward voltage was also measured.  My experiments to date are consistent with cruder than his although and I have not run detailed experiments on temperature influence.

     

    Here is a circuit for a milliohm meter, modified using the information above, and using the LM334 to set current.

    image

    The forward voltage drop across the 2N3904 transistor and the values of R1 and R2 in series with R3 are used to set the current through the load.  The tempco of the 2N3904 must also be known in order to properly offset temperature effects from the LM334.  The trimming potentiometer R3 allows error in the measured current to be corrected.  Spreadsheets were developed to make the calculations which are described in the LM334 datasheet easier as shown below:

    image

    My current experimental setup on a breadboard looks like this:

    image

    During the test the following were relatively constant:

    • Input Voltage from Lab Power Supply: 5 V
    • Ambient Temperature: 19 deg C
    • Vf = Vd = 0.7183 V
    • R1 = 17.66 Ohms
    • R2 = 123.54 Ohms (includes trim pot, R3)

     

    The small meter at left is measuring the voltage in millivolts across the DUT which is a 1 ohm 1% resistor.  The larger bench meter behind is measuring current in milliamps.  Since the current is very nearly 10 mA and the voltage drop is very nearly 10 mV the setup is performing properly for a 1 ohm resistor.  The current was remarkably steady over the desired input voltage range of 3 to 6 Volts:

    image

    The test setup was then left to run for one hour exposed to ambient with no observed change in the current.  Tests by Shabaz in the comments above better illustrate the temperature sensitivity.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 7 years ago

    This is a summary of experiments with the LM334 Adjustable Current Source as the comments are getting pretty long and possibly difficult to follow.  See the running dialog above for greater detail.  Shabaz has provided links to interesting information on an improved variation of the LM344 circuit and the advantages of using BJT transistors as a PN junction for temperature compensation.  He also ran a very interesting series of experiments to better determine the temperature coefficient of various common transistors as well as the diode recommended in the LM344 datasheet.  The forward voltage was also measured.  My experiments to date are consistent with cruder than his although and I have not run detailed experiments on temperature influence.

     

    Here is a circuit for a milliohm meter, modified using the information above, and using the LM334 to set current.

    image

    The forward voltage drop across the 2N3904 transistor and the values of R1 and R2 in series with R3 are used to set the current through the load.  The tempco of the 2N3904 must also be known in order to properly offset temperature effects from the LM334.  The trimming potentiometer R3 allows error in the measured current to be corrected.  Spreadsheets were developed to make the calculations which are described in the LM334 datasheet easier as shown below:

    image

    My current experimental setup on a breadboard looks like this:

    image

    During the test the following were relatively constant:

    • Input Voltage from Lab Power Supply: 5 V
    • Ambient Temperature: 19 deg C
    • Vf = Vd = 0.7183 V
    • R1 = 17.66 Ohms
    • R2 = 123.54 Ohms (includes trim pot, R3)

     

    The small meter at left is measuring the voltage in millivolts across the DUT which is a 1 ohm 1% resistor.  The larger bench meter behind is measuring current in milliamps.  Since the current is very nearly 10 mA and the voltage drop is very nearly 10 mV the setup is performing properly for a 1 ohm resistor.  The current was remarkably steady over the desired input voltage range of 3 to 6 Volts:

    image

    The test setup was then left to run for one hour exposed to ambient with no observed change in the current.  Tests by Shabaz in the comments above better illustrate the temperature sensitivity.

    • Cancel
    • Vote Up +3 Vote Down