Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog JFET Static Charge Detector
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 22 Aug 2021 4:02 AM Date Created
  • Views 8142 views
  • Likes 13 likes
  • Comments 9 comments
  • detector
  • electrostatic_discharge
  • jfet
  • static
  • led
  • esd
Related
Recommended

JFET Static Charge Detector

fmilburn
fmilburn
22 Aug 2021

In a recent element14 Essentials on Static Control, shabaz said this:  "A 2N3819 + meter or LED makes a nice simple charge detector too : )"

 

So, I thought I would try it.  I don't have a 2N3819 but I do have a J112 N-channel JFET.  The circuit is shown below:

image

Power is supplied by a bench power supply set to 3V current limited to 10mA.  The "antenna" is a 5-inch long piece of wire.

 

So how does it work?  A JFET has extremely high input impedance - hardly any current flows into the gate - it is voltage controlled.  Current flow from drain to source is determined by the voltage differential between the gate and the source.  The drain to source current flow is highest when the gate to source voltage differential is zero.  As the gate to source voltage differential becomes more negative the drain to source current flow decreases.  At the pinch-off (sometimes called cutoff) voltage the drain to source current essentially ceases.  In the detector circuit, the gate/antenna becomes negative relative to the source and the FET turns the LED off gradually as the statically charged object comes closer.  I demonstrate it in the following 40-second video:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

As one of the resident mechanical engineers who has never seen this demonstrated, I was suitably impressed.  Comments and corrections to my understanding are always welcome image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 5 years ago +4
    Hi Frank, Awesome results! It's definitely a fun experiment too. Great diagram too by the way!!
  • jc2048
    jc2048 over 5 years ago +3
    Good experiment and demonstration. The drain to source current flow is highest when the gate to source voltage differential is zero. Although this is obviously nit-picking, I think you'd find, if you tried…
  • fmilburn
    fmilburn over 5 years ago in reply to jc2048 +3
    Good points and thanks for the comments... I originally used the word "positive" instead of zero. But one of my references stated the gate should not be biased positive so I changed it to zero. Your explanation…
  • fmilburn
    fmilburn over 5 years ago in reply to jc2048

    Good points and thanks for the comments...  I originally used the word "positive" instead of zero.  But one of my references stated the gate should not be biased positive so I changed it to zero.  Your explanation makes the reasoning for doing that and the true behavior clear.

     

    I researched how the gate/antenna works on the internet before writing but most of what I found made no sense and seemed like hand-waving blather.  I couldn't find anything in my textbooks.  Not wanting to add to the misinformation on the internet I made it vague.  In truth, I don't know the physics but it seems more likely that electrons are redistributed in the wire than that they are somehow transferred to the wire.  I like your explanation.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago

    Good experiment and demonstration.

     

    The drain to source current flow is highest when the gate to source voltage differential is zero.

    Although this is obviously nit-picking, I think you'd find, if you tried it, that it would keep increasing as you went above zero. Obviously, at some point, the gate-source diode is going to start to become forward-biased and spoil things by conducting, but you'd probably have a small amount of leeway before that happened.

     

    In the detector circuit, the gate/antenna becomes negative relative to the source...

    That's a bit vague. How does it become negative? Are you claiming that the statically-charged object adds negative charge to the gate/antenna? An alternative hypothesis might be that it causes a redistribution of the free electrons in the wire, so that there's a greater concentration down the gate end.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago in reply to shabaz

    Thanks Shabaz,

     

    I've modified the explanation of how it works to be what I think is more accurate.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago

    Hi Frank,

     

    Awesome results! It's definitely a fun experiment too. Great diagram too by the way!!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<