Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog Microscopes and Solder Masks
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 15 Jul 2018 10:33 PM Date Created
  • Views 2438 views
  • Likes 11 likes
  • Comments 22 comments
  • kicad
  • microscope
  • pcb design
Related
Recommended

Microscopes and Solder Masks

fmilburn
fmilburn
15 Jul 2018

Now that the TI-RSLK robot RoadTest is finished I have turned my attention back to a problem spotted in the last round of PCBs ordered for the AIS alarm project.  But first, I have a new toy.

image

I have been looking for the right used Nikon microscope in budget but finally could not stand it any longer and bought this Chinese model after my friend bought one.  I am amazed at how much better this is than peering through a magnifying glass or loupe.  At low magnification stereoscopic details pops and there is good depth of field.  I bought a version that takes a C-mount camera but don't have a camera yet.  Good value for the money I think but this was a "want" rather than "need" purchase.

 

I went back and put some of my old PCB designs under the microscope and discovered several had a problem I reported in a previous blog - that is, the solder mask did not extend between the pins of smaller SMD packages.  This of course makes solder bridging and the resultant need for rework more likely.

 

I have had the problem occur for two reasons:

  1. The PCB manufactures had a minimum guaranteed spacing specification between the pad and the solder mask.  Check the specification especially with low cost prototyping services.
  2. I use KiCad and the default pad mask clearance is pretty high - so high that there is no mask between some SMD pins.  For KiCad the fix is to go into Dimensions -> Pad Mask Clearance while in pcbnew and change the default to the desired value.  OSHPark has a discussion on the topic and recommends 2 mil (0.05 mm) clearance for 2 layer boards.

 

The MSP430FR2xxx protoboard I put together a while back had the second problem and I did not realize it until I looked under the microscope.  They were made by OSH Park and it is hard to see the problem with the naked eye on that purple background.  Pesky default values....  I have reordered the board with the fix since they are inexpensive and I have another project in mind for that particular microcontroller.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +6
    Hi Frank, That looks like a nice piece of equipment : ) 2mil sound good, or maybe a tiny bit higher may be preferable if you also plan to use prototyping services in China. If you look at the fourth photo…
  • rachaelp
    rachaelp over 7 years ago +6
    Hi Frank, I'd been looking at various microscopes for quite a while, hoping to find a bargain used one from a high end manufacturer. In the end I did the same as you and went for one of the Chinese ones…
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz +5
    Hi Shabaz, RE equipment - I plan to take the grandkids and go looking for bugs and small stuff in the garden next week :-) Thanks for the tips and the helpful link - I will go back and read that carefully…
Parents
  • Fred27
    Fred27 over 7 years ago

    Nice microscope. I've got the same one. I got mine with a camera included but it captures a much smaller area than you can see through the eyepiece. I intended to sort out something better but haven't managed to yet. Tried a DSLR C mount adapter without success.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Fred27
    Fred27 over 7 years ago

    Nice microscope. I've got the same one. I got mine with a camera included but it captures a much smaller area than you can see through the eyepiece. I intended to sort out something better but haven't managed to yet. Tried a DSLR C mount adapter without success.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fmilburn
    fmilburn over 7 years ago in reply to Fred27

    Fred27  wrote:

     

    Nice microscope. I've got the same one. I got mine with a camera included but it captures a much smaller area than you can see through the eyepiece. I intended to sort out something better but haven't managed to yet. Tried a DSLR C mount adapter without success.

    Hi David,

    Thanks for the comment.  I was planning to try a C mount adapter for my DSLR.   Can you describe more  the issues you had with it? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to fmilburn

    As far as I remember it was impossible to get the focus even close to being right. It got thrown in a box and I've not tried anything else as it wasn't really a priority. It was a cheap one from eBay so other adapters may be better.

     

     

    For anyone getting one of these I can recommend also getting a 2x barlow lens. When I got mine the two pack of barlow lenses was a good deal. The 0.5x is ideal for soldering and general electronic work, but the 2x is even better if the kids want to be grossed out by a spider, etc. You might as well get more use out of it!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to Fred27

    Mine came with a 2x as well as the 0.5x.  I tried the 2x for the first time last night and as you say it will be great for the kids and may come in handy for some electronic stuff.  The distance to the stage really shrinks and it is no longer possible to easily work under it.  The depth of field is also greatly diminished of course.  Fun stuff....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to Fred27

    The first accessory that I bought for my microscope was a barlow lens (0.5x).  It cost almost as much as my microscope, but it was really worth it.  The increase in working distance was so necessary, as it made it less cramped working under the scope.  The second accessory (built not bought) was a light ring.  Again, what a difference!  The bright and direct light is so useful as in makes everything pop and reduces shadows.

     

    But, I guess these are things that you get when you buy a new Chinese scope.

    Enjoy!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 7 years ago in reply to Fred27

    It would be interesting to know if you manage to get it working at some point. Adding a DSLR body with a C-mount adapter is one option I was considering because a second hand body from eBay plus the adapter is way cheaper than it appears equivalently specced C-mount cameras cost (Here is an Amscope one on Amazon: https://www.amazon.co.uk/AmScope-USB3-0-C-mount-Microscope-Calibration/dp/B072833HKR/ref=sr_1_fkmr0_1?ie=UTF8&qid=153177…  which maybe you can get cheaper elsewhere but it's probably in the ballpark). Amscope do sell adapters specific to their equipment so maybe this has a specific length which enables it to work. I know they are also 2x lenses so maybe that's a factor if the cheap ones aren't actually lenses just adapters.

     

    Here is the Amscope video on using a DSLR with their microscopes using their adapter: https://www.youtube.com/watch?v=pzpHh1PQAEM

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down