Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog Microscopes and Solder Masks
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 15 Jul 2018 10:33 PM Date Created
  • Views 2997 views
  • Likes 11 likes
  • Comments 22 comments
  • kicad
  • microscope
  • pcb design
Related
Recommended

Microscopes and Solder Masks

fmilburn
fmilburn
15 Jul 2018

Now that the TI-RSLK robot RoadTest is finished I have turned my attention back to a problem spotted in the last round of PCBs ordered for the AIS alarm project.  But first, I have a new toy.

image

I have been looking for the right used Nikon microscope in budget but finally could not stand it any longer and bought this Chinese model after my friend bought one.  I am amazed at how much better this is than peering through a magnifying glass or loupe.  At low magnification stereoscopic details pops and there is good depth of field.  I bought a version that takes a C-mount camera but don't have a camera yet.  Good value for the money I think but this was a "want" rather than "need" purchase.

 

I went back and put some of my old PCB designs under the microscope and discovered several had a problem I reported in a previous blog - that is, the solder mask did not extend between the pins of smaller SMD packages.  This of course makes solder bridging and the resultant need for rework more likely.

 

I have had the problem occur for two reasons:

  1. The PCB manufactures had a minimum guaranteed spacing specification between the pad and the solder mask.  Check the specification especially with low cost prototyping services.
  2. I use KiCad and the default pad mask clearance is pretty high - so high that there is no mask between some SMD pins.  For KiCad the fix is to go into Dimensions -> Pad Mask Clearance while in pcbnew and change the default to the desired value.  OSHPark has a discussion on the topic and recommends 2 mil (0.05 mm) clearance for 2 layer boards.

 

The MSP430FR2xxx protoboard I put together a while back had the second problem and I did not realize it until I looked under the microscope.  They were made by OSH Park and it is hard to see the problem with the naked eye on that purple background.  Pesky default values....  I have reordered the board with the fix since they are inexpensive and I have another project in mind for that particular microcontroller.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +6
    Hi Frank, That looks like a nice piece of equipment : ) 2mil sound good, or maybe a tiny bit higher may be preferable if you also plan to use prototyping services in China. If you look at the fourth photo…
  • rachaelp
    rachaelp over 8 years ago +6
    Hi Frank, I'd been looking at various microscopes for quite a while, hoping to find a bargain used one from a high end manufacturer. In the end I did the same as you and went for one of the Chinese ones…
  • fmilburn
    fmilburn over 8 years ago in reply to shabaz +5
    Hi Shabaz, RE equipment - I plan to take the grandkids and go looking for bugs and small stuff in the garden next week :-) Thanks for the tips and the helpful link - I will go back and read that carefully…
Parents
  • Fred27
    Fred27 over 8 years ago

    Getting back to your original question, I think it's normal not to try putting soldermask between SMD pins of such a small pitch. That board looks fairly normal to me.

     

    I can't remember where I read it, but I'm fairly sure the recommendation is not to try mask between the pins as it tends to flake off. Any misalignment may also mean you could get soldermask on the pads. (I'm thinking of 0.5mm or 0.4mm pitch LQFP and QFN packages here)

     

    I'm now going to go search and see if I can find more info. If anyone else beats me to it feel free to correct me.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 8 years ago in reply to Fred27

    Very interesting conversation.  I have an order in on the board photographed above which will meet OSH Park specs and has soldermask between pins.  It is a small sample from one manufacturer so I won’t learn anything about variability but I will be checking from now on.  I also want to see how much difference it makes in reducing rework. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 8 years ago in reply to Fred27

    Very interesting conversation.  I have an order in on the board photographed above which will meet OSH Park specs and has soldermask between pins.  It is a small sample from one manufacturer so I won’t learn anything about variability but I will be checking from now on.  I also want to see how much difference it makes in reducing rework.