Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog New Improved DIY Milliohm Meter V2.0
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 21 Sep 2020 6:44 AM Date Created
  • Views 16239 views
  • Likes 11 likes
  • Comments 17 comments
  • kelvin measurement
  • 4-wire resistance measurements
  • 4-wire measurement
  • kelvin
  • milliohm
  • milliohm meter
Related
Recommended

New Improved DIY Milliohm Meter V2.0

fmilburn
fmilburn
21 Sep 2020

The milliohm meter has been one of the most popular projects I've posted on element14 judged by views, comments, and stated interest.  Thanks to a modification by shabaz (documented way down in the comments here) and much help over time it appears to have reached or is very close to the design objectives:

  • Low cost
  • Dual range covering from 1 milliohm to 40 ohms
  • Choice of power source - USB or batteries
  • Kelvin (4-wire) probes
  • Low current (1 to 10 mA) through the Device Under Test (DUT)
  • Provision for "out of range" indication
  • 1 milliohm accuracy down to 1 milliohm

 

The current Version 1.3 PCB requires bodging in some parts and the documentation, posted over many blogs with endless comments, is difficult to follow.  So I've set a goal to clean it up and post a new version before yearend.  I'd also like to add some features like microcontroller auto-ranging and output, otherwise known as unnecessary wishes and feature creep.  But before adding the feature creep there will be an interim step documented here.

 

Schematic

 

The revised schematic has these features:

  • Added resistors R29 and R30 to remove the intermittent instability that occurred when measuring resistance below 20 milliohms or so
  • Took out diodes D1 and D2 which did not seem to help
  • Moved the connections on the PCB for probes and the User Interface to a single 14 x 2 header

 

The revised Version 2.0 schematic is shown below:

image

One thing I'd like thoughts on is the addition of input protection as there is none currently.  There is not much headroom with the lower limit of USB voltage and the 4.7 V LDO voltage regulator.  There is an alternate source of voltage (labelled battery input - it could be anything) that could be hooked up backwards by the user or power applied with the USB source simultaneously.  Is it worth dropping USB and designing for a higher voltage (could be USB-C or just a jack) with more input protection?

 

Enclosure

 

One of the concessions I will make to accommodate feature creep is a larger enclosure and PCB.  The enclosure selected is the 5.287" L x 5.323" W (134.29mm x 135.20mm) X 2.008" (51.00mm) Hammond 1598BHammond 1598B.  There are PCB standoffs on Eurocard centers so the PCB may well fit other enclosures of a similar size.  It can be purchased with brushed aluminum or plastic end panels.  The slots for the end panels will also take a PCB.  Of course 3D printed end panels will also work.

image

credit:  Hammond Manufacturing

 

PCB

 

The new layout and design decisions are described below.

image

The noisy stuff and future digital stuff is on the bottom and analog is on top.  Power input and regulation is lower left.  All tracks in and out of the power section are widely separated with ground in between tracks and a clean ground plane beneath.  The constant current section is located just above it.  The ICs are spaced out in order minimize temperature influence.  The panel behind the constant current section and the power section could be vented.

 

The amplification of the differential signal from the Kelvin sensing clamps attached to the device under test are upper center.  I am curious about thoughts on the spacing of the feedback resistors and the trimmer pots.

 

All connections to Kelvin clamps, panel meter, and other user interfaces are on the 28 pin header to the far right.  A comparator to determine when the instrument goes out of range is sandwiched between it and the amplification.  In future it would be replaced an ADC for the microcontroller located bottom right.  A separate ground plane with star connection could be set up for the digital section.

 

Front view with silk screen:

image

Back View with Silk Screen:

image

All Tracks and Pads:

image

Front Copper

image

Back Copper:

image

 

Conclusion:

 

I plan to send off for a new set of PCBs by mid-week and given that it works will then start working on Version 3.0.  All thoughts and suggestions are appreciated.  And if anyone is interested in building one and has an idea let me know.  KiCad files are available as well.

 

 

  • Sign in to reply

Top Comments

  • Andrew J
    Andrew J over 6 years ago in reply to fmilburn +4
    I Concur. It’s now as cheap, if not cheaper, to get a PCB created than use prototyping board. Even 4-layer PCBs are pretty cheap. Definitely worth taking the time to learn how to use Kicad or Eagle.
  • shabaz
    shabaz over 6 years ago +3
    Hi Frank, That looks nice! The different areas on the board (power, current source, amplifier, processor) make it easy for people to tweak and enhance the design I think. Also, it seems a great idea to…
  • genebren
    genebren over 6 years ago +3
    Looking very good! If you are talking about batteries and battery indicator, why not consider a Li-ion solution with a built in recharging circuit. I have a clean little charger/boost circuit that you…
  • fmilburn
    fmilburn over 6 years ago in reply to dubbie

    Hi Dubbie,

     

    Having a PCB manufactured is so inexpensive these days, plus reasonably quick turnaround, that it is definitely worth investigating.  The only issues I had was learning the software quirks and of course good PCB design regardless of the software which I am still working on.

     

    Frank

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago

    Frank,

     

    A nice PCB. One dayt, probably in the far distant future, I too will be able to make PCBs like this.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to fmilburn

    Hi Frank,

     

    I'm wondering if maybe the supply might need to be 3.3V for the SDA/SCL lines to the microcontroller (unless it is tolerant but I've not checked). Nice idea to try the XMC board, it's really fun developing for that chip. Incidentally by accident I discovered during experimentation for the Pocket-Nim game Creating your own Handheld Electronic Games – Pocket Nim that that XMC board consumes a lot of power due to the debugger. (Not normally an issue since that board is designed for USB use, but is a problem for battery operation). However the debugger can be disabled, but needs a wire soldered to one of the pads on the edge (described at that Pocket NIM blog post).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago

    I've added a new sheet to the schematic above with an ADC and microcontroller:

    image

    Below is the revised board:

     

    image

    I'm currently doing a RoadTest that came with two Infineon XMC 2Go boards and I decided to use one for this experimental version of the Milliohm Meter.  I have been looking for a small and inexpensive ARM chip to replace the MSP430 that I have mostly using up until now and the XMC 2Go has a M0 ARM microcontroller and is tiny enough to fit on the PCB and inside the enclosure.  I haven't made a decision on the microcontroller but any microcontroller could work and I can use flying leads if needed.

     

    The ADC to the right of it is the MCP3421 which is the same ADC in the little voltage meter that Shabaz recommended and works so well.

     

    I tried putting in a more general prototyping area but KiCad was giving me problems this evening.  For a change, I think it might be KiCad and not me and noticed I am using quite an old version so will update.  I fully plan to spin another board and this should be good enough to validate the changes made so far.  If the microcontroller and ADC work then can add reed switches? to auto-range, a new display, and power management.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to Andrew J

    Thanks Andrew.  I will keep batteries and MCU in mind.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>