Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog NSA1166 7-Segment 6-Digit Bubble Displays
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 21 Oct 2021 6:23 AM Date Created
  • Views 4145 views
  • Likes 0 likes
  • Comments 5 comments
  • led display
  • nsa1166
  • 7-segment
  • bubble display
  • display
  • arduino
Related
Recommended

NSA1166 7-Segment 6-Digit Bubble Displays

fmilburn
fmilburn
21 Oct 2021

Jameco has these National Semiconductor NSA1166 7-segment 6-digit bubble displays and I bought a couple to distract me from what I should be doing.

image

 

They are very simple to drive as each segment has its own pin that is driven high and each digit has a pin to act as the cathode.  I plan to write my own driver but like everything these days, there is an Arduino library that I am using at the moment.  It might make an interesting display for use with my milliohm meter project which is waiting patiently for me to return.

 

I tested one with my bench multimeter current limited to 3mA to start to make sure I knew which pins were which and then set it up with an Arduino MKR1010 and the SevSegPlus library.

image

 

It works!  Behold the mighty '70s technology!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
Parents
  • javagoza
    javagoza over 5 years ago

    Thanks for sharing.

    For some reason the links don't work. When redirecting, jive ignores the ":" that should follow "https".

     

    NSA1166: National Semiconductor : LED Display 7-Segment Red 0.10 Inch 6-Digit 1.65V 5mA 2 Inch Long : Opto & Illumination (jameco.com)

     

    8bitkick/SevSegPlus: Improved Arduino seven segment LED display library for NSA1166 (github.com)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago in reply to javagoza

    Thanks - Jive doesn't like the way I copy/paste.  Fixed, I think :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 5 years ago in reply to javagoza

    Thanks - Jive doesn't like the way I copy/paste.  Fixed, I think :-)