Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog ToorCamp
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 25 Jun 2018 11:18 PM Date Created
  • Views 1139 views
  • Likes 9 likes
  • Comments 8 comments
  • toorcamp
Related
Recommended

ToorCamp

fmilburn
fmilburn
25 Jun 2018

I was able to attend an interesting "hacker" camp last week and thought it worth a post.  ToorCamp is advertised as "The Five Day, Open Air, Tech Camping Event where you create more than just ideas and build more than just inventions".  I don't think that is a particularly good description but I really enjoyed it.   It is located in the Orcas Islands which are located between Washington state in the U.S. and British Columbia in Canada, a very beautiful location.

 

Around 500 people attended.  We had a cabin but most people stayed in tents.  Here is the view from our cabin which was located above the main venue and had a peekaboo view of the bay through the trees.

image

 

I set up my AIS alarm and also a battery powered Raspberry Pi based AIS I have been working on running on the small screen at left.  The small screen is the official 7" model which I obtained from Newark after winning an element14 contest - Thanks element14!

 

I also put together a decoration for the cabin.  I obtained the mask sometime back while working in Papua New Guinea.  It was made for the tourist trade and no cultural artifacts of significance were damaged.  It normally occupies a place of honor in a covered area of my garden and I wanted to return it unharmed so nothing was permanently attached.  I used one of my MSP430 "wearable" boards for the controller and a PIR sensor to detect movement.  When movement is detected it lights up the WS2812 LEDs behind the eyes and mouth and runs a little sequence.  Construction incorporated hot glue, popsicle sticks and paper for diffusing.

image

There was a software silly hacks contest which was pretty good.  My favorite was a web app which automatically created code. It worked by typing a line of code in and hitting enter.  It would then go to github and find that line or something similar and fill in a complete program.  Perfect for the lazy programmer.

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +2
    Frank, Sounds like a great time. Did you get to wow some people with your AIS alarm? Gene
  • fmilburn
    fmilburn over 8 years ago in reply to genebren +2
    There was some interest but besides being a poor salesman I would guess most of the attendees were security related people and the alarm doesn't have anything to hack over the internet or break into and…
  • genebren
    genebren over 8 years ago in reply to fmilburn +2
    Frank, I too am a poor salesman, but sometimes that does not bother me too much. Gene
  • genebren
    genebren over 8 years ago in reply to fmilburn

    Frank,

     

    I too am a poor salesman, but sometimes that does not bother me too much.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 8 years ago in reply to genebren

    There was some interest but besides being a poor salesman I would guess most of the attendees were security related people and the alarm doesn't have anything to hack over the internet or break into and do mischief with :-).  As well, there were flame throwers, drones delivering tacos, and high voltage demonstrations which are hard to compete with.

     

    I did get a suggestion that I filter out the AIS shore stations and beacons which I plan to incorporate.  They have long range and of course aren't moving.  Both the firmware and hardware were stable and there was a fair amount of marine traffic in the area.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago

    Frank,

     

    Sounds like a great time.  Did you get to wow some people with your AIS alarm?

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<