Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gene Breniman's Blog Colorcoding Wires
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 24 Jun 2019 8:40 PM Date Created
  • Views 2494 views
  • Likes 14 likes
  • Comments 20 comments
Related
Recommended

Colorcoding Wires

genebren
genebren
24 Jun 2019

(Updated 7/15/2019 - See Below)

 

During my roadtest of the PicoScope 5444D MSO, one of the disappointments that I had was with the quality of the supplied Digital Probes.  Here are my comments from the review:

 

  • The quality of the probes felt a little cheap for this nice of a scope.  The plastic felt very cheap and brittle, while the probes did not operate smoothly (very sticky and sometimes refusing to slide at all).
  • The marking on the probe tip connectors were somewhat difficult to read, which along with the strange mapping made it quite difficult to attach the probes to the board under test.  Placing the marking on multiple sides of the connector and/or using color-coded wiring (or connector shells) would have made this a lot clearer.

 

In an attempt to address these concerns, I starting looking around and I even posted a question to the community (Wire/Cable Markers ).  After a while, I just decided to order the markers (https://www.element14.com/community/external-link.jspa?url=https%3A%2F%2Fwww.newark.com%2Fhellermanntyton%2Fw1-270%2Fcab… ) and give them a try. They were a little loose for the gauge of the wires on these probes, but a bit of heat shrink and here they are:

 

imageimage

The marker clips are a little too wide to allow me to attach wires side-by-side to a 0.1" header, but at least I can more quickly identify the leads, by either the color coding of the markers or by the slightly larger font.  Also, I found a bunch of grabbers from an old HP logic analyzer (that I still have not unpacked from my move of almost 3 years ago).  The combination of markers and clips should help make these probes a little more usable.

 

After working with this modification, I noticed that the clip on markers moved a little to freely and the thickness of the markers made in difficult to have probes placed on adjacent pins of a header.  This got me thinking if maybe there was a better solution.  While shopping on element14 to claim my project14 winnings, I started looking for colored heatshrink (1/16 ") that I could use to mark my wires, but I was unable to find the 10 colors necessary (this might make a nice assortment/kit).  I ended up just ordering some clear heatshrink with the thought of using it over colored tape/labels.

 

I designed some labels that contained the probe number along with a standard 'resistor' color coding stripes (as I could not print white, I used a dashed line (clear/black) for '9').  I went with stripes on either side of the probe numbers, with the outermost stipes being the '10s' field (either black or brown for probe numbers 0-15). These labels were then printed onto clear labels (return address style) with my color laser printer.  Here is a sample of labels and finished probes.

imageimage

The colors did not come out as nice as I would have liked (D8 - the gray is almost black and some color were not vivid enough or smeared), the labels did make it considerably easy to locate a specific probe as I added probes to a debug connector on a board I was testing.  These will work for now, bit I still might come back to this design to see if I can improve on it.

 

Gene

 

Update - 7/15/2019 -

Not too long after posting this blog entry jw0752 (Thanks John!) had suggested using multi-color heatshrink tubing to mark the wire numbers.  I immediately searched on Ebay and found the 10 colors (resistor color codes) available in 1/16".  I had been a little busy, but ran into some time today and decided to try it out.  Here are the results:

 

image

Using the standard resistor code colors, I used two pieces of heatstrink per wire.  The first piece, represents the 10's place, I used black (0) or brown (1), using 0.3" of 1/16" heatshrink tubing.  For the second piece, representing the 1's place, I used the remaining colors, using 0.1" of 1.16" heatshrink tubing which I centered over the first piece.  For D0 (black/black) and D11 (brown/brown) I left off the second marker.  (Note: the heatshrink supplier sort of cheated on the green and blue tubes as these were actually small diameter, fortunately I had also ordered some other sizes of these multi-color heatshrink (1/8" and 3/16" diameters) so I was able to substitute the 1/8" diameter for the second piece).  The results are far more readable and I am quite happy with the readability of the leads.

 

In applying the heatshrink, I did run into a couple of problems, due to the distortion that I had cause on the black molex connector housings.  In my last attempt to use labels and clear heatshrink, I reattached the housing prior to shrinking the plastic and I messed up a few of the plastic housing.  The D2, D6 and D8 housing were so distorted that I had a very difficult time extracting the wires from the housing so that I could slip on the heatstrink pieces.  I need to use some very solid tweezers to 'tweak' the housing openings enough to slip out the contacts.  This time to prevent further damage to the housings I shrunk the tubing with the housings off.

 

In shrinking the tubing (before and presently) I used https://www.newark.com/nte-electronics/hg-300d/input-power-350w/dp/80R3536?st=heat%20gun   that I received from Newark using one of my $100 carts from project14 prizes (Thanks element14!).  I am super happy with the performance of this heat gun, once I stopped and read the directions to better understand the two heat ranges.  This tool has found a well deserved spot on my workbench.

 

Thanks for reading!

Gene

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 7 years ago in reply to genebren +6
    Hi Gene, Along with labels, heat shrink ranks right up there as one of my obsessions. I buy it whenever I see a deal or a good looking assortment. For the fun of it I just checked to see if I could cover…
  • genebren
    genebren over 7 years ago in reply to jw0752 +5
    John, I will have to try looking for other heatshrink vendors/distributors. You would think that resistor-like color coding would be a pretty normal usage of heatstrink. Thanks for the kind words, Gen…
  • jw0752
    jw0752 over 7 years ago +4
    Hi Gene, I like your process for working towards a solution to this need. I too have looked for the proper colored heat shrink so that it could be used for color coding numbers using the standard resistor…
  • jw0752
    jw0752 over 7 years ago in reply to genebren

    Hi Gene,

    Along with labels, heat shrink ranks right up there as one of my obsessions. I buy it whenever I see a deal or a good looking assortment. For the fun of it I just checked to see if I could cover the 10 colors. It seems that the only one I am missing is Orange.

     

    image

     

    Unfortunately this is 1/16th and I can't do it in all sizes. If I had to give a vendor I would have to point to E-Bay and the plethora of Chinese vendors.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to jw0752

    John,

     

    I will have to try looking for other heatshrink vendors/distributors.  You would think that resistor-like color coding would be a pretty normal usage of heatstrink.

     

    Thanks for the kind words,

    Gene

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to three-phase

    Donald,

     

    The color was smearing as I was cutting down the label and wrapping it around the wire.  (I don't believe that there was any glue on the heatshrink, but this is something that I might have to look into)  Although the labels are listed as 'Laser Printer', they might have been a little old or improperly stored (I found this sheet inside one of my other packages as a single sheet.  If I try it again, I might try white labels (with a less plastic feel) as it might hold the color better), plus that would also solve the issue with not being able to print white stripes.

     

    Thanks,

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago

    This is a nice tidy solution. Did the heat shrink have a glue inside? I remember when I have covered laser printed labels with clear sheet in the past, there has been a reaction between the covering and the print that has faded / smeared it.

     

    Kind regards.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago

    Hi Gene,

     

    I like your process for working towards a solution to this need. I too have looked for the proper colored heat shrink so that it could be used for color coding numbers using the standard resistor number correlation. Thanks for posting your quest.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<