Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gene Breniman's Blog Programmable DC Load connection adapter.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 14 Jul 2022 7:44 PM Date Created
  • Views 2659 views
  • Likes 10 likes
  • Comments 12 comments
  • Programmable DC load
  • 3D Printing
Related
Recommended

Programmable DC Load connection adapter.

genebren
genebren
14 Jul 2022

When I first acquired my BK PRECISION 8500 (used on eBay), I was a little disappointed with the screw knobs that secured the leads to the device being loaded.  I had hoped that the screws were cross drilled so that I could easily connect stripped wire through the threaded lugs (sure, I could just wrap the wire around the lugs and tighten the screw knobs).  I ended up using some U-type crimp lugs which were suitable for my uses.  Recently while purchasing some Banana-to-Banana leads I started thinking about how I might be able to mount some banana jacks to the front of the Programmable DC Load.  My first ideal was a U-type crimp attached to a solid copper wire (10 gauge) with a banana jack attached to the other end.  While this might have been a fairly simple hack, I was not completely sold on this as a solution.

This brings me to my Maximum Overkill solution which I sharing with you today.  I found some copper bar (0.1875" x 0.75" x 12") in my scrap material collection and cut off a couple of 2" sections.  I then drilled to 15/64" (0.234375" or slightly under 6mm) holes, 1/2" front each end and centered in bar. I then filed/sanded the bar smooth and rounded the corners.

imageimageimageimage

The Banana Jacks in the image are CT2224 from CAL TEST ELECTRONICS.  I had these parts left over from some work that I did on custom building some Synthesizer modules for a client (passed the jacks through an insulated sleeve through an aluminum panel and fitted to the PCB with a 6mm through hole).  Here are some shots of the adapters installed to the from the Programmable DC Load.

imageimageimageimage

As I started test fitting the adapters, I became a little concerned about the copper bars shorting out, so I went to work on an insulator/spacer that I could 3D print.  After a bit of work, this is what I came up, a two part cover that could be secured with a 2/56 screw between the two copper bars.

image

The upper piece goes on first (rectangular through hole for the copper bars), then the banana jacks are installed and then the lower piece slips over the bottom stubs of the copper bars. A 1 1/4" 2/56 screw is used to secure the top and bottom halves of the cover together with the two semi-circles surrounding the hex nuts of the banana jacks, keeping the cover in place.

After a couple hours of printing, here are the final results:

imageimageimageimage

Overall, I am very happy with the results.  I might reprint the upper half of the cover, lowering the overall height of that piece.  The screw knobs rubbing/interfering with the top of the cover.  Dropping the height of this piece by 1/4" would be a big improvement (I might also want to make the back of the upper cover a bit thinner as it is tight up against the rubber bezel bumper).

For now I'll call it a day.

  • Sign in to reply
Parents
  • genebren
    genebren over 4 years ago

    Now don't get me wrong, as I really like the solution that I came up with, but this weekend as I was looking for some dip clips that I could hack up for another project, I found this collection of parts (Notice the big beefy banana jack to lug adapters to the left in the first image, closeup of these in the second image):

    imageimage

    The spade lug to Banana Jack is the functional equivalent to the Banana Jack adapters that I built.  Looking up the specifications for these beauties (Pamona Electronics 1614), shows that they have been replaced by a much lighter weight product (1614A - thinner, stamped metal), but currently rated at 15A.  I am sure that these big guys would be rated well above 15A. I don't remember where or when I got these, but I am sure that they came off of Ebay, where I did a lot of shopping to build up by test equipment and prototype part stock. (I found one site with some NOS parts and these were asking $60+ dollars apiece for these.)

    These would have worked just fine, but at least I had a fun project!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to genebren

    Nice selection of parts!

    I've been using these on my BK E-load:

    https://uk.farnell.com/gustav-klauke/2-r6/crimp-terminal-lug-2-r6-pk10/dp/3348490?CMP=i-ddd7-00001003

    they are pretty good too, I can't fault them, but needs the appropriate crimper (it's a fairly popular shape, but not as popular as the insulated terminals one).

    They are cylindrical/closed-barrel without a seam, so it needs the crimper that pushes in from one side to make a kind of U shape with an indent.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 4 years ago in reply to shabaz

    Those are nice lugs.  Too bad the ID on the crimp region is 4.5mm, which would be a loose fit for a banana plug.  I guess I could try the 1/R6 and drill the ID (3.5mm) out to 4mm .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 4 years ago in reply to shabaz

    Those are nice lugs.  Too bad the ID on the crimp region is 4.5mm, which would be a loose fit for a banana plug.  I guess I could try the 1/R6 and drill the ID (3.5mm) out to 4mm .