Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gene Breniman's Blog X-Acto Knife upgrade
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 16 Jan 2024 8:57 PM Date Created
  • Views 2223 views
  • Likes 13 likes
  • Comments 16 comments
  • X-Acto
  • wood turning
Related
Recommended

X-Acto Knife upgrade

genebren
genebren
16 Jan 2024

Freezing weather has forced a stop on my backyard fountain project, which happens to be a part of my Roadtest of the Keysight E36731A Battery Emulator.  I have been working on firmware for my controller boards for the project, but a last minute change has also forced a stop as I wait for new PCBs.

All these stops in turn led me into cleaning up my office space.  In the process, I came across one of less than functional X-Acto knives.

image

This is a picture of a good knife.  Unfortuately, I failed to take a picture of the broken one.  What happed with my knife is that overtightening of the blade holder broke the plastic sleeve. I had initially thought that there was a very chance that I would have a suitably size brass tube that I could use for a replacement for the broken black sleeve.  Look as I might, I was only able to find a short section of tubing with the correct inside diameter, so I decided to see if there was another approach.  It didn't take too long to come up with another solution.  I went down to my (cold) shop and looked around for a suitably scrap of wood.  Finding a nice piece of maple, I proceeded to rough cut it to shape, leaving me with a 3/4" x 3/4" x 5" rectangle.  I then drilled a 3/16" hole through the wood (entering both ends of the block with a 3/16" drill and a self-centering hole guide). Once I was able to have a through hole, I enlarged it to 1/4".  I then mounted the block into a 4-jaw chuck of my metal lath and held the other end of the block with a live center (finding neatly into the 1/4" hole).  I then proceeded to turn the piece down with a very light taper (0.45" at the blade end and 0.55" at the knurled tightener end).  A little cutting and sanding and I was ready to fit it all together.

image

imageimage

When it warms up a bit I will stain and finish the handle, but so far, I am pretty happy with the look and feel.

Thanks for reading along,

Gene

  • Sign in to reply
Parents
  • shabaz
    shabaz over 2 years ago

    That looks better than the plastic version!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 2 years ago in reply to shabaz

    It also has a much better hand feel too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 2 years ago in reply to shabaz

    It also has a much better hand feel too.