Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gough Lui's Blog A Modern Digital Etch-a-Sketch
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 11 Jan 2020 8:31 AM Date Created
  • Views 6821 views
  • Likes 15 likes
  • Comments 18 comments
  • RoadTest
  • bk
  • kids
  • b_and_k_precision
  • chart recorder
  • b&k
  • heart
  • etch
  • data acquisition system
  • etch-a-sketch
  • sefram
  • das240-bat
  • recorder
  • b&k precision
  • data acquisition
  • multi_channel
  • bk precision
  • holidayspecial19ch
  • data_acquisition_systems
  • b&k_precision
  • presents
  • project14
  • art
  • bk_precision
  • multi-channel
  • toy
  • data_acquisition
  • das240
Related
Recommended

A Modern Digital Etch-a-Sketch

Gough Lui
Gough Lui
11 Jan 2020
image

Holiday Special 19

Enter Your Holiday Season Project for a Chance to Win Over $20,000 Worth of Prizes and Gifts to Give!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

When I posted my projects for the RF Project 14 in November, I mentioned that things might get busy, meaning I would not have much of a chance to post more projects. Well guess what? I was right! The Christmas-New Year period was exceedingly busy as I blogged on my own personal blog and tried to finish a few different projects that I have always wanted to do. Seeing that the Holiday Special Project14 deadline is coming up, I thought I'd do my best to cobble together a short project.

 

When I think of holiday periods, I think of gifts. When I was a child, one of the toys that people would play with is an Etch-a-Sketch - a board with some magnetic material that turns dark on the action of the magnet, which is suspended by cords along two axes with two controls on the front that control the X and Y axis motions independently. Using this, one could draw some rather simple images without needing paper, or pens. I never had an Etch-a-Sketch as a child, but then again, I was never really artistic anyway.

 

But then, just as the holiday season approached, I got news that I was awarded the B&K Precision / Sefram DAS240-BAT RoadTest review. Just two days before new year, the unit arrived, which got me thinking ... could this become an expensive modern digital Etch-a-Sketch? The answer was yes!

 

Building the System

Lucky for me, the DAS240-BAT supports direct measurement of resistance as it has an internal bias generator and the unit is capable of plotting in X-Y mode. All I have to do is supply the resistance.

image

Rummaging in my junk box, I found two new 500-ohm linear carbon-track long-stem potentiometers. I soldered a wire to one end of the track and the wiper and covered the connection in heatshrink. I then wired it to the input pluggable terminal block with the resistance across the +/- connections and the bias tied into the negative side as instructed by the manual.

image

I twisted the wires for some noise suppression, while plugging it into the 20-channel input module. Using some Blu-Tack, I stuck the potentiometers down to the table so they could be manipulated safely and then grabbed the camera.

 

In Action

I'm not much of an artist, nor have I used an Etch-a-Sketch before, but I tried my best to do a project with heart, by literally drawing a heart. Then I decided to try and draw my name ... I guess I don't have much finesse when it comes to turning pots ... as you'll see in the video

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

But I suppose it could be improved if I had used higher-quality 10-turn potentiometers as the 270-degree range of these pots combined with the mechanical backlash means that it's hard to get it to move precisely. The same sort of set-up can be used with a voltage source and infinite persistence in X-Y mode to do the same thing on an oscilloscope.

 

Conclusion

It's portable, it has an X and Y control and it draws an image. But it's not an Etch-a-Sketch ... it's a sophisticated, expensive piece of test equipment being tested in a rather whimsical manner. It's a pretty expensive way to get Etch-a-Sketch-style functionality, but it does work and it took all of about an hour to complete (from ideation through to uploading the blog and video). A project with heart? Maybe. A holiday project? Definitely.

 

It's also a bit of an experiment of mixing a Project14 with a RoadTest - within the next month or so, the full RoadTest review for the B&K Precision / Sefram DAS240-BAT should be complete and published, so I hope you look out for it as there's been a lot of interesting findings to say the least.

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 6 years ago +7
    Hi Gough, What a fun project; a heart is a very tricky shape for just X and Y input. I'm sure you can also print the output (which the original Etch-a-Sketch could not). It makes me now think of two things…
  • Gough Lui
    Gough Lui over 6 years ago in reply to beacon_dave +5
    Well, if I was doing that, I might as well get myself a two-channel arb waveform generator and draw everything with vectors ... but I think that's cheating . I could do it (slowly) with the multi-channel…
  • beacon_dave
    beacon_dave over 6 years ago in reply to Gough Lui +5
    yes, (drum roll) it's a 'fine line' (cymbal clash) I seem to recall several attempts with stepper motors attached to real Etch-a-Sketch tablets, and I think one even was connected up to a R-Pi camera so…
  • genebren
    genebren over 6 years ago

    Interesting project!  Back in the early 90's, while I was on a period of unemployment, I was very interested in attempting a project built around a Nintendo GameBoy.  I found a game developer that had an unused development system for the GameBoy that I was able to borrow.  I was interested in building a graphical interface that was not sprite based (the device did not have a true X/Y mapped interface to the LCD), so as an example of drawing line segments (hopefully waveforms) I attempted to build an Etch-a-Sketch.  I was able to prove that it was possible to draw multiple spaces, including free form sketches to LCD.  My son and his friends were so excited, being able to play around with a home-brewed GameBoy game (think Super Hero Dad!). Unfortunately the company needed their system back before I was able to interface to the necessary hardware to build my handheld scope, but I did have a lot of fun in the process.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago

    This is an interesting idea for a project. I'm not sure where it would end up but it could be fun, maybe with some form of OLED display and colour changing dot.

     

    Dubbie

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to Gough Lui

    If you look at an accelerator, that could be a way to induce the resistance to the board and direct the  xy plot. An added bonus it could have a micro controller to smooth the changes out...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to Gough Lui

    yes, (drum roll) it's a 'fine line' (cymbal clash) image

     

    I seem to recall several attempts with stepper motors attached to real Etch-a-Sketch tablets, and I think one even was connected up to a R-Pi camera so it would attempt to sketch the photo just captured. I guess you could take it a step further by capturing a video frame-by-frame and then doing a time-lapse of the sketches generated for each frame back into a new video...

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 6 years ago in reply to beacon_dave

    Well, if I was doing that, I might as well get myself a two-channel arb waveform generator and draw everything with vectors ... but I think that's cheating. I could do it (slowly) with the multi-channel power supplies I have, especially with some code over SCPI or loading in AWG points into the internal memory. That would be too perfect. There's no heart in that! I'd have to say, buying a real Etch-a-Sketch and rigging up stepper motors to the knobs would probably be more exciting.

     

    - Gough

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>