Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gough Lui's Blog An Expensive Mistake: I blew a fuse, and now I feel like a fool!
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 2 May 2015 2:11 AM Date Created
  • Views 4066 views
  • Likes 1 like
  • Comments 9 comments
  • RoadTest
  • accidents
  • keysight
  • fuse
  • handheld_dmm
  • digital_multimeter
  • accident
  • dmm
  • accidental
  • safety
  • agilent
Related
Recommended

An Expensive Mistake: I blew a fuse, and now I feel like a fool!

Gough Lui
Gough Lui
2 May 2015

Last week, I delivered a review of the Keysight U1461 Insulation Resistance Test Multimeter. It's a lovely unit, and as with all new and wonderful tools, it's become my new "go to" unit when it comes to experiments. In my review, I commended it for the convenience feature of being able to detect an open fuse without actually taking it out and testing it by using the Earth Bond test selection as the manual said ...

image

Had I been a little more awake this morning, I might not have had to use this feature ... and subsequently feel like an absolute fool.

 

The Story

 

Just last night, while I was sleeping, a thought came to me that I should probably investigate the old E-I core laminated transformer I pulled out of some gear a while ago. Its condition was unknown, but it was an unremarkable step-down transformer from an old discarded piece of equipment, maybe even 30 years old. It was pretty small, no more than 10VA at the most. I was thinking of using it in series as a current limiting choke for some AC experiments with a miniscule load, as we know, the transformer should be perfectly safe just hooked across the mains anyway, so in case of a short, we shouldn't be getting dangerous levels of current. After all, this is basically the same principle behind an old-fashioned magnetic/iron fluorescent tube ballast.

 

Being ever cautious, of course, I don't like playing with mains directly, and I don't like the massive fault currents that can arise. I don't even like using mains through an isolation transformer, fused. Instead, I opted for my go-to - a pure sine wave inverter driven by a lab benchtop supply. As the inverter is "insulated" and the benchtop supplies are "floating", there is no likelihood of me tripping RCDs or having current flow through me and ground - it's purely isolated. Better still, as it's a wimpy 300W inverter, the fault currents are limited too. For an additional safety measure, the power has to go through a 1A Variac/autotransformer (so I can vary the voltage) and it's fused too.

 

image

With this sort of arrangement, I should be able to measure the magnetizing current of the transformer to see what it's quiescent losses are (and hence, the current it will "let through" on a worst case scenario). Simple enough right? Not quite.

 

I did have a thought about whether such an arrangement would be good - there's likely some form of inrush (despite the small transformer) current which may be large enough to stress the fuse (although I doubt it). Of course, with 10VA, the quiescent current should be a lot smaller than 440mA, so I thought, what the heck, lets just get the measurement before I get breakfast. Bad move.

 

Whoops, I did it again ...

 

I flipped the switch on the lab supply and immediately, something didn't feel right. There wasn't any sound, but the meter was reading an infinitesimal amount of current when I was expecting something in the order of at least milli-amps. I check my wiring, and it's fine. I check the output voltage on the Variac, all good.

 

Then I decided to flip the U1461A over to Earth Bond mode ... and the bad news was there ...

image

That would explain it. A fuse open, meaning the circuit had opened inside the meter and somehow we've exceeded 440mA for long enough to blow the HRC fuse inside. Damn, I feel like a fool now. I blew a fuse when reviewing the Tektronix PA1000 due to inrush currents. You would've thought I'd have learnt my lesson by now.

 

Interestingly, it wasn't due to inrush currents. Further investigation with the resistance showed what appeared to be a shorted primary turn, meaning that the transformer was busted anyway. Why didn't I check that before I powered it up? It's so obvious in hindsight. Lesson learned ... maybe.

 

The Fuse

 

The fuse is housed in the bottom panel section on the U1461A and requires two screws to be removed to get to it. The rear panel markings state the specifications for the fuse. It is to be a 440mA fuse, with a working voltage of 1000V and an interruption rating of 10kA minimum. The size isn't specified, but since I have to replace it anyway, it gives me a reason to pull it out.

image

The fuse used is a type specially used in digital multimeters, and is a fast, high-rupture capacity fuse with a large size. Levering it out of the clips took the use of some screwdrivers.

imageimage

The original fuse comes from SIBA - a reputable German manufacturer of fuses. It is designated as a DMI fuse. It has a length of 35mm. The unit exceeds the requisite 10kA interruption capacity, and has 30kA interruption rating.

image

The fuse has a diameter of 10mm. With this information, lets scour the element14 Australia catalogue for some replacements.

 

Replacement Fuses

 

After looking for some replacement fuses, did the actual sense of what I had done finally sink in. I wished I could just say "sorry" and everything would be forgiven. Okay, it's not quite that big of a mistake, but if I were to do it again, I wouldn't be too happy. There are several options for replacements:

  • The Cheapest: 546719 Fluke 440mA Fast Acting Cartridge Fuse - intended for Fluke DMMs, 10x35mm size, 440mA with 20kA interruption rating, currently AU$11.00 each.
  • The Exact Replacement: 1827166 SIBA Fuse for DMI 1000VAC/DC 10x35 0.44A - the exact fuse as supplied by the OEM, with 30kA interruption rating. Currently AU$21.84 each.
  • The "Just Enough": 9943331 Littelfuse 0FLU.440T Fast Acting 440mA Fuse - another suitable 10x35mm fuse, with a 10kA interruption rating which is just enough. Currently AU$70.31 each - you might as well buy the other ones unless you have no other option.
  • Another "Just Enough": 1241957 Bussmann by Eaton DMM-B-44/100 Fast Acting 0.44A Fuse - also with 10kA interruption rating, currently at AU$71.24 each - again, might as well buy one of the others unless you're out of options.
  • For Insane People: 1688829 Chauvin Arnoux P01297094 Fuse HPC 10x38 0.44A 1kVX5 - Um. I'm not sure what the interruption rating is, and at 3mm longer, it probably will fit. Good thing they are awaiting delivery because it's AU$421.09 each. Not the one you'd opt for.

 

As a result, there are plenty of options if you're looking to replace the fuse, but none of them particularly cheap. That being said, I'll probably go with the Fluke unit, as it's the cheapest one that meets specs. If you're looking to be most authentic, the SIBA one is available at about twice the price. None of the other options seems to be in the realm of reasonableness.

 

Conclusion

 

In the end, it was a case of mea culpa - I didn't check the winding resistance and shoved power right onto the winding which happened to be shorted. I didn't think carefully about the discrimination of the fuses - I'm just used to the 1A fast blow fuse in the Variac going before anything significant happens, but when your meter has a 440mA fast blow as well, that will be the "weak" spot which goes first. It's a good thing that it worked for the safety of the meter. I suppose this is why I wished the U1461A also had a high current range, which might be fused less aggressively. At least it's not a permanent mistake.

 

The fuse is a relatively expensive part, and after you blow a few, you'll do your darned best not to blow any more. That being said, it's an integral part of the safety of the meter, and your safety as well, so it's critical to replace it with a part that meets specifications - regardless of the cost. If you're looking for a replacement, it just so happens that element14 stocks several alternatives, so that's nice.

 

Maybe next time, I should have breakfast first before I try doing anything.

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to Gough Lui +2
    I think the benefit of the lamp is that you can easily adjust the sensitivity by changing the wattage. They instantly light up if there is a short so its pretty obvious. They also are resistive which means…
  • Problemchild
    Problemchild over 11 years ago in reply to mcb1 +2
    Yep I've seen that a lot for Radio /Tv repairs /Switch mode stuff/ High power RF or Valves in general. In fact I was building one in to my isolation transformer & Variac setup for just that reason I agree…
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild +2
    That Siba fuse is £4.41 even in CPC here in the UK
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild

    That Siba fuse is £4.41 even in CPC here in the UK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to mcb1

    Yep I've seen that a lot for Radio /Tv repairs /Switch mode stuff/ High power RF or Valves in general.

    In fact I was building one in to my isolation transformer & Variac setup for just that reason  image

    I agree it's all a bit old school thus all the "dated" use cases I thought up but who cares if it saves the day.

    I too learnt this trick from people who were very grey even  way back then, at least they had all their fingers and stuff so must of been a good idea image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Gough Lui

    I think the benefit of the lamp is that you can easily adjust the sensitivity by changing the wattage.

    They instantly light up if there is a short so its pretty obvious.

    They also are resistive which means they don't alter or affect the device under test.

     

    It was probably one of the best (and cheapest) things I learnt in 30+years of playing with electronics and stopping the "magic smoke" from escaping.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 11 years ago in reply to mcb1

    Definitely a good idea to have image Thanks Mark! ... I was going to use the transformer as an inductance for a similar current-limiting purpose in future testing for very sensitive pieces of equipment, for the main benefit that unlike a resistive load, it doesn't put out a load of heat. I suppose it's all moot when it comes to repair and servicing, and the series light globe will always be a handy "first step". I've heard others have used variacs as series inductances for current limiting purposes but I haven't tried that myself.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    Gough Lui

    I'm glad you've identified the fuse and the costs ...I'll bookmark it for future.

     

    One of the older guys at work taught me a very good safety circuit he used for testing switchmode supplies.

    If you wire a lamp in series with the device you are testing, then any fault current will tend to light the lamp.

     

    For his unit he had it wired as an extension cord and simply swapped a 100w or 150w lamp.

    You could make it with two lamps and switches, connection points for current, or more safely the voltage across the lamp.  image

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>