Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gough Lui's Blog Designing & Building a USB/LAN 40-input 1W/2W/4W Solid-State Relay Multiplexer with RP2040
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 24 Sep 2022 7:31 AM Date Created
  • Views 2025 views
  • Likes 11 likes
  • Comments 7 comments
  • project
  • ethernet
  • usb
  • test and measurement
  • rp2040
Related
Recommended

Designing & Building a USB/LAN 40-input 1W/2W/4W Solid-State Relay Multiplexer with RP2040

Gough Lui
Gough Lui
24 Sep 2022

Having recently finished my blog series for the Experimenting with Thermistors Design Challenge, and taking a breather on a RoadTest at the moment, I found some time to embark on a project that I had wanted to do during the challenge but did not have time to. Part of my experimentation used a mechanical relay multiplexer shield that I built to measure multiple thermistors quasi-simultaneously with the DMMs I have. Unfortunately, that relay multiplexer being mechanical has a limited lifetime and makes quite the racket - not ideal for use in a bedroom. The ten inputs were also a potential limitation for future experiments

As a result, I decided to embark on a journey to build a solid-state relay multiplexer that could operate in one-wire, two-wire or four-wire mode. I also decided it would be a good chance to put the RP2040 into action as well, being my first project to use the Raspberry Pi Pico microcontroller. I fought component shortages, redesigned the PCB after missing out on stock and did my best to do SMD at home with the minimal equipment (double sided too!) and 3D printed myself a matching case to go with it.

image image

In the end, I managed to get it all working just as I expected ... building something I just couldn't commercially buy at a price which was a fraction of what such modules would cost assuming I had the right scanning DMM to go with them. Performance was not bad either - the RP2040 is a bit of a beast. Even my spaghetti code decided to hold in there, with stress testing running over 5.25-million select operations without a single failure ...

Read the full article over at my personal blog - https://goughlui.com/2022/09/24/project-usb-lan-40-input-1w-2w-4w-solid-state-relay-multiplexer-w-rp2040/

  • Sign in to reply
  • Gough Lui
    Gough Lui over 4 years ago in reply to phoenixcomm

    Umm ... this one supports USB and Ethernet thanks to using a W5100S-EVB-Pico?

    I don't usually use USB, but there are instances where (for security) people do not allow the use of Ethernet, so USB is more of a fallback.

    Usually, I use USB for power or for resetting the Ethernet config as the board supports allocation of a static IP and custom MAC.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 4 years ago

    cool, but personally I would have used a different communication other than USB. The problem I have with USB while it is ubiquitous, it never seems to come back at the same address twice, I have been burnt by USB so I try and avoid it.  Ethernet comes to mind as well as CAN..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago

    Just when I thought I was done ... I decided that I wasn't ... so I'd spend some time improving the code and testing it more thoroughly. The results are in a follow-up posting:

    https://goughlui.com/2022/10/03/project-solid-state-mux-new-code-performance-stress-resistance-b-w-power-tests/

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago in reply to neuromodulator

    Glad to see I'm not the only one with the need. Would have to say that I learned quite a bit by doing this one - had I designed it with 2W as the priority, perhaps I would have changed the shape/terminal arrangement to make wiring such a beast more simple. But I thought 1W switching is good enough for many needs, so hence this compromise solution.

    Would be good to see what you come up with ...

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neuromodulator
    neuromodulator over 4 years ago

    Very interesting, funnily this is something I've also been working on for the same reason.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>