Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gough Lui's Blog element14 to the Rescue: Toyota Camry (2000) Remote Repair
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 31 May 2016 11:05 AM Date Created
  • Views 1145 views
  • Likes 5 likes
  • Comments 7 comments
  • replacement
  • part
  • car
  • repair
  • battery
  • obsolescence
  • automotive
  • 433mhz
  • 433
  • remote
Related
Recommended

element14 to the Rescue: Toyota Camry (2000) Remote Repair

Gough Lui
Gough Lui
31 May 2016

I suppose all the car owners out there love the luxury of having a remote keyfob to lock and unlock their cars, but periodically, they need their batteries replaced. Imagine my surprise when my Dad said that "the battery doesn't seem to be replaceable" ... when every remote I had met to date had a socket for some odd-ball A21 12v cell or a lithium coin cell.

 

Thanks to element14 and their prompt order fulfillment, we were on our way with nothing more needed than a soldering iron, desoldering braid, solder, superglue and an AU$1.18 part. Beats buying a new remote for $88 ... one with an unknown lifetime, but it does give pause to think why they would engineer a product in this way, and whether this inbuilt obsolescence was the right thing to do in the first place.

 

Full work-log at http://goughlui.com/2016/05/31/repair-teardown-toyota-camry-2000-remote-key-fob/

 

- Gough

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 10 years ago +2
    Good work. I guess since it doesn't have a chip and the sync process is in the manual they are replaceable. Many of the domestic Japanese cars are designed for 5yr life, as they then require lots of items…
  • Gough Lui
    Gough Lui over 10 years ago in reply to mcb1 +2
    They technically are replaceable in the sense they are not hard coded in particular ways, although some of the similar models require a "voodoo" style procedure to "pair" a new key with the car (e.g. here…
  • jw0752
    jw0752 over 10 years ago +1
    I love it when I can beat the system and watching someone else do it is just about as satisfying. Good Job Gough. John
  • aspork42
    aspork42 over 8 years ago

    Very cool post! I just came across this. I have two key fobs that need some "TLC" - One is this from Adafruit which basically requires a similar "permanent" battery since there is a lot of corrosion buildup on the battery contacts. I always have to clean the contacts to make them work again... I also have a remote start that has very poor reception. I actually need to scope out the signals from the fob to see what's really going on with it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to mcb1

    They technically are replaceable in the sense they are not hard coded in particular ways, although some of the similar models require a "voodoo" style procedure to "pair" a new key with the car (e.g. here) which is an absolute PITA. That being said, this particular car was a domestic AU spec provided by a local dealer, but we do get some Japanese Imports around here too but since the import restrictions and registration requirements are somewhat onerous, they are not as numerous as might be imagined.

     

    That being said, most surface mount push buttons do last a good deal of time. I just picked a random cheap switch with the same sort of shape (MC32882 - MULTICOMP - SWITCH, TACTILE, SPST-NO, 50mA, SMD | element14 Australia) for about AU$0.40 and according to the datasheet, the operating life is a whopping 200,000 cycles. Assuming one uses it 10 times a day for the past 15 years ... that's only about 27% of the life consumed. Given it's used a lot less, I suspect the button mechanism still has quite a way to go yet image.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to shabaz

    I suppose with the newer key-integrated style of controller, it's easy for the car's RFID field that's normally used for the key transponder to be used to trickle charge the battery and top it off. Glad to see they have a decent lifetime - it could almost be excusable if it was not replaceable if they had made it rechargeable but sadly technology was not quite there yet in the "consumer value grade" cars of 2000.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago

    Good work.

    I guess since it doesn't have a chip and the sync process is in the manual they are replaceable.

     

    Many of the domestic Japanese cars are designed for 5yr life, as they then require lots of items replaced under local laws.

    Hence in NZ we have lots of "Japanese Imports" that have strange things compared to something for the Aust/NZ market.

     

    Given that the button cover is worn out (and most likely the actual button next), making it a non-replacable item is not as bad as first thought.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago

    Hi Gough,

     

    Interesting article! Yeah a shame Toyota shaved some cost this way.

    The car I have uses a wireless charging method, and the battery is completely sealed. It uses a VL2020 lithium battery, apparently with 1000 charge cycles so I guess there is some intelligence to figure out when to charge the battery (e.g. after 100 lock/unlock cycles etc, or the key reporting battery status). It could explain why occasionally (well, very rarely, e.g. once per year perhaps, for a period of a week or so) I thought the battery was dying - perhaps my driving pattern had changed and I'd not drive the car for long enough to charge it. It always seems to recover.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>