Personal Blogs
  • Community Hub
  • More
Personal Blogs
Hardware Camera Location and Mounting
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mcb1
  • Date Created: 25 Aug 2013 11:29 AM Date Created
  • Views 3559 views
  • Likes 3 likes
  • Comments 19 comments
  • wifi
  • raspberryp-pi
  • raspberry_pi_camera
  • solar
  • temperature_measurement
Related
Recommended

Camera Location and Mounting

mcb1
mcb1
25 Aug 2013

This is part of my project to fit a solar powered RaspberryPi webcam at Mt Lyford that starts here

 

An excuse for a field trip (to a skifield) on a nice day, is not to be missed, however this trip was all business, with a couple of other things to look at/repair as well.

The exact location and mounting method was one of the things on my list.

 

Snow, ice and the odd heavy machine (groomer) means that unless its well anchored, its very likely to move.

Snow is a strange thing, and this year they received the largest dump in 30 years, over 2m (78 inches)

Many barns and sheds around the area, caved in with the weight of the fairly wet snow dump.

 

The snow was also delivered with high winds, which meant some drifts were 6m deep, and the only access to the field was by helicopter.

 

Obviously any mounting (and what its fitted to) needs to withstand some abuse, add in some brittleness from extreme and prolonged cold, and you need to plan carefully.

 

 

imageimage

 

This pole is driven well into the ground and is solid.

It also is far enough away from the groomers when they shape the return track, as the corner is widest at that point.

 

The base of the pole has a nice area for a wooden battery box, that will withstand the elements (and the odd hit from a shovel ... if they need to dig it out).

 

The view from the location is right, and while this isn't from the RPi, gives the option of two tow lines to aim at.

(There has been very little additional snow and warm weather since that first dump, and as a conseqence a lot off trail has been lost.)

 

image

 

While I was there, I considered where the sun would be, and looked at what options there were for the solar panel.

This photo was taken at 12:46 pm and gives me a pretty good idea of the panel angle and orientation.

It can be combined with the other mount and will fit on the pole easily.

 

imageimage

 

Because I couldn't ski that day, I had to borrow one of the new Snow mobiles, which I have to say are a bit addictive.

However it wasn't a joyride as I helped deliver some fuel to the rope tow ...

 

 

Mark


  • Sign in to reply
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    Mostly interested in the comms link to be honest the two modules I was on about  were

    http://uk.farnell.com/jsp/search/productdetail.jsp?SKU=1348829

    and

    http://uk.farnell.com/jsp/search/productdetail.jsp?SKU=1348837

     

    The Transiever module is probably more useful for you so this is it:

    http://uk.farnell.com/radiometrix/nim2-434-650-10/rf-mod-txrx-fm-434-65mhz-10kbps/dp/1348860

     

    don't know if they stock it in NZ but there are so many RF modules it's easy to miss them image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to Problemchild

    John

    Thanks for the query.

    I have about three other projects on the go, so its taken a back seat at the moment.

    The ski season is about to finish (due to staffing but also rapidly warming weather here), but its not at the stage of being field tested anyway.

     

    Jonathon Brooks has offered a 'SleepyPi' to beta test and it seems to be exactly what I'm doing with seperate components.

     

    So sorry nothing to report.

    Did you have a particular part you were interested in finding out more information about.?

    I'm still going to use the 2.4Ghz link, but I wouldn't mind a link to the 433MHz modules you suggested. I couldn't find them on the AUS/NZ site.

     

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    Mark how have you got on with comunicating to the PI up that mountain ....any further yet ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    The 433 Mhz modules can go for miles especialy if you can get the antenna arangement right and if you have the narrow band ones the  distance is something like 10 times that of the wide band units.

     

    Have you considered using a small sheet of insulating foam board like Kingspan or similar one side is aluminised and keeps the heat in cold out etc and does not itch or nasty stuff like glass wool

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to Problemchild

    John

    Thanks for the ideas.

     

    I was intending to use a foam insultator around the Pi just like the high alt balloon.

    'Glass Batts' (insulation) is another, but they have other problems (scratchy and irritate some people, easy to blow away)

    Surprisingly they don't work as well when compressed...

     

    I stuck with WiFi, because it was easy, and allowed remoting into the device, etc.

    My first thought was a USB and external antenna, but I was convinced that a seperate unit was a better option, that has been reliable on other skifields.

    It also will allow future expansion.

     

    I was shown a 433Mhz telemetry link last night, and need to order one.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>