Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Alexander's Blog PIFace Control & Display Tear Down
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Problemchild
  • Date Created: 25 Dec 2013 11:01 PM Date Created
  • Views 3838 views
  • Likes 5 likes
  • Comments 26 comments
  • santa
  • mcp23s17
  • catcher
  • piface
Related
Recommended

PIFace Control & Display Tear Down

Problemchild
Problemchild
25 Dec 2013

Currently involved  with the rather fun PiNoir & Santa Catcher Challenge one

of the main Components for the Challenge Kit is the PIFace Control & Display

image

We wanted to know what's inside and what's connected to what but unfortunately

the 16x2 LCD is soldered to the main PCB. Fortunately I have a good de-solder tool to hand

and a few minutes latter we had this.

image

 

First thing you see is the 16 bit SPI port expander from Microchip MCP23S17

 

image

 

From a set of very close photos I'm taking an educated guess the IR Receiver (SV2)  is a Vishay TSOP 34438.

Take a look at the data sheet and the drawing below to get an idea of how it's connected..

 

I've done a check over with the multimeter and checked the continuity and values where appropriate and I feel they are

more or less right .. please contact us with any comments or corrections ..cheers

 

Here's the Johnny CAD drawing image and yes I know I can't draw !!

image

  • Sign in to reply

Top Comments

  • Problemchild
    Problemchild over 12 years ago in reply to shabaz +1
    Cheers Shabaz, Shame I couldn't stump up for the Ruler option and have some straight lines
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to Robert Peter Oakes +1
    oh, Bat moment.... Perhaps Nicole can provide some licensed E14 branded Cad copies for us to use, that would be cool and can be delivered with the E-14 Caffeine Concentrate delivery system (E14 Mugs) …
  • Problemchild
    Problemchild over 12 years ago in reply to Robert Peter Oakes +1
    You can tell this is a geeky blog ... I reed "Doodes" as "bat Diodes" Bat diodes sound cool ...not sure what they are but some one should invent them!! :
  • Problemchild
    Problemchild over 12 years ago in reply to jwier92

    And CE1 for the SPI CS Line

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jwier92
    jwier92 over 12 years ago

    So to be sure, they use pins 2 (5V), 17 (3.3V), 19 (SPI MOSI), 21 (SPI MISO), 23 (SPI SCLK), 25 (Ground).  All of these pins should also be re-usable, so no worries about expanding the header.  Also used is pin 16 (GPIO 23), which cannot be re-used.

     

    Please correct me if my notes are wrong on the pins used.  Great job in tearing it apart and documenting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to shabaz

    Cheers Shabaz, Shame I couldn't  stump up for the Ruler option and have some straight lines image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to gregoryfenton

    Yes they have done a simple nibble mode interface rather than a full 8 bit mode. Each of the 5 tactile switches have a single port and 3 are used for the Jog Control at the top.

    Johnny CAD is available for hire but please check the extensive installation requirements before purchase  image £££££image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago

    Now that's a great CAD system! image

    And useful documentation for the board!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>