Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog $8.00 US Signal Generator Kit
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 27 Aug 2016 6:08 AM Date Created
  • Views 1963 views
  • Likes 9 likes
  • Comments 15 comments
  • signal_generator
  • xr2206
  • kit
Related
Recommended

$8.00 US Signal Generator Kit

jw0752
jw0752
27 Aug 2016

Every once in a while I find one of these irresistible buys from the Chinese sources. Such was the case when I came across this little Signal Generator Kit the other day from Banggood.

 

http://www.banggood.com/XR2206-Function-Signal-Generator-DIY-Kit-Sine-Triangle-Square-Output-1HZ-1MHZ-p-1060825.html

 

At the time I saw it they were having a sale of 23% off which brought the price down to $7.23. Also keep in mind that this also includes shipping from China to Wisconsin USA. I could not resist and ordered 2 of them. It took a little over two weeks for the package to arrive. I like the waiting time between when I order and when the package arrives. It reminds me of waiting for Christmas as a child. I have since learned that, many times, the waiting is actually more fun than the getting.

 

I also like the Chinese Kits as they always present a nice challenge due to the often poor instructions. It forces me to carefully analyze the kit and the parts. Most of the time they have a good screen print to the board so this becomes the primary guide along with the schematic if one is provided. This time there was both a good schematic and a well printed board. Another nice feature of this kit is that it came with a pre-cut and pre-printed plexiglass case. Here is a scan of the instructions so you can see the familiar instructions in Changlish.

 

image

 

Once of the first things to do is inventory the parts and identify the capacitor and resistor values.

 

image

 

Here is a closeup of the circuit board front and back:

 

    imageimage

 

And here is the board after population:

 

image

 

The heart and brains of the little Signal Generator is the XR2206 Signal generator chip. I was eager to see what type of quality and range I would get from the board so I finished assembly of the unit.

 

    imageimage

 

I took some regular stick on feet and cut holes in the middle to accommodate the screws that stuck out. The screws that were sent with the kit to mount the board to the back plexiglass were too short and I found that some washers were needed to make things line up and fit properly. I also had to put some threads in the plastic (M3.5 x 0.5) for the long screws that hold the front panel in place. While the plastic was closely sized to the threads experience has taught that failure to thread usually results in breaking the plexiglass. The unit is designed to work best with a 9V to 12V power supply. I had a 9 volt battery pack handy so this is what I used.

 

Here is the unit in operation:

 

image

 

Testing showed the actual range of the generator was from 600 milli Hz to a little better that 1.2 MHz. Square, Triangle, and Sine signal were available over the entire range. The range is selected by moving a jumper between header pins and the choice of triangle or sine waves is also selected by using a jumper between header pins. They have supplied some very nice little green header jumpers that are easily accessible from the front panel and are just about as convenient as a switch.

 

image

 

The jumpers show a little better in this picture. The left potentiometer controls the amplitude of the sine and triangle output. It is a little counter intuitive for me as it turns the signal down in a clockwise rotation and increases it with the counter clockwise turn. Perhaps it is a Chinese convention but I will have to think about it each time I use it. The amplitude of the square wave is fixed and not adjustable. The other two controls are for Coarse and Fine frequency adjustment. They work very well and allowed me to pull up any target frequency that I tried. In order to get good looking wave forms I had to back off the amplitude to stay below the level where they clipped. I have had a lot of fun waiting for these kits and also had a good time putting them together. To top it off they work a lot better than I expected for the reasonable price.

 

John

  • Sign in to reply

Top Comments

  • idanre1
    idanre1 over 9 years ago +3
    Hi John I read your review and it gave me a drive to shop one for myself First, thanks allot for detailed review. I managed to solder my kit (see attached photos) and when I finished I connected it to…
  • jw0752
    jw0752 over 9 years ago in reply to idanre1 +3
    Hi Idan, It looks like you did a great job of constructing the kit. The two things that seems most likely is that your power supply may have the wrong polarity or it may not be a DC power supply. The center…
  • DAB
    DAB over 10 years ago +2
    Nice post John. Nothing like putting toys together to brighten your day. Nice build. DAB
  • jw0752
    jw0752 over 9 years ago in reply to idanre1

    Looks like you have done a good job of testing and correcting the mistake. Don't be too concerned that the transformer says 9 volts but tests at 13 volts. It is probably not regulated and they expected the original application to pull the voltage down. It should still work on your unit as the chip is rated for up to 26 volts. At least you will get the fun of making another one. I have built a couple of them too, so far. It doesn't matter how many time I do something like this I always learn something new. I am glad you have not given up.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • idanre1
    idanre1 over 9 years ago in reply to jw0752

    Hi John

    Short story: It seems all circuit got fried up...

     

    Long story:

    I found myself digging around for capacitors image

    I found 2 47uF from a very old circuit i made when i was 8 years old... (took some soldering hobby class in school). this is a old goodie i found at my parents house couple of years ago when they moved apartment and decided to give/throw all my old stuff. and i thought to myself this one might be a use someday image

     

    When i measured capacitance one happened to be 47.9uF and the other 84uF, somehow the years added some capacitance.

    I soldered them up in parallel to the circuit in a messy way (see photo) and connected to the circuit.

     

    I took a deeper look on the transformer.

    it does mention the center prong is the negative supply (see photo attached)

    I cut the wire in the middle and switch the wires, soldered it and put some insulation (see photo)

    Then i decided to measure it to see positive 9V. the voltage sampling with my multimeter showed 13V (!!!) instead of 9V.

    Well, this is from an old 200$ wireless phone from panasonic. strange... at least they wrote the polarity is inverted on the transformer....

     

    I took a 9V battery from some clock in my bedroom and nothing:

    GND->SIN shows 0DC,0AC,0Hz

    GND->SQR shows 9DV, 0AC, 0Hz

    After trying every many jumper permutation i have decided to let it go and but additional kit image

     

    https://goo.gl/photos/65Gss1ahX6UwnStz7

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to idanre1

    Hi Idan,

     

    I have done a little research and it is probable that damage was done to the XR2206CP but you will have to replace the cap and give it a try. Any sign of heat from the XR2206 will be a good indication of damage. Fortunately you can get a replacement for $3.59 with free shipping if you are in the USA.

     

    http://www.ebay.com/itm/1-x-XR-2206-XR2206CP-XR2206-Monolithic-Function-Generator-IC-USA-Seller-/322300781213?hash=item4b0a9fa29d:g:st8AAOSwpDdVWBt8

     

    Here is a Data Sheet for the XR2206. I don't always understand everything on the data sheets but they are a good reference and often suggest other circuits that can be built with the chips. Here is a link to the Data Sheet.

     

    http://www.farnell.com/datasheets/314520.pdf?_ga=1.160973309.118307707.1475274175

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • idanre1
    idanre1 over 9 years ago in reply to jw0752

    Hi John

    First, thanks for the quick response!

     

    Your info might be very usefull, now i remember that when i tried to measure dc voltage with my multimeter on the sine output and i saw the voltage was negative...

     

    I really hope only the capacitor is fried and not the whole board or the chip.

    I hope to buy such a capacitor real quick and update on the results.

     

     

    Thanks again

    Idan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to idanre1

    Hi Idan,

     

    It looks like you did a great job of constructing the kit. The two things that seems most likely is that your power supply may have the wrong polarity or it may not be a DC power supply. The center prong of the AC adapter must receive the positive voltage. If negative voltage or AC voltage is applied to the center pin the 100 uF cap which is polarity sensitive will begin to heat up. As soon as the heat passes the boiling point of the electrolyte pressure will build up until you get an explosion or a leak of gas and fluid as it appears that you had. The current rating of your power supply will have had no relevance to the problem because at 9 volts the unit would have taken the appropriate current. If your unit was hooked up in reverse polarity for five minutes there is a real possibility that more than the capacitor got fried. You can try replacing the capacitor, making sure the power is DC and the correct polarity and try it again. There is also the remote chance that the capacitor was defective or that the polarity label was on incorrectly but this is very rare. If you don't have a scope you could also check the output with a small speaker as you should be able to hear the frequency output that is in the audio range. Let me know how it works out for you.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>