Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog $8.00 US Signal Generator Kit
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 27 Aug 2016 6:08 AM Date Created
  • Views 1696 views
  • Likes 9 likes
  • Comments 15 comments
  • signal_generator
  • xr2206
  • kit
Related
Recommended

$8.00 US Signal Generator Kit

jw0752
jw0752
27 Aug 2016

Every once in a while I find one of these irresistible buys from the Chinese sources. Such was the case when I came across this little Signal Generator Kit the other day from Banggood.

 

http://www.banggood.com/XR2206-Function-Signal-Generator-DIY-Kit-Sine-Triangle-Square-Output-1HZ-1MHZ-p-1060825.html

 

At the time I saw it they were having a sale of 23% off which brought the price down to $7.23. Also keep in mind that this also includes shipping from China to Wisconsin USA. I could not resist and ordered 2 of them. It took a little over two weeks for the package to arrive. I like the waiting time between when I order and when the package arrives. It reminds me of waiting for Christmas as a child. I have since learned that, many times, the waiting is actually more fun than the getting.

 

I also like the Chinese Kits as they always present a nice challenge due to the often poor instructions. It forces me to carefully analyze the kit and the parts. Most of the time they have a good screen print to the board so this becomes the primary guide along with the schematic if one is provided. This time there was both a good schematic and a well printed board. Another nice feature of this kit is that it came with a pre-cut and pre-printed plexiglass case. Here is a scan of the instructions so you can see the familiar instructions in Changlish.

 

image

 

Once of the first things to do is inventory the parts and identify the capacitor and resistor values.

 

image

 

Here is a closeup of the circuit board front and back:

 

    imageimage

 

And here is the board after population:

 

image

 

The heart and brains of the little Signal Generator is the XR2206 Signal generator chip. I was eager to see what type of quality and range I would get from the board so I finished assembly of the unit.

 

    imageimage

 

I took some regular stick on feet and cut holes in the middle to accommodate the screws that stuck out. The screws that were sent with the kit to mount the board to the back plexiglass were too short and I found that some washers were needed to make things line up and fit properly. I also had to put some threads in the plastic (M3.5 x 0.5) for the long screws that hold the front panel in place. While the plastic was closely sized to the threads experience has taught that failure to thread usually results in breaking the plexiglass. The unit is designed to work best with a 9V to 12V power supply. I had a 9 volt battery pack handy so this is what I used.

 

Here is the unit in operation:

 

image

 

Testing showed the actual range of the generator was from 600 milli Hz to a little better that 1.2 MHz. Square, Triangle, and Sine signal were available over the entire range. The range is selected by moving a jumper between header pins and the choice of triangle or sine waves is also selected by using a jumper between header pins. They have supplied some very nice little green header jumpers that are easily accessible from the front panel and are just about as convenient as a switch.

 

image

 

The jumpers show a little better in this picture. The left potentiometer controls the amplitude of the sine and triangle output. It is a little counter intuitive for me as it turns the signal down in a clockwise rotation and increases it with the counter clockwise turn. Perhaps it is a Chinese convention but I will have to think about it each time I use it. The amplitude of the square wave is fixed and not adjustable. The other two controls are for Coarse and Fine frequency adjustment. They work very well and allowed me to pull up any target frequency that I tried. In order to get good looking wave forms I had to back off the amplitude to stay below the level where they clipped. I have had a lot of fun waiting for these kits and also had a good time putting them together. To top it off they work a lot better than I expected for the reasonable price.

 

John

  • Sign in to reply

Top Comments

  • idanre1
    idanre1 over 9 years ago +3
    Hi John I read your review and it gave me a drive to shop one for myself First, thanks allot for detailed review. I managed to solder my kit (see attached photos) and when I finished I connected it to…
  • jw0752
    jw0752 over 9 years ago in reply to idanre1 +3
    Hi Idan, It looks like you did a great job of constructing the kit. The two things that seems most likely is that your power supply may have the wrong polarity or it may not be a DC power supply. The center…
  • DAB
    DAB over 9 years ago +2
    Nice post John. Nothing like putting toys together to brighten your day. Nice build. DAB
  • idanre1
    idanre1 over 9 years ago

    Hi John

    I read your review and it gave me a drive to shop one for myself image

    First, thanks allot for detailed review.

     

    I managed to solder my kit (see attached photos) and when I finished I connected it to a 9V/600mAH transformer.

    Acording to the intruction 9V is a legal voltage (don't know, maybe 600mHA is too much) but after 5 min of operation the 100uF capacitor just puffed with a light whistle image

    during these 5 min I connected my multipeter to try reading the frequencies with no success (I don't have a scope so this is my best solution).

     

    I wonder if you could see attached photos and manage to figure out if i did some 0-order mistake...

     

    Photos: https://goo.gl/photos/Bx41CmWwZ78eCJK86

     

    Also:

    I managed to insert it into the plexi glass... maybe they increased the screws or something...

    I i needed to break two edges on the box to make room for the power jack and to the output cables.

     

    Best regards

    Idan

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to DAB

    Thanks DAB,

     

    If I had enough variety and quantity of these little kits I would crawl into my basement shop and they would never see me again.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Nice post John.

     

    Nothing like putting toys together to brighten your day.

     

    Nice build.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to michaelkellett

    Hi Michael,

     

    I have played with the 8038 before but I don't remember it being quite as impressive as tthe XR2206. At least I was not able to put it into a usable configuration. I checked and you can still buy the XR2206 chips on e-bay for about $1.60 each.

     

    http://www.ebay.com/itm/10PCS-Monolithic-Function-Generator-IC-EXAR-DIP-16-XR2206CP-2206CP-/401043601761?hash=item5d600fb961:g:5o8AAOSwCQNWdBMf

     

    I down loaded the data sheet for the XR2206 for my library just in case I want to look at it in the future. As you mentioned the chip is now out of the main stream and sometimes this means the documentation gets pulled too.

     

    Thanks for checking out my blog.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago

    Hello John,

     

    I wonder who (if anyone) is making the chip now - it was made by Exar but they don't seem to make them any more (Digikey say it's obsolete and there is no reference to it as a product on Exar's website.)

     

    These little analogue signal generators can be quite useful.

     

    I once designed a  signal generator that worked on the same principle but used CA3080s (also obsolete now I think) for the triangle sweep generator and the sine converter. There was a reason we couldn't use the Intersil 8038 (which is like and was around before the XR2206).

     

    There's a good article here with links to Exar's data sheet and an applications note.

     

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<