Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog A Do Nothing Machine
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 20 Jun 2020 9:15 PM Date Created
  • Views 5779 views
  • Likes 17 likes
  • Comments 30 comments
  • do_nothing_machine
Related
Recommended

A Do Nothing Machine

jw0752
jw0752
20 Jun 2020

The Thinker Revisited

 

          The Thinker Revisited is an Electronic Sculpture built on an X-Ray Control circuit board. I usually salvage these boards for the parts but since I had already taken a couple of identical boards apart I decided to have some fun and see what would happen if I began to add electronic systems and some little electronic kits to it.

 

image

 

          The system runs on 9 to 12 volts and can be supplied with a battery pack or with an AC adapter. There are over 30 LEDs which are driven by 4 scanner kits that use a 555 timer and a CD4017 ripple counter. Each scanner is adjusted to a different cycle time so that there appears to be a random blinking of the lights. The fourth ripple counter kit is set to a slow speed of approximately 2 minutes. This counter, lights some LEDs but it also triggers the operation of some of the other kits that are installed on the sculpture. One of the kits that is triggered once each cycle is the Dice Kit. It is on the left side of the unit in the picture above. You might note that it currently displays a “4”.

 

Another kit that is triggered is one that plays a siren sound. This kit is in the upper left hand corner of the unit. A series of 4 slide switches allows the user to program a variety of 16 different sirens. There is a switch in the vicinity of the siren module so that it can be silenced.

 

image

 

 

A third kit that is actuated each cycle is the voice play back kit. This kit allows the user to record a voice message of up to ten seconds and then that message is played back each time the module is triggered. My first message is, “Please don’t bother me, I am thinking” in keeping with the title of the sculpture “The Thinker Revisited”.

 

image

image

 

Back of the sculpture

 

          Besides the LEDs on the first 3 banks of ripple counters there is a beeper attached to one LED. This beeper sounds each time the light is lit. There is a switch in the vicinity of the beeper so that it can be silenced.

 

image

 

          The sculpture is equipped with a PIR (Passive Infrared) sensor that allows the sculpture to see a person coming 15 or 20 feet away. When the person is detected the sculpture comes to life and starts flashing its LEDs and cycling through its’ kit program. Near the PIR there is a center off switch that allows the user to select continuous operation when the switch is up and PIR operation when the switch is down. When the switch is in the center the unit will not be on or turn on but the idler 5 volt rail remains powered.

 

image

 

PIR and Mode Switch

 

The unit also has an ear in the form of a microphone that is dead center of the top edge of the circuit board. The sound that is picked up by this microphone is amplified and fed to a VU meter on the left edge of the unit. A person can talk or sing and the VU meter will respond to the intensity of the sound.

 

image

 

Mic in upper right corner and VU meter on left side

 

          Along the top of the sculpture there are 3 voltmeters that read out the voltage on the three power rails of the unit. There is a 5 volt supply that is active any time the unit has power. This provides Power to the PIR so that the unit can wake up. There is a secondary 5 volt rail that is used to power some of the kits and a main voltage rail that carries the 9 to 12 volts from the AC adapter or the battery pack. You may note that some of the pictures have decorative frames on the Voltmeters and others don't. This sculpture is evolving and is being changed and added to as I go. It was easier to use some of the pictures that I took along the way.

 

          Whenever possible, components on the original board were used to provide the structure and circuit for the sculpture. The regulators for the two 5 volts rails are part of the original board layout.

 

Addendum

 

 

          The Unit now has an Infrared proximity sensor in the lower left hand corner that can detect an approaching hand that is within 15 cm of the unit. The detection triggers a relay and a red LED on the board. The relay in turn powers a small 12 volt fan that is mounted above the infrared sensor which has 4 red streamers for extra effect. If you look closely at the picture at the top of this blog you can see that the LED is lit and the streamers are flailing in the wind.

 

image

 

          When I was a boy I built several “Do Nothing Machines” out of scrap electronics and parts. This is the first one of this magnitude that I have built in perhaps 55 years. This may be a sign that I have finally gone far enough over the hill that I am regressing to my childhood. In any case it was a nice escape from the stress of the Pandemic, Politics, and Civil strife of today’s world. While I have had a lot of fun with this it I didn't really know how to classify it. I am afraid the people into electronics will call it Art and the Artists will call it electronics neither wanting to own this poorly mixed child of both worlds.

 

John

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +8
    Honestly if someone had asked me this morning if I was finished with this thing I would have said yes. Then as I made my morning walk an idea began to form and before the walk was over I had committed…
  • jw0752
    jw0752 over 6 years ago in reply to ralphjy +7
    Thank you to everyone for your kind comments. Ralph, while my video skills leave a lot to be desired I have made an attempt in this video to answer your request. After standing very still and waiting for…
  • fmilburn
    fmilburn over 6 years ago +6
    John, This definitely belongs in the electronic arts competition. Frank
Parents
  • jw0752
    jw0752 over 6 years ago

    Honestly if someone had asked me this morning if I was finished with this thing I would have said yes. Then as I made my morning walk an idea began to form and before the walk was over I had committed myself to a few more hours of electronic sculpturing.

     

    image

     

    I have decided to give The Thinker arms and hands. In his right hand he is holding a "Clap Switch Module" and in his left hand he is holding a Flashlight that the clap switch will turn on and off. Both the clap switch module and the light are designed to run on 5 volts. Due to the number of things that I have put on the unit I had a concern about power consumption. Therefore the first thing I did before installing the upgrade was to verify the current draw. The test revealed that with everything that could possibly load the circuit functioning the current draw from the main 11 volt source was 400 mA. This reassured me that I was still within an acceptable current draw.

     

    I got some 12 gauge wire and began to fashion a couple of hand shapes. Once the basic hands were formed I bent them into the positions to hold the module and the flashlight. The flashlight presented a small challenge as the fasten points on the circuit board for the left hand also tied the hand to ground. The metal of the flashlight is also ground but I want it isolated and only pulled to ground through the MOSFET. Therefore the flashlight ended up with a couple layers of electrical tape between the fingers and the flashlight body.

     

    I have a long history with the Chinese Clap Switch Kits as I have used them in several previous builds. Here is the schematic for the Clap Switch Module:

     

    image

    I wanted the LED in this circuit to light at the same time as the flashlight. The LED in the circuit turns on with a low from the flip flop and I needed a high to the gate of my flashlight activating MOSFET so I took the signal from the other side of the flip flop which is the junction of R9 - R10 - and the collector of Q3. I already had a spare NTD4906 MOSFET on the board so it was just a matter of running a wire from this point on the board to the gate of the MOSFET. I did buffer this line with a 100R resistor and I also had to pull the gate low with a 10K resistor to ground.

     

    Here are a couple close-ups of the new hands, flashlight and clap module.

     

       imageimage

     

    Finally here is a demo of the clap flashlight in operation:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    With this addition I wanted to continue to enhance the interactive nature of the sculpture. Now the unit can sense the presence of a person, turn on a fan when a hand is near the IR detector, modulate the VU meter when noise is heard and turn on a flashlight with a clap or other sharp noise.

     

    Perhaps it is finished now. (Fingers Crossed)

     

    John

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 6 years ago

    Honestly if someone had asked me this morning if I was finished with this thing I would have said yes. Then as I made my morning walk an idea began to form and before the walk was over I had committed myself to a few more hours of electronic sculpturing.

     

    image

     

    I have decided to give The Thinker arms and hands. In his right hand he is holding a "Clap Switch Module" and in his left hand he is holding a Flashlight that the clap switch will turn on and off. Both the clap switch module and the light are designed to run on 5 volts. Due to the number of things that I have put on the unit I had a concern about power consumption. Therefore the first thing I did before installing the upgrade was to verify the current draw. The test revealed that with everything that could possibly load the circuit functioning the current draw from the main 11 volt source was 400 mA. This reassured me that I was still within an acceptable current draw.

     

    I got some 12 gauge wire and began to fashion a couple of hand shapes. Once the basic hands were formed I bent them into the positions to hold the module and the flashlight. The flashlight presented a small challenge as the fasten points on the circuit board for the left hand also tied the hand to ground. The metal of the flashlight is also ground but I want it isolated and only pulled to ground through the MOSFET. Therefore the flashlight ended up with a couple layers of electrical tape between the fingers and the flashlight body.

     

    I have a long history with the Chinese Clap Switch Kits as I have used them in several previous builds. Here is the schematic for the Clap Switch Module:

     

    image

    I wanted the LED in this circuit to light at the same time as the flashlight. The LED in the circuit turns on with a low from the flip flop and I needed a high to the gate of my flashlight activating MOSFET so I took the signal from the other side of the flip flop which is the junction of R9 - R10 - and the collector of Q3. I already had a spare NTD4906 MOSFET on the board so it was just a matter of running a wire from this point on the board to the gate of the MOSFET. I did buffer this line with a 100R resistor and I also had to pull the gate low with a 10K resistor to ground.

     

    Here are a couple close-ups of the new hands, flashlight and clap module.

     

       imageimage

     

    Finally here is a demo of the clap flashlight in operation:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    With this addition I wanted to continue to enhance the interactive nature of the sculpture. Now the unit can sense the presence of a person, turn on a fan when a hand is near the IR detector, modulate the VU meter when noise is heard and turn on a flashlight with a clap or other sharp noise.

     

    Perhaps it is finished now. (Fingers Crossed)

     

    John

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dubbie
    dubbie over 6 years ago in reply to jw0752

    A good idea.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 6 years ago in reply to jw0752

    And now it is also "interactive art" !

    • Cancel
    • Vote Up +4 Vote Down