Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog An Extreme Ripple Power Supply Build
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 8 Apr 2019 2:49 AM Date Created
  • Views 2529 views
  • Likes 10 likes
  • Comments 20 comments
  • variac
  • isolation transformer
  • ac bench power supply
Related
Recommended

An Extreme Ripple Power Supply Build

jw0752
jw0752
8 Apr 2019

I usually like to build my projects before I blog about them. This is probably due to the number of times the initial plans do not lead me down the envisioned path. The simplicity of this build along with a good pile of solid resources and the fact that I must wait for my panel meters to arrive has made me decide to blog a preview.

 

In my shop almost never a week goes by with out the need of an AC voltage source. I use the AC source to test motors, lights, power supplies, and circuit boards as well as a substitute for transformers. Since I have built several DC bench supplies and blogged about them over the recent years I decided that it was about time to build an AC power supply suited to my needs. I am currently using a Variac that is plugged into an isolation transformer for my applications but it doesn't monitor the voltage or the current so there is always a lot of patch wires and a couple meters to clutter the bench.

 

Here is my wish list for the new bench AC power supply:

 

0 to 160 volts no load output

2 to 3 Amps capable

Isolated from the mains

Binding post and AC receptacle Output

High Voltage warning light

Meters for indication of Output Volts and Current

 

Initially I found the following items in my parts grave yard:

 

image

This will be the isolation transformer. I can put 115 volts on the primary and it will have 130 volts on the secondary. This will drive the small Variac pictured below.

 

image

 

The case will be from an old Dental Cavitron Scaler. I have used this same style case before to build a Bench Power Supply and a DC Electronic Load.

 

imageimage

 

The Plexiglas blank control panel was cut a couple years ago in anticipation of an application for this case. The case as seen in this picture it still needs a cleaning and a coat of paint.

 

image

 

The case has been painted and I have the tentative control panel layout on the sheet of paper next to the case.

 

image

 

The chassis has had some modifications. The metal that the variac is mounted to was originally part of the chassis deck but it has been cut and folded up to provide additional support for the relatively heavy variac. The cut out on the right side of the chassis came with the original piece of equipment. Anomalies like this often dictate where components and controls need to be placed. In this case it will be the recess needed to allow the mounting of an AC line Output jack on the front panel.

 

I have also produced a tentative Schematic for the power supply. I say tentative as I do not yet have the digital AC panel meters and so I am guessing at their requirements. Nothing ever runs true to plans so I will very likely have to take back a few of the things I told you here when I blog about the completion of the build.  Here is the tentative schematic.

 

image

 

One advantage to giving a preview of what I am building is that I can welcome any advice that anyone is willing to send my way. In the past ideas and advice from my many friends here on element 14 have resulted in renovations and improvements in subsequent builds.

 

Sorry about the title but sometimes it helps to get people in the door when I leave them asking what the heck is he talking about now.

 

Thanks John

 

 

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +4
    John, This looks like another interesting build. And yes, the title was a little catchy. I can see the use for a good A/C supply, although in my case, I live in such a D/C world. Only recently (my home…
  • Gough Lui
    Gough Lui over 7 years ago +4
    jw0752 - I don't claim to be an expert, but there are a number of notes and suggestions I would make. 1. Consider putting fuses on both primary and secondary sides of the Variac. They are expensive and…
  • jc2048
    jc2048 over 7 years ago +4
    Don't the test meters need their GND connection to be tied to the output neutral? Otherwise the voltmeter measurement is relative to a floating supply. If you'd incorporated a Pi, it could have been a…
  • three-phase
    three-phase over 7 years ago in reply to jw0752

    The old Foster SCITS100 injection test sets we used simply had a limit switch that was activated by the wiper when the variac was turned to minimum. This energised a contactor to switch the output on. There was then a holding circuit that kept the contactor energised until the test set was turned off, tripped or the e-stop hit.

     

    You may be able to conjure up something similar, unless someone else has some other thoughts.

     

    Kind regards.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to three-phase

    Hi Donald,

     

    Thank you for the information. I will move the 3A fuse to the wiper side of the output. I did not know that either side of the isolated output could be designated as Neutral since neither is tied to ground but I can see your point from a convention standpoint. I had given some thought to having a way to make sure the wiper is at zero volts relative to the other output before the unit would turn on and I may still figure out how to do this. It is a great safety feature as I can see where I might forget to turn the wiper to zero and put too much voltage on a project before I realized. Thanks for taking the time to help with the design.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago in reply to jw0752

    On the output, you have independently fused the neutral with a 3A and fused the line side between the isolating transformer and variac with a 4A. It would not normally be recommended to fuse a neutral line unless it is a double pole device that switches both the neutral and line together.

     

    If you get a fault, the neutral is disconnected but this leaves the line still connected out to what ever it is feeding. The shock potential is reduced as you are operating an isolated supply from mains, but is could still give someone a nasty surprise if they weren't paying attention.

     

    I have also come across supplies that utilised a switch on the variac so that on initial power up it would only ever switch on the output if the variac was at its minimum. The prevents unwittingly applying too high a voltage to the load, if the supply is energised without setting it up correctly first.

     

    Kind regards.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to jw0752

    Wow! That is a monster!

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to Gough Lui

    Sounds like you have a good system for your needs. It is always a compromise of one type or another. I have on a couple occasions bought a used 600 watt computer power conditioner and modified it to be an isolation transformer. This has worked pretty good and being used it has saved a lot of money on the cost of a large toroidal transformer. Here is the one i have sitting on the shelf awaiting my next need.

     

    image

     

    This is a PowerVAR 6.0.  I have one like it that feeds a mains strip on my bench which I use when needed. One still has to be very careful but at least I don't have to feel quite so threatened by the anti-static strip on the edge of the bench.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>