Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Auto Power off for Solder Station
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 26 Oct 2014 5:03 AM Date Created
  • Views 2774 views
  • Likes 1 like
  • Comments 13 comments
  • automatic
  • timer
  • iron
  • soldering
  • tools
  • switch
  • safety
Related
Recommended

Auto Power off for Solder Station

jw0752
jw0752
26 Oct 2014

Recently there has been a good discussion on how to monitor Soldering Irons and Stations. I was going to add this post on to the thread that was already in progress but since it was really a comment thread for someone else's build I decided to post this as a stand alone blog post.

 

I too have had problems in the past with a soldering iron at our business site. Since multiple people use the solder iron it seems that too often we were forgetting to turn it off and would come back to the shop after a weekend only to find it running. The last time it was left on it was my fault. Having chewed my son out many times before for his transgression it was his turn to let me have it. After enduring my deserved dressing down I went back to my home shop and designed a simple solution.

 

I put together a simple 555 powered monostable timer tied to a relay. It was my goal to have the timer run for 60 minutes and then shut off the solder iron that would be plugged into it. Due to the tolerance of the components that I used this actually turned out to be 68 minutes which was in the ballpark. The timer plugs into the 120VAC outlet in the shop and the solder iron plugs into the other side of the timer box. When the RESET button is pressed the timer turns on the iron for 68 minutes and then automatically turns it off. If one is still using the iron it is necessary to push the reset button for a second 68 minute period. This solution has proved very effective and the iron has not been left on since the timer was installed.

 

 

Here is a schematic of the Soldering Iron Timer

 

Correction to Schematic: There needs to be a 10 k resistor between the 12V rail and pin 2 of the 555 timer to work properly.

 

 

image

 

I wasn't too concerned with cosmetics for this project and so I built it into a used plastic box and labeled it.

 

 

image

 

John

  • Sign in to reply

Top Comments

  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild +1
    BTW I got a Metcal from a mate at the right price so was quite happy... went to check them out again on Ebay to find silly sods paying as much as a new one for some well worn model. Some times people go…
  • jw0752
    jw0752 over 11 years ago in reply to Problemchild +1
    Hi John, You are right, we could monitor the delta temp of the stand using a microprocessor and then everytime we encountered a negative change of a specified duration we would start the shut down timer…
Parents
  • Problemchild
    Problemchild over 11 years ago

    I was wondering about the fixed period  for the  usage. I think that maybe you could do something measuring not the absolute temperature but a relative dip in say the stand temperature. The act of removing and replacing the Iron would cause the temperature to cycle. The Relay would then go off after a fixed time after the last cycle!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to Problemchild

    Hi John, You are right, we could monitor the delta temp of the stand using a microprocessor and then everytime we encountered a negative change of a specified duration we would start the shut down timer. If a second dip was not encountered in the given time period the shut down would be completed. This would work best with a cheap iron like mine. Any regulated iron would be cycling naturally.  In my case I had good knowledge of the situation at our shop and decided that the fixed shut down time was an adequate solution.

    John W.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 11 years ago in reply to Problemchild

    Hi John, You are right, we could monitor the delta temp of the stand using a microprocessor and then everytime we encountered a negative change of a specified duration we would start the shut down timer. If a second dip was not encountered in the given time period the shut down would be completed. This would work best with a cheap iron like mine. Any regulated iron would be cycling naturally.  In my case I had good knowledge of the situation at our shop and decided that the fixed shut down time was an adequate solution.

    John W.