Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Checking Out a Small Variac
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 29 Jun 2016 6:26 AM Date Created
  • Views 4267 views
  • Likes 4 likes
  • Comments 5 comments
  • variac
Related
Recommended

Checking Out a Small Variac

jw0752
jw0752
29 Jun 2016

When I passed the junk pile at my son's dental repair business today I noticed an old Ritter Meteor X-Ray unit sitting in parts. It was slated to go for scrap metal the next day. The one item that caught my eye immediately was a small Variac mounted to the front panel. I took a few minutes and removed it and brought it back to the electronics shop. In case you are not already familiar with variacs, they are a single winding transformer with some extra taps and a wiper that can slide across the full winding and tap at any point. I will draw a diagram of this one after I figure it out.

 

image

 

Variacs like this one were common in the dental x-ray units from the 1960s. They were used to adjust voltages to the electronics of the x-ray unit so that the x-rays would be more consistent.  Another purpose was to adjust the filament voltage of the x-ray tube so that the intensity of the x-ray beam could be adjusted. Now days all these adjustments are done automatically with microprocessors. Being an old guy, pieces of electronic equipment from the 1960s get me all teared up. At slightly over 1 kg it felt like a brick of pure electronic gold in my hand.

 

image

 

This picture gives a clear view of the wiper mechanism. Turning the knob on the front rotates the wiper from one end of the winding to the other. The winding is set in a hard plastic and the enamel has been removed from the wires. The wiper is made of a spring loaded arm with a carbon point, very much like the carbon used in motor brushes.

 

image

 

This particular Variac had contacts for the two end points of the winding, numbered 1 and 2, the wiper which was numbered 3, and 3 additional taps numbered 4, 5, and 6. I began the process of determining the position of the 3 extra taps by putting AC voltage across the end winding points 1 and 2. For this I used an AC bench power supply that I built 50 years ago. This power supply is isolated from the mains and allows me to slowly increase the voltage while monitoring the current. When the voltage on the outer ends of the winding reached 120 VAC the current was reading 14.3 mA. This is the no load current of the Variac and was low enough so I was comfortable with continuing my investigation. The voltage from one end of the winding to the taps, numbered 4, 5, and 6 were now measured with a meter. Tap 6 had a voltage of 60 volts, tap 5 had a voltage of 100 volts and tap 4 had a voltage of 110 volts. It is common in the wiring of a variac to put the mains voltage between one end of the winding and one of the taps. This allows the wiper to cover a voltage range from 0 volts to a voltage 10 or 20 volts in excess of the input mains voltage. At this point it seemed that pin 1 should be the 0 point (Neutral) and either 5 or 6 should be the mains (Line) voltage. The two taps 4 and 5 were probably provided to adjust for locations having either 110 volts or 120 volts for mains voltage. For this experiment tap 5 was chosen and as noted in the diagram this created a 60 mA no load input current. Here is a diagram of the Variac with the mains hooked to pins 1 and 5.

 

image

 

As you can see this provides for the wiper to travel as high as 140 volts from a 120 volt mains supply. In the case of this variac, I decided that the load would most suitably be connected across pins 3, and 2. The reason that pin 2 was chosen as 0 volts for the load instead of pin 1 was that the direction of the wiper moves towards pin 1 when the knob is rotated in a clockwise direction. It is customary for me to expect an increase in voltage or volume with a clockwise rotation. This configuration gives an increase in voltage between 2 and 3 when the knob is rotated clockwise. Strangely, I expect just the opposite from water faucets where a clockwise rotation lowers the flow but that is another story. I have not been able to determine a purpose for pin 6 the center tap of the variac. As part of the experiment I put the line voltage across pins 1 and 6 but the current was too high for it to have been intended as line input.

 

    imageimage

 

Here are a couple pictures of my experimental set up. The picture on the left shows a Load Bulb attached from pin 2 to pin3 and dialed up to 100 volts. The AC ammeter is showing input current of 260 mA.

 

Before we had all the cool semiconductor devices that we have today the Variac was a simple solution to provide a variable voltage source. It is still the best way to have a variable AC source at the mains frequency but there are some important safety considerations. If you use a variac without also using an isolation transformer you will have live mains power on one of your power supply wires and it WILL eventually give you a shock.

After learning this lesson the hard way I have refused to use a Variac unless there is an isolation transformer between it and the mains power. Even with an isolation transformer it is important to remember that any voltage over 40 volts or so can be fatal. While an isolated supply will not give you a shock to ground there is still full voltage between the 2 output wires.

 

Caution! Working or experimenting with a variac can be dangerous unless you are experienced working with mains power.

 

John

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 10 years ago +2
    You can still buy new ones quite easily - I have one but I very rarely use it. In the 1970s I used them all the time to start up mains powered audio power amplifiers. We didn't have any DC supplies able…
  • DAB
    DAB over 10 years ago +2
    Hi John, Once again you provided me with many memories of the old days of electronics. I have an old variac I found when we cleaned out my father in law's basement. I have not fired it up but he used in…
  • jw0752
    jw0752 over 9 years ago in reply to volly +2
    Hi Yunus, Thank you for all your kind words on my posts today. As I encounter interesting components or if I do a project I take pictures and write about it. I am sure something new will pop up soon. Thanks…
  • jw0752
    jw0752 over 9 years ago in reply to volly

    Hi Yunus,

    Thank you for all your kind words on my posts today. As I encounter interesting components or if I do a project I take pictures and write about it. I am sure something new will pop up soon. Thanks again for reading and for all your support.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • volly
    volly over 9 years ago

    jw0752. What else do you have in your "arsenal of goodies"....I really enjoy you posts...very informative and useful.....

    Thanks John....

     

    Yunus.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Hi John,

     

    Once again you provided me with many memories of the old days of electronics.

     

    I have an old  variac I found when we cleaned out my father in law's basement.

     

    I have not fired it up but he used in in his electronics repair business in the 1920's.

     

    I do agree with Michael, be very careful with these devices.  They can provide a lot of current, so treat them with the respect they deserve.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to michaelkellett

    Hi Michael,

     

    Thanks for the information on the origin of the name. I love learning the history behind names and unique words. I use my big variac frequently when trouble shooting switching supplies.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago

    You can still buy new ones quite easily - I have one but I very rarely use it. In the 1970s I used them all the time to start up mains powered audio power amplifiers. We didn't have any DC supplies able to put out +/- 50V at 5A or more so we just used the amp's main supply. The only way to start it gently was to wind up the mains via the variac and watch the current.

     

    BTW - Variac is  a Hoover - ie the historically dominant manufacturer's name has become the part name.

     

    There are lots of Chinese ones on Ebay - many with built in meters (and rather lethal looking 4mm terminals)

     

    MK