Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Experimenting with Weak Batteries
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 29 Apr 2016 5:22 AM Date Created
  • Views 1062 views
  • Likes 6 likes
  • Comments 12 comments
  • energy harvesting
Related
Recommended

Experimenting with Weak Batteries

jw0752
jw0752
29 Apr 2016

Many of the small electronic gadgets that I use daily, cameras, labeler, and test equipment, do not tolerate battery voltages below 1.4 volts. As a result I have always quickly accumulated a lot of AA batteries with voltages around this level. When I counted the other day I had over 40 such batteries. Traditionally they have gone out with the recycling. This time however I decided to do a little experimenting to see if I could capture and use some of the remaining energy. A wealth of small DC to DC converters are available today with very impressive efficiency. My first step in doing some of my experiments will be to construct a couple of battery holders so I can put 10 of the AA batteries in series. This way I will have sufficient voltage available so that even a cheap 12 VDC to 5VDC converter will have enough room before we approach its drop out voltage. This should occur when the used batteries reach 0.8 volts and are truly ready for the recycling bin.

 

A search of the local hardware store revealed that 1/2 CPVC pipe had just about the correct inside diameter to serve as a battery tube. I also brought home 4 cap ends. Here is the results of a half hour of cutting and drilling.

 

image

One pipe cap is fitted with a spring to keep contact on the batteries and the other cap has a terminal that is made of a brass screw that has been flattened. The pipe caps friction fit onto the pipe tightly enough so that they do not have to be secured in any other way. Here are some detail pictures of the internal construction.

 

         imageimage

This is the negative end of the battery tube.

 

      imageimage

Here is the Positive end cap of the tube. The finished tubes (I made two) were 54 cm long. I attached appropriately colored test lead wire onto each cap and terminated the wire with a female banana binding post. I have a lot of adapters using banana plugs and jacks so this termination will allow me to easily attach to any test rig that I might set up.

 

The first simple experiment that I had in mind was to use the batteries to charge my cell phone. To do this I took apart a cheap Dollar Store 12 volt USB adapter and wired it so I could plug it into a bread board. I ran some bench tests on the small converter and determined that it was probably designed to deliver 500 mA. Here is a picture of the set up charging my cell phone. I have used one of the small voltmeters to monitor the output of the 5 volt converter. The second picture is a closeup of the small converter circuit.

 

      imageimage

 

After my phone charged I hooked up a small rechargeable battery pack. It was noted that the battery pack loaded the converter down more than recharging my phone had. Within 20 minutes the load lighten up and the voltage level came back up to the 5 volt area. Here is a picture of the set up. You will also note that in this photo I have been at work with the label machine as is customary for me.

 

image

 

I am not sure where I will go with this project from here but the continued interest in salvaging energy on the forum made me want to be prepared for a few experiments. I believe that I will use the battery packs to charge my phone for a few days but the size of the battery tubes and the mess of wires makes it unlikely that they will be allowed to stay on my bedside stand for too many days.

 

John

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 10 years ago +3
    In an Experiment suggested by friend Jan Cumps I have installed 10 AA batteries into one of my battery holders and I am going to analyze the energy output as the batteries go from their current approximate…
  • Jan Cumps
    Jan Cumps over 10 years ago +2
    A cool experiment, jw0752 . I don't think you'll be overly excited about the results though. Once a battery's voltage has dropped to say 1V, there's nada* energy left in there. You'll spend more personal…
  • jw0752
    jw0752 over 10 years ago in reply to Jan Cumps +1
    Hi Jan, You are correct. Trying to get the last drop of energy from batteries that have already dropped below a basic usable level is for the most part inconvenient, pointless, and a waste of time. However…
Parents
  • jw0752
    jw0752 over 10 years ago

    In an Experiment suggested by friend Jan Cumps I have installed 10 AA batteries into one of my battery holders and I am going to analyze the energy output as the batteries go from their current approximate 1.4 Volt level each down to approximately 0.8 Volts each. These are good quality batteries that have been rejected by my Canon camera as too low for use in the camera. I am going to use the small Chinese 12 volt DC to 5 volt DC converter mentioned previously in this post.

     

    image

     

    In order to calculate energy use value it is necessary to test and calculate the efficiency of this converter. I will use a bench power supply and an electronic load to calculate the voltage and current into the converter and compare it to the voltage and current output. If the Output power is divided by the Input power we will have the efficiency of the converter at that point. The efficiency will be calculated at two points. First I want to see what the efficiency is at the starting point of 14 volts. Next I want to test and calculate the efficiency when the batteries are down to the end of their lives at 8 volts. Here are the results of the test.

     

    Initial conditions:

    Input 13.9 volts  102 mA which equals 1.42 watts    Output  5.07 volts  200 mA which equals 1.01 watts.      1.01 watts divided by 1.42 watts is equal to 71% efficiency

     

    Final Conditions:

    Input  8 volts  160 mA which equals  1.28 watts     Output  4.57 volts  200 mA which equals 0.91 watts       0.91 watts divided by 1.28 watts is equal to 71% efficiency

     

    This shows that the efficiency of the DC to DC converter will be linear for our purposes over the test range. Note the Output has dropped in the final condition test from 5.07 volts to 4.57 volts. This is caused by the fact that an 8 volt input on the converter is encroaching on the drop out point. This converter needs at least 3.43 volts more input voltage than output to maintain its rated output.

     

    To save us from having to sit and watch meters for several hours as the voltage levels in the battery pack drop under the steady load of the Electronic Load I will be using a device that I used in a previous blog. I call it a Battery Duration Analyzer. The Analyzer works by monitoring a battery that is under load to an external load. The analyzer allows us to set a target voltage level. As long as our test battery's voltage remains above this target voltage the clock of the analyzer will continue to run. As soon as the test battery voltage drops below the target voltage the clock will stop. I will set the clock initially to 12:00 and then we will read the final time on the stopped clock when we return to the test at a later time.

     

    Here is a link to the original blog on the Battery Duration Analyzer:

     

    https://www.element14.com/community/people/jw0752/blog/2015/08/16/battle-of-the-batteries--e-vs-d-vs-bargain

     

    One of the critical parameters that can make a big difference in the out come of this experiment is the level of load that is placed on the battery pack. I have run some tests to determine the current that is drawn by my cell phone when it is recharging or 230 mA. This seems like a reasonable level and will actually translate the amount of time measured by the Analyzer into how long I could charge my phone on the bank of 10 used AA batteries. If we use our knowledge of the efficiency of the converter we can calculate a load of 230 mA on the output will translate to a load of 120 mA when the batteries begin at 14 volts and 200 mA when the voltage of the battery pack is at 8 volts.

     

    Here are some pictures of the test set up:

     

            imageimageimage

     

    Our target cut off voltage is 4.5 volts. The initial voltage of our converter under the 230 mA load is 4.96 Volts. The Fluke is displaying the voltage of the 10 series AA batteries under load 14.09 volts. At this point there is nothing left to do except wait. I returned to the test several times over the course of the day. When I checked on it at supper time it was over and this is the reading on the analyzer.

     

    image

     

    This tells me that the battery pack was able to supply enough power to keep the converter above 4.5 volts for 7 hours and 5 minutes. At the end and still under the load the batteries were showing only a fraction of a volt but when I removed the load from the battery pack it almost immediately jumped back to 10 volts. This would indicate to me that just as Jan Cumps had earlier indicated the drop off point is really 1 volt and not 0.8 volts per battery. If I had been watching the test I suspect the drop from 10 volts for the 10 pack to zero volts would have occurred in a matter of minutes.

     

    Now that we have the time of 7 hours and 5 minutes we can calculate the amount of energy used by the load with 5 volts and 230 mA for that period of time. This works out to 8.14 watt hours of energy. If we extrapolate back to the battery pack through the 71% efficiency of the converter this means that the battery pack actually supplied about 11.5 watt hours of energy in this time period.

     

    Watt Hours = Current X Voltage X Time

     

    When I consider that this is also equivalent to charging time on my cell phone it means that there is enough energy left in 10 otherwise used batteries to charge for 7 hours 5 minutes. On the other hand at the current cost for electricity in my area which is $0.13 per kWh I have about 0.15 cents of value. Doesn't seem worth the trouble to use the batteries and converter for only a fraction of a penny but now I know.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 10 years ago

    In an Experiment suggested by friend Jan Cumps I have installed 10 AA batteries into one of my battery holders and I am going to analyze the energy output as the batteries go from their current approximate 1.4 Volt level each down to approximately 0.8 Volts each. These are good quality batteries that have been rejected by my Canon camera as too low for use in the camera. I am going to use the small Chinese 12 volt DC to 5 volt DC converter mentioned previously in this post.

     

    image

     

    In order to calculate energy use value it is necessary to test and calculate the efficiency of this converter. I will use a bench power supply and an electronic load to calculate the voltage and current into the converter and compare it to the voltage and current output. If the Output power is divided by the Input power we will have the efficiency of the converter at that point. The efficiency will be calculated at two points. First I want to see what the efficiency is at the starting point of 14 volts. Next I want to test and calculate the efficiency when the batteries are down to the end of their lives at 8 volts. Here are the results of the test.

     

    Initial conditions:

    Input 13.9 volts  102 mA which equals 1.42 watts    Output  5.07 volts  200 mA which equals 1.01 watts.      1.01 watts divided by 1.42 watts is equal to 71% efficiency

     

    Final Conditions:

    Input  8 volts  160 mA which equals  1.28 watts     Output  4.57 volts  200 mA which equals 0.91 watts       0.91 watts divided by 1.28 watts is equal to 71% efficiency

     

    This shows that the efficiency of the DC to DC converter will be linear for our purposes over the test range. Note the Output has dropped in the final condition test from 5.07 volts to 4.57 volts. This is caused by the fact that an 8 volt input on the converter is encroaching on the drop out point. This converter needs at least 3.43 volts more input voltage than output to maintain its rated output.

     

    To save us from having to sit and watch meters for several hours as the voltage levels in the battery pack drop under the steady load of the Electronic Load I will be using a device that I used in a previous blog. I call it a Battery Duration Analyzer. The Analyzer works by monitoring a battery that is under load to an external load. The analyzer allows us to set a target voltage level. As long as our test battery's voltage remains above this target voltage the clock of the analyzer will continue to run. As soon as the test battery voltage drops below the target voltage the clock will stop. I will set the clock initially to 12:00 and then we will read the final time on the stopped clock when we return to the test at a later time.

     

    Here is a link to the original blog on the Battery Duration Analyzer:

     

    https://www.element14.com/community/people/jw0752/blog/2015/08/16/battle-of-the-batteries--e-vs-d-vs-bargain

     

    One of the critical parameters that can make a big difference in the out come of this experiment is the level of load that is placed on the battery pack. I have run some tests to determine the current that is drawn by my cell phone when it is recharging or 230 mA. This seems like a reasonable level and will actually translate the amount of time measured by the Analyzer into how long I could charge my phone on the bank of 10 used AA batteries. If we use our knowledge of the efficiency of the converter we can calculate a load of 230 mA on the output will translate to a load of 120 mA when the batteries begin at 14 volts and 200 mA when the voltage of the battery pack is at 8 volts.

     

    Here are some pictures of the test set up:

     

            imageimageimage

     

    Our target cut off voltage is 4.5 volts. The initial voltage of our converter under the 230 mA load is 4.96 Volts. The Fluke is displaying the voltage of the 10 series AA batteries under load 14.09 volts. At this point there is nothing left to do except wait. I returned to the test several times over the course of the day. When I checked on it at supper time it was over and this is the reading on the analyzer.

     

    image

     

    This tells me that the battery pack was able to supply enough power to keep the converter above 4.5 volts for 7 hours and 5 minutes. At the end and still under the load the batteries were showing only a fraction of a volt but when I removed the load from the battery pack it almost immediately jumped back to 10 volts. This would indicate to me that just as Jan Cumps had earlier indicated the drop off point is really 1 volt and not 0.8 volts per battery. If I had been watching the test I suspect the drop from 10 volts for the 10 pack to zero volts would have occurred in a matter of minutes.

     

    Now that we have the time of 7 hours and 5 minutes we can calculate the amount of energy used by the load with 5 volts and 230 mA for that period of time. This works out to 8.14 watt hours of energy. If we extrapolate back to the battery pack through the 71% efficiency of the converter this means that the battery pack actually supplied about 11.5 watt hours of energy in this time period.

     

    Watt Hours = Current X Voltage X Time

     

    When I consider that this is also equivalent to charging time on my cell phone it means that there is enough energy left in 10 otherwise used batteries to charge for 7 hours 5 minutes. On the other hand at the current cost for electricity in my area which is $0.13 per kWh I have about 0.15 cents of value. Doesn't seem worth the trouble to use the batteries and converter for only a fraction of a penny but now I know.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to jw0752

    John, the drop-off point of 0.8 is more realistic than 1 V. I typed 1 V out of mental lazyness image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 10 years ago in reply to jw0752

    Good work John,

    When designing battery operated devices, it is useful to keep in mind that alkaline batteries supply useful energy down to half their fresh voltage. And when drawing significant current, their output voltage sags.

    Another point about alkaline batteries - when they get cold (below zero C) their apparent capacity drops dramatically (to less than 40% of normal capacity). But a battery that got depleted at cold temperature will regain its normal remaining capacity when it is warmed up.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago in reply to dougw

    Hi Douglas,

     

    You just gave me an interesting idea for heating up older alkaline batteries to excite them to produce more current.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 10 years ago in reply to DAB

    They do work a bit better when hotter, but mainly when they get frozen it inhibits the physical movement of ions, at least that is how I visualize it. It seems some areas or paths are not completely locked up when frozen, although some are, so perhaps the electrolyte is not perfectly homogeneous. If you could come up with a way to make the electrolyte more homogeneous you might see a major improvement in alkaline batteries. Even when hot there would be less internal resistance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to DAB

    DAB, we should in that case measure if we're not putting more energy in the heating up than what we get out of it.

    It would be a nice test though.

     

    I think I'll have to work on a configurable load with power measurement.