Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog I Need an Extra Finger
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 10 Sep 2014 6:09 AM Date Created
  • Views 2032 views
  • Likes 4 likes
  • Comments 26 comments
Related
Recommended

I Need an Extra Finger

jw0752
jw0752
10 Sep 2014

Since I retired a couple years ago I have returned to my life long interest in electronics. What I have discovered is that I had not kept up with the technology. The manageable, through the hole, components that I was familiar with in the past have been replaced by something that is very small and solders directly to the surface of the board. Not wanting to miss out on playing with some of these really neat goodies I decided to begin to acquaint myself with the components and the new techniques I would need to learn. While I have been soldering for 55+ years I have seldom had to deal with the soldering of leads so closely spaced. To assist in trying the surface mounted chips I bought some Capital Advanced adapter boards from Newark Electronics and proceeded to attempt to solder the chips to them. The most difficult part was keeping the chip in place while I soldered the first leg. I was explaining to my very supportive wife how difficult it was not to disturb the position of the chip while soldering and in her usual intuitive way she volunteered to hold the chip with her finger while I soldered it. ( At this point she had not seen the size of the chip in question ,1.5mm x 2.5mm) While it was not practical for her to hold it, as usual she was right, what I needed was an extra finger.

 

I got together the following materials:

 

30 cm of bare 12 gauge copper wire

4 screws

piece of spring

6 cm of 3 mm brass tubing

 

20 minutes later after bending and soldering the pieces together I had cobbled together THE FINGER

 

image

 

I got one of the Capital Advance boards out and an LM 3410 LED driver that I wanted to try out.

 

image

 

I placed the IC on the board under THE FINGER. Once it was held down by the finger I made the minor adjustments needed to position it properly.

 

image

 

Now all that was left was the still challenging job of soldering the legs of the LM 3410 to the board.

 

Final product:

 

image

 

Now all that was left was to plug the LM 3410 LED Driver into a breadboard and wire up the circuit to see if it really would drive 5 series LEDs off of a 3.3 volt supply as advertised.

 

Not much to look at but it works as advertised.

 

image

 

Good Night Guys 1:10 AM

 

 

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 12 years ago in reply to fvan +3
    "The Finger" a la Frederick Or better for soldering access John
  • mcb1
    mcb1 over 12 years ago in reply to shabaz +1
    Ah yes but then we John describes using it to solder the "latestwzizbangIC" the headline might read. John gives "latestwzizbangIC" the finger probably not the headline he wants.... Mark
  • jw0752
    jw0752 over 12 years ago in reply to DAB +1
    Thanks DAB - By the way I have on my to do list getting a copy of your book. It sounds very interesting. John
Parents
  • michaelkellett
    michaelkellett over 12 years ago

    A long time ago (about 1994) when I had multiple minions I got one to make me a similar device: a spring steel prong fixed to a round metal base. About 12 years ago when I left to work on my own one of my last acts was to scrounge some of the spring steel wire with which I made the thing in the picture. (The third hand thingy came from a car boot sale.)

     

    I don't use it so much now for small parts - I often tack one leg down (using the microscope to see what I'm doing) but I still use it for ICs with more than 8 legs.

     

    image

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 12 years ago in reply to michaelkellett

    Hi Michael, The reach on yours looks much better for reaching into existing boards.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 12 years ago in reply to michaelkellett

    Hi Michael, The reach on yours looks much better for reaching into existing boards.

    John