Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog I Need an Extra Finger
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 10 Sep 2014 6:09 AM Date Created
  • Views 1987 views
  • Likes 4 likes
  • Comments 26 comments
Related
Recommended

I Need an Extra Finger

jw0752
jw0752
10 Sep 2014

Since I retired a couple years ago I have returned to my life long interest in electronics. What I have discovered is that I had not kept up with the technology. The manageable, through the hole, components that I was familiar with in the past have been replaced by something that is very small and solders directly to the surface of the board. Not wanting to miss out on playing with some of these really neat goodies I decided to begin to acquaint myself with the components and the new techniques I would need to learn. While I have been soldering for 55+ years I have seldom had to deal with the soldering of leads so closely spaced. To assist in trying the surface mounted chips I bought some Capital Advanced adapter boards from Newark Electronics and proceeded to attempt to solder the chips to them. The most difficult part was keeping the chip in place while I soldered the first leg. I was explaining to my very supportive wife how difficult it was not to disturb the position of the chip while soldering and in her usual intuitive way she volunteered to hold the chip with her finger while I soldered it. ( At this point she had not seen the size of the chip in question ,1.5mm x 2.5mm) While it was not practical for her to hold it, as usual she was right, what I needed was an extra finger.

 

I got together the following materials:

 

30 cm of bare 12 gauge copper wire

4 screws

piece of spring

6 cm of 3 mm brass tubing

 

20 minutes later after bending and soldering the pieces together I had cobbled together THE FINGER

 

image

 

I got one of the Capital Advance boards out and an LM 3410 LED driver that I wanted to try out.

 

image

 

I placed the IC on the board under THE FINGER. Once it was held down by the finger I made the minor adjustments needed to position it properly.

 

image

 

Now all that was left was the still challenging job of soldering the legs of the LM 3410 to the board.

 

Final product:

 

image

 

Now all that was left was to plug the LM 3410 LED Driver into a breadboard and wire up the circuit to see if it really would drive 5 series LEDs off of a 3.3 volt supply as advertised.

 

Not much to look at but it works as advertised.

 

image

 

Good Night Guys 1:10 AM

 

 

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 11 years ago in reply to fvan +3
    "The Finger" a la Frederick Or better for soldering access John
  • mcb1
    mcb1 over 11 years ago in reply to shabaz +1
    Ah yes but then we John describes using it to solder the "latestwzizbangIC" the headline might read. John gives "latestwzizbangIC" the finger probably not the headline he wants.... Mark
  • jw0752
    jw0752 over 11 years ago in reply to DAB +1
    Thanks DAB - By the way I have on my to do list getting a copy of your book. It sounds very interesting. John
  • jw0752
    jw0752 over 11 years ago in reply to fvan

    Thanks Frederick - That is a very good observation and in fact might be an easy way to make one. One would have to modify the kill bar so that it wasn't in the way when you wanted to solder. I will have to experiment with a mouse trap when I get the time.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago

    It's like a mouse trap for tiny ICs image well done!

     

    Frederick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to mcb1

    Very good point!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to shabaz

    Ah yes but then we John describes using it to solder the "latestwzizbangIC" the headline might read.

     

    John gives "latestwzizbangIC" the finger

    probably not the headline he wants.... image

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    That looks very effective! It should now officially be THE FINGERTm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>