Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Nominal VS Actual Power of USB Power Pack
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 21 Nov 2015 6:55 AM Date Created
  • Views 1030 views
  • Likes 3 likes
  • Comments 8 comments
  • usb_power_pack
  • mah
  • battery_capacity
Related
Recommended

Nominal VS Actual Power of USB Power Pack

jw0752
jw0752
21 Nov 2015

The other day I was reading a blog by raspjoenoob   about trying to run a Raspberry Pi with a USB Power Pack.   USB POWER BANK // PORTABLE POWER SUPPLY  Later the same day I was in Walmart where I noticed they had 2200 mAh Power Packs on sale for $5.00. I bought 2 of these with the intention to test them to see just how much power they would actually deliver.

 

image

A while back I built a little battery duration tester that is used in conjunction with a Load Unit to test battery energy available under different loading conditions.

Battle of the Batteries - E*** vs D*** vs Bargain


image


These are better pictures of the USB Power Packs that will be evaluated. The specifications say that they are 5 volts in for charging and that they will supply 5 volts output at 1 Amp. The power rating was of course 2200 mAh.


    imageimage


I alternated between the two units in my tests. Each time the Power Pack was allowed to fully charge before testing. The units were tested under loads of 250 mA, 500 mA, 750 mA, 870 mA, and 1000 mA. In each test the unit was run until the internal circuitry of the Power Pack disconnected the unit from the load due to low battery condition. The time on the clock was then noted and a calculation of milli Amp hours was calculated. Here is how the test setup looked:


     image image

 

As I have seen before in battery tests the Power Packs were able to do slightly better under a low load than they did at the upper end of their rated load capability. Of course we are not dealing with a pure battery situation here as there is internal monitoring circuitry as well as a boost converter to deliver the nominal 5 volt output. Quite a neat little package all things considered. I will post a graph of the results of the tests below. The best power out that I was able to obtain was 1388 mAh under a continuous load of 250 mA. This level was very linear until the load got in excess of 750 mA at which point it dropped quite quickly until it was down to 750 mAh at it full rated 1000 mA output. Here is the Graph:


image


Obviously at $5.00 and clearly marked as Made in China this battery pack was not top of the line quality. It would be interesting however to see how well an expensive top brand would stack up against it.. When we tested the Alkaline AA batteries we were surprised to find little to no difference between the top brands and the dollar store cheapies. If I can get my hands on a better unit with the same specifications I will post an addendum to this blog.


John

.



.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +2
    Excellent job John. You learn quickly in the engineering world that stated capabilities are often NOT met by the devices. On one large project I identified a problem with the selected processor and predicted…
  • jw0752
    jw0752 over 10 years ago in reply to mcb1 +2
    Thanks Mark, Of course one of the main reasons for carrying out such an experiment is to be able to make predictions about battery life in more practical situations. As a follow up test I decided to set…
  • mcb1
    mcb1 over 10 years ago in reply to jw0752 +2
    That's not bad since I suspect there is some peaking of the current. It would be interesting to see if the performance changes over several cycles of the pack. In theory it shouldn't but I'm told that…
Parents
  • DAB
    DAB over 10 years ago

    Excellent job John.

     

    You learn quickly in the engineering world that stated capabilities are often NOT met by the devices.

     

    On one large project I identified a problem with the selected processor and predicted that they would only support about 80% of the stated capability.

    The VP of the primary contractor got up and stated that THEY were satisfied with the stated capabilities.

     

    Six months later I went for a check up visit only to have the programmers complain about how the processor were only about 80% of their promised capabilities.  I just smiled.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 10 years ago

    Excellent job John.

     

    You learn quickly in the engineering world that stated capabilities are often NOT met by the devices.

     

    On one large project I identified a problem with the selected processor and predicted that they would only support about 80% of the stated capability.

    The VP of the primary contractor got up and stated that THEY were satisfied with the stated capabilities.

     

    Six months later I went for a check up visit only to have the programmers complain about how the processor were only about 80% of their promised capabilities.  I just smiled.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 10 years ago in reply to DAB

    Yes when the bosses or the customers are too focused to listen all that is left is to smile. I have done quite a bit of smiling too over the years. image

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to DAB

    I find it is those who are least qualified that read the hype and won't listen to the advise from more experienced people.

    One the other day said it was likely it would come full circle, and we laughed at him and told him we had been working here long enough to have seen that ... several times.

     

    Fortunately they tend to last 4 years, although we have some that are overdue to move.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago in reply to mcb1

    Hi Mark,

     

    Yes the unwary get fooled like this often.

    The term "Trust but verify" needs to be every engineers byword.

    Marketing brochures are aimed at selling, sometimes they lie.  No you should not be shocked.

     

    When possible, you test, just like @John Wiltrout did and get the real parameters.

     

    DAB