Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Not Everything is Electronics
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 23 Oct 2018 4:07 AM Date Created
  • Views 1050 views
  • Likes 13 likes
  • Comments 7 comments
  • dual_601
Related
Recommended

Not Everything is Electronics

jw0752
jw0752
23 Oct 2018

I have had a Dual 601 turntable for many years, perhaps 50, and it used to work great. Sometime ago it started acting strange as the motor became unstable and would power up and lock on a higher RPM than proper. From the information on the internet it seemed that this was a design problem and would not be easily solved. I tried to fix it anyway. I tried external electronics to see if I could make it come up to the proper speed. I even messed with the pole spacing on the stater but the internet had been correct and it wasn't going to be easy. A friend of mine Eric repairs turntables in his spare time and he offered to watch for a motor from a different model that could be installed with a little modification. When a motor was finally located Eric installed it and brought the table back to me. He mentioned to me at the time that there was a small ferrule that was in bad shape and may fail soon but I didn't pay much attention at the time. The turntable sat for about a month until yesterday when I finally got around to hooking it up and trying it out. The new motor worked like a charm and the speed was solid. When the tone arm got to the center of the record it picked up as expected but it did not return to its rest. It just continued to cycle through lifting and setting back onto the record.

 

I decided to open up the changer and see what was not working. I had the turntable up on pop cans so I could watch the mechanism as it reacted to the end of the record. I turned the table slowly by hand so I could watch what was taking place. There was a small brown ferrule that had cracked in two and was just held in place by the grease on it.

 

image

 

It had a diameter of 0.15 inches a thickness of 0.15 inches and the diameter of the shaft it was mounted to was 0.075 inches. When the record is at the end, the mechanism applies pressure to this ferrule and uses the friction of the ferrule against a moving plate to move the tone arm back to its rest. After some consideration I decided to try to use a nylon screw as the raw material for a new ferrule. The nylon would be an easy material to cut and drill. After a little experimentation and 2 failed prototypes I finally got what I was looking for. Here is the new ferrule mounted to the post that moves the tine arm back to its rest.

 

image

 

If you notice you will see the pop can supporting the turntable so that the mechanism is able to be watched. 50 years ago when I serviced turntable for a living and I had a jig made up so that I could suspend the turntables from the ceiling and work underneath them much as a garage mechanic works under the cars. The trouble with working on turntables is that you can't turn them on their sides or upside down to watch what is going on and it is always difficult to get the vantage point needed to see what isn't doing what it is suppose to. This was a relatively easy fix and it was fun to refresh old memories.

 

Here is the finished product doing what it is supposed to do - playing a Swedish group singing in Spanish to my old ears. Gracias Por La Musica.

 

image

 

John

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 7 years ago +5
    Nice fix. I've had a Dual Turntable for ... umm 40 years?? ... It hasn't been used for so long I'm certain the belt will need replacing. I've resisted throwing it out as once it's gone you can;t go get…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to mcb1 +4
    I typically use a tiny bit of empty ballpoint ink container. I pais most of my lab components and records by buying defect Duals, fixing, then selling on the internet. it’s never the electronics. always…
  • jw0752
    jw0752 over 7 years ago in reply to shabaz +3
    Vacuum cleaners usually have stacked aluminum turbine blades inside a housing. Water has 833 times the density of air so you can imagine the force that is put on the blades when they get a feed of water…
Parents
  • mcb1
    mcb1 over 7 years ago

    Nice fix.

    I've had a Dual Turntable for ... umm 40 years?? ...

     

    It hasn't been used for so long I'm certain the belt will need replacing.

    I've resisted throwing it out as once it's gone you can;t go get another one.

     

    Mark

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 7 years ago

    Nice fix.

    I've had a Dual Turntable for ... umm 40 years?? ...

     

    It hasn't been used for so long I'm certain the belt will need replacing.

    I've resisted throwing it out as once it's gone you can;t go get another one.

     

    Mark

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to mcb1

    I typically use a tiny bit of empty ballpoint ink container. I pais most of my lab components and records by buying defect Duals, fixing, then selling on the internet.

     

    it’s never the electronics. always sticky grease and deteriorated steuerpimpel.

    • Cancel
    • Vote Up +4 Vote Down