Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Repairing an Inexpensive Scope Probe
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 18 Aug 2020 9:22 PM Date Created
  • Views 4366 views
  • Likes 10 likes
  • Comments 5 comments
  • oscilloscope_probe
Related
Recommended

Repairing an Inexpensive Scope Probe

jw0752
jw0752
18 Aug 2020

Recently my scope and I had an unfortunate encounter with some high voltage and it left me with one channel out. I am slowly working through the process to see if I can fix the scope. I will blog about my journey at a later date whether I can fix it or not. Among the damage the high voltage caused was the loss of the 1X circuit in the probe cord set.

 

image

 

This is an inexpensive 80 MHz Hantek probe and after the high voltage experience the 1X  10X switch had no effect. My first thought was to junk the probe and see if I could use the wire with the BNC connector for another purpose. The probe itself looked like it was molded in plastic and as I sat trying to decide how to cut it apart I noticed that the strain relief on the wire would slide off the handpiece. Next I noticed that the plastic handpiece would also slide off the internal barrel. Little by little with lots of pulling and I admit even some prying I got the handpiece apart.

 

image

 

So far everything that I had done to the handpiece was reversible. I measured all the components and the only problem was the little switch itself.

 

image

 

When examined closely the switch looked like it could be disassembled by opening a metal cover clip. I removed the clip and took out the white plastic slide with the metal contact fingers. Looking inside the switch I could see the black burn caused by a high voltage electric arc.

 

imageimage

 

It is hard to see the burn spot inside the switch but it is on the left side. I cleaned the wiper contacts and the contacts inside the switch body using a little De-ox-id on some paper towel bits. The switch snapped back together and worked like new. The metal sheath that covers the circuit board and carries the ground forward to the alligator clip was a little loose when pushed back together as it was not designed to be repaired so I had to use a sharp center punch to make it tight. The plastic pieces all slid back into place and when fully reassembled the probe worked just like new.

 

It was fun to see what was inside an oscilloscope probe and it was even more fun to fix something that was never designed to be fixed.

 

John

  • Sign in to reply

Top Comments

  • genebren
    genebren over 6 years ago +3
    Nice repair job John! I never get that adventurous with my broken gear. I usually grumble a bit and then buy a new one. It is good to see someone do the right thing and fix/repair the problem. Well done…
  • jw0752
    jw0752 over 6 years ago in reply to dubbie +3
    Hi Dubbie, If I remember correctly the exact formula is: Prying = Breaking + Bleeding John
  • DAB
    DAB over 6 years ago +2
    Good job John. You were lucky that it was only a carbon score problem. You usually lose the input channel on the scope unless there is some protection circuitry built into the design. DAB
Parents
  • dubbie
    dubbie over 6 years ago

    John,

     

    There's nothing wrong with a little 'prying' now and then, although I must admit that when I try any prying it usually results in some breaking as well.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago in reply to dubbie

    Hi Dubbie,

     

    If I remember correctly the exact formula is:

     

    Prying = Breaking + Bleeding

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 6 years ago in reply to dubbie

    Hi Dubbie,

     

    If I remember correctly the exact formula is:

     

    Prying = Breaking + Bleeding

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dubbie
    dubbie over 6 years ago in reply to jw0752

    John,

     

    You're quite right, there is often pleeding, although I've taken to wearing glues more now (not for electronics) and that has definately reduced the bleedingi

     

    Dubbie