Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Repurposing Salvaged Circuit Board
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 5 Aug 2019 5:28 AM Date Created
  • Views 2470 views
  • Likes 12 likes
  • Comments 15 comments
  • bench power supply
Related
Recommended

Repurposing Salvaged Circuit Board

jw0752
jw0752
5 Aug 2019

I recently bought a power control module from a Chinese source. All I needed to do was provide the input power, up to 75 volts at 12 Amps and the module would allow me to output a digitally controlled voltage or current up to 60 Volts and 12 Amps. I will not go into the assembly of the unit as I have perhaps done one too many power supply builds in my blog already.

 

I had on the shelf a perfect candidate for an enclosure for this unit. It was really heavy duty with an already available fused and switched AC input. It had a 12 volt thermally controlled fan and it looked very nice. The only stumbling block (and there is always one) was the front panel of the enclosure was special purpose for the original application and it was contoured.

 

image

 

With the way that the front panel fit on the unit it was not going to be practical to abandon it altogether. This project has been on the shelf for a couple weeks while I mulled over what my approach was going to be to make this sculpted panel suitable for me to adapt one of my traditional flat control panels to the front of the unit.

 

Finally I decided to launch into it and with the unit in a vise I took a carpenters hand saw and sawed the contours of the front panel as flat as I could while still retaining the basic structure of the mount. My new front panel did mount to the flattened original panel and the unit worked well. Unfortunately I could not get past the cosmetics of the appearance where the new flat  front did  not integrate totally with the contours that were left on the original panel. Perhaps you can see a little of the problem in this picture:

 

image

 

The next step I took was to try to fill in and bridge the gaps and mismatch with a white silicone sealer. While this worked to fill in the holes and gaps it did nothing to improve the cosmetics. The silicone is very hard to work with if one is looking for any kind of a professional appearance. When it was done it looked like crap and I knew there had to be at least one more step to make it look finished. I thought that maybe I would make a bezel out of copper or brass. When I did not have sufficient pieces of either of these in the shop the box of scrap circuit boards caught my eye. You may have guessed that when I salvage all the components from a circuit board I seldom throw the board itself away. The circuit board material makes very good structural material for building other things.

 

I decided that it would be a unique solution to build the decorative bezel for the power supply from strips of salvage circuit board.

 

Here is the finished power supply with a circuit board decorative bezel.

 

   imageimage

 

I haven't quite gotten used to its appearance yet but it fits well with my collection of other unusual pieces of test equipment.

 

Incidentally the 60 Volt 12 Amp marking is a lie. The Chinese module has this for a rating and I have no way to test if it is true or not. I was only able to come up with a power transformer than can deliver 180 Watts of power to the control module. Therefore when I have the unit powered and loaded to the max I can get about 45 Volts at 4 Amps. Until I can find a higher VA transformer that will still fit in the enclosure the current one will have to do. The fact is that I seldom have an application for the higher voltage and current that this unit can provide anyway. The main purpose of the build was to experiment with the Chinese Digital power supply control module.

 

John

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago in reply to Andrew J +7
    Hi Andrew! This one might be more interesting actually, it's the same price, but with colour pellets too (although, it's all in a bag, whereas the other one is in a more convenient pot): https://www.amazon…
  • shabaz
    shabaz over 7 years ago +6
    Hi John, Very nice looking PSU : ) Although you didn't need it here, I found a material recently, that may interest you. It's possibly well-known, but it was new to me. It's called ' polydoh mouldable…
  • shabaz
    shabaz over 6 years ago in reply to jw0752 +4
    Hi John, The Polydoh came in handy today. The washing machine debris catcher has a plastic knob which is near-impossible to open by hand, since it has very little to grip on, and is very stiff due to rubber…
  • jw0752
    jw0752 over 7 years ago in reply to genebren

    Hi Gene,

     

    I have a lot of fun putting pieces together and making something new out of them. I guess I am a little like a cat lady with the cats replaced with power supplies.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to ralphjy

    Hi Ralph,

     

    I drilled clearance holes in the boards and pilot holes in the bezel and attached the board pieces using self tapping plastic screws.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    John,

     

    Another nice power supply for your already well equipped shop.  I really like the creativity that you applied to your build.  It is good when you can think outside of the box, while you are working on making your box work.

     

    Well done!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 7 years ago

    Very unique solution.  What did you use to attach the PCBs to the bezel?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago

    Nice solution!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<