Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Reverse Engineering an Alarm Siren Module
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 17 Jan 2015 7:42 AM Date Created
  • Views 2866 views
  • Likes 4 likes
  • Comments 23 comments
  • circuit_board_to_schematic
  • reverse_engineering
Related
Recommended

Reverse Engineering an Alarm Siren Module

jw0752
jw0752
17 Jan 2015

One of the things that I enjoy doing is taking a small one or two sided circuit board and creating a schematic of it. Today I have a circuit board from a 105 db piezo siren for which I am going to create a schematic.  Here is the Module.

 

       imageimage

 

 

The first step is to get some paper and choose a starting point. In this case I picked the output transformer and then worked my way back. As you can imagine the board must be flipped back and forth and ones perspective must constantly shift from topside to mirror image and back. The resistors must be read and measured if they can not be seen. This is also done with the capacitors. On this board the identification of the small green mylars were face to face and so one had to be removed to determine the value. When the rough draft of the schematic is finished it is never very pretty. Here is my rough draft.

 

 

image

 

This is obviously not very good or very clear. In order to not put too many line on this draft the ground line was replaced with ground symbols and one junction point was labeled #3 and a second junction point was labeled *. What happened to #1 and #2? I am not sure it just seemed ok at the time to call them * and #3. After the rough draft is finished I use it to produce a more conventional looking hand done draft. Here is what it looks like after it has been cleaned up.

 

 

image

 

 

This one while still not very neat at least looks more conventional and at this point I also add component numbering. I also take close up photos of the board and label the components to match the schematic. This serves to tie things together and to make certain that I have not left anything out of my schematic. Here are the pictures and labels that correspond to the schematic.

 

 

     imageimage

 

 

Now I take all the drafts and produce a CAD drawing of the schematic to complete my file on this particular circuit.

 

 

 

image

 

This process is good exercise for the brain and gives me a very good understanding of the circuit by the time I have finished.

 

John

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 11 years ago in reply to mcb1 +2
    Yes Mark you are correct on a number of counts. With the advent of multi-layer boards and SMD parts I can see the end of the trail for people like myself who like to repair circuit boards. Through the…
  • jw0752
    jw0752 over 11 years ago in reply to clem57 +1
    Hi Clem, The circuit came from a Radio Shack Alarm Siren that I was using in one of my inventions. Something went wrong and it fried. I fixed it with a new filter cap and new output transistor before I…
  • shabaz
    shabaz over 11 years ago +1
    Hi John, Thanks for the great blog post : ) This is nice, and also probably goes to show that when cost-saving, transistors may end up cheaper than a 555 circuit by a few pence/cents, and hence make more…
  • mcb1
    mcb1 over 11 years ago in reply to clem57

    Clem

    Which bit did you miss ...

    Today I have a circuit board from a 105 db piezo siren for which I am going to create a schematic.  Here is the Module.

     

    It's one of those things that make a REALLY LOUD noise when you apply power to it.

    They come in different forms (I'm guessing this looks like a horn speaker) and are mostly used with burglar alarms.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Hi John,

     

    Nice post.

     

    I have done more of these reverse engineering tasks than I care to remember.

     

    I agree that it is an excellent practice to learn.  There are a lot of secrets hidden in some circuits and you are always rewarded by figuring them out.

     

    One of my dream projects is to have and system that you can just take front and back pictures of the board in question and have a circuit diagram drawn automatically.

    It would be a great task for a collaborative project.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago

    @John Wiltrout

         Did you know what this board does? This does not seem too obvious to me

     

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to D_Hersey

    Hi Don, As usual your observations are very pertinent. LTSpice is on my bucket list but as of now I have no experience with it. The transformer has a DC resistance ratio of approximately 1 to 100 Primary to Secondary. I put a load potentiometer in series with an IR drop and hooked up my scope to look at the AXB of the voltages across the load and the IR drop. I then adjusted the load for max AXB output. Next I measured the DC resistance of the load and found it to be 5K. Next I estimated the primary impedance to be in the same ratio to the secondary impedance as the DC resistance of the transformer. I am assuming that I also have some knowledge deficiencies in this area as well.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    Also, I am a little confused by your documentation of the transformer.  Are you describing the turns ratio, or the square of the turns ratio, the impedance ratio?

     

    And, BTW, could you model the electrical characteristics of the load as well?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>