Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Shop Tips - Bread Board Alligator Clips
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 2 Sep 2019 3:32 AM Date Created
  • Views 5028 views
  • Likes 11 likes
  • Comments 19 comments
  • bread_board_cables
  • shop_tips
Related
Recommended

Shop Tips - Bread Board Alligator Clips

jw0752
jw0752
2 Sep 2019

Recently I was working on a bread board circuit provided by jc2048 . One of the things that I find very convenient when wiring up a bread board are short wires with an alligator clip on one end and a bread board pin on the other. I use these cables to hook up peripheral meters, sensors, and actuators to the bread board circuit. In the past I have taken cheap alligator to alligator jumper cables, cut them in half and just added a bread board pin to the cut end. While this works the cables do not turn out to be long term durable or dependable. For one thing the wires of these cables are seldom soldered to the alligator clip. Instead the copper wire (what little there is) is folded back alongside the outer insulation and then the alligator clip is crimped down on the wire and the insulation. I have taken brand new jumper cable made like this and had resistance readings of 1 Ohm from alligator to alligator.

 

After fighting with my old patch wires on this last bread board I decided to take the time and make up some that would be of better quality and more durable. I began the project with a bag of the same old cheap jumper cables.

 

image

 

This would be the source of Alligator clips and covers for the new Bread Board Clips. I will be using special wire that I have salvaged from dental handpiece cords for the wire in the new BB patch cables. This wires has an overall small diameter but has an over sized multi strand conductor. One day I took the time to count the strands on one of these type of wires and there was over a hundred strands. This many strands makes the wire very flexible and the over all gauge allows the wire to carry a reasonable current. In the dental application this type of wire will often carry 2 or 3 amps. Here is a picture of the original jumper cable wire along side one of the special wires.

 

image

 

The alligator clips that I had salvaged from the cheap jumper cables were next soldered to the high strand wire and the crimp at the back of the alligator clip was used as intended to provide a strain relief on the wire. As much as possible I try to use matching colors in the construction of the BB clips. At 70 there are enough things to confuse me when I build without any color confusion.

 

For the pin end of the cables I will take standard square pin, breakable, male headers and add them to the free end of the wire. The solder is covered with a short piece of heat shrink which serves as an insulator and also a strain relief so that the wire is not stressed at the solder joint.

 

Here is what the bag of jumper cables has turned into:

 

   imageimage

 

With the new alligator patch cables in hand I set up the experiment that had inspired me to make them.

 

image

 

The flexibility of the cables make it easy to set up and position. My old cables were constantly applying torque to the circuit board in one direction or another making it difficult to get things to stay where I wanted them. The net out of pocket cost of this project was under $3.

 

John

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +8
    Hi John, They look great! I have soldered the alligator clips to the wire that comes with them in the past, but it really is poor quality wire. Do you find this approach for the pin end: For the pin end…
  • dougw
    dougw over 7 years ago +7
    Great idea John. One thing I find frustrating is how slippery some of those sleeves are on the alligator clips. It is hard to get your fingers squeezing in the right direction on some of them. I have some…
  • Gough Lui
    Gough Lui over 7 years ago +6
    Doing some searching on element14 - it seems it is possible to buy such wire in the Hook-Up wire section. One just has to be careful to filter by gauge and strand counts to find something decently flexible…
  • jw0752
    jw0752 over 7 years ago in reply to fmilburn

    Hi Frank,

    I have not used the crimp pins but there is no reason that they would not be just as good. For me the header pins are cheap and convenient.

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi John,

     

    Up until recently, I still had a few of those alligator cables, they look like an identical set, that I think I'd purchased from Radio Shack! : ) They lasted a long time.

    Since then I've just been just purchasing the occasional solo alligator clips to attach to wires.

    The slipping issue you and Doug mention was the reason I didn't end up getting any PVC boots for the bare alligator clips, but then they're a shorting risk : (

    These are ok-ish: https://www.aliexpress.com/item/32813835739.html?spm=a2g0s.9042311.0.0.27424c4dEPvGRZ

    (not designed for crimping/soldering, but they are solderable, if you use heatshrink to provide the final strain relief, because nothing grips that).

    For wire, I've been using some flexi stuff from one of the UK consumer Farnell stores (CPC), I think its construction is very close to the dental wires you describe, with about 100 fine strands, but it's very low-cost (it is PVC insulated), and only available in red and black unlike the ones you've found.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago

    Doing some searching on element14 - it seems it is possible to buy such wire in the Hook-Up wire section. One just has to be careful to filter by gauge and strand counts to find something decently flexible (i.e. lots of fine strands). I remember in the past, some people used to refer to these as "test lead wire" as many multimeter leads (should) be made with such wire with nice silicone insulation.

     

    I did a search on the AU site with wire gauges 16-28AWG and >100 strands:

    https://au.element14.com/w/c/cable-wire-cable-assemblies/hook-up-wire/prl/results?wire-gauge=16awg|17awg|18awg|19awg|20a…

     

    As expected, prices aren't cheap but not as dear as I would have expected. Staubli seems to dominate the results with their Hi-Flex and Super-Flex range of wire.

     

    - Gough

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago

    Hi John,

     

    They look great!  I have soldered the alligator clips to the wire that comes with them in the past, but it really is poor quality wire.  Do you find this approach for the pin end:

    For the pin end of the cables I will take standard square pin, breakable, male headers and add them to the free end of the wire

    better than crimping so called Dupont male pins?  I had not thought to try your approach.

     

    Frank

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to dougw

    I was thinking of a liner that would act like a stabilizer between the smooth metal of the clip and the plastic insulator. The only material that comes immediately to mind is tack cloth which is used in wood working. I will have to get some and run a few tests. I do not believe fusing the insulator to the wire would work as the wire isn't stable enough.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>