Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Shop Tips - Bread Board Alligator Clips
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 2 Sep 2019 3:32 AM Date Created
  • Views 5029 views
  • Likes 11 likes
  • Comments 19 comments
  • bread_board_cables
  • shop_tips
Related
Recommended

Shop Tips - Bread Board Alligator Clips

jw0752
jw0752
2 Sep 2019

Recently I was working on a bread board circuit provided by jc2048 . One of the things that I find very convenient when wiring up a bread board are short wires with an alligator clip on one end and a bread board pin on the other. I use these cables to hook up peripheral meters, sensors, and actuators to the bread board circuit. In the past I have taken cheap alligator to alligator jumper cables, cut them in half and just added a bread board pin to the cut end. While this works the cables do not turn out to be long term durable or dependable. For one thing the wires of these cables are seldom soldered to the alligator clip. Instead the copper wire (what little there is) is folded back alongside the outer insulation and then the alligator clip is crimped down on the wire and the insulation. I have taken brand new jumper cable made like this and had resistance readings of 1 Ohm from alligator to alligator.

 

After fighting with my old patch wires on this last bread board I decided to take the time and make up some that would be of better quality and more durable. I began the project with a bag of the same old cheap jumper cables.

 

image

 

This would be the source of Alligator clips and covers for the new Bread Board Clips. I will be using special wire that I have salvaged from dental handpiece cords for the wire in the new BB patch cables. This wires has an overall small diameter but has an over sized multi strand conductor. One day I took the time to count the strands on one of these type of wires and there was over a hundred strands. This many strands makes the wire very flexible and the over all gauge allows the wire to carry a reasonable current. In the dental application this type of wire will often carry 2 or 3 amps. Here is a picture of the original jumper cable wire along side one of the special wires.

 

image

 

The alligator clips that I had salvaged from the cheap jumper cables were next soldered to the high strand wire and the crimp at the back of the alligator clip was used as intended to provide a strain relief on the wire. As much as possible I try to use matching colors in the construction of the BB clips. At 70 there are enough things to confuse me when I build without any color confusion.

 

For the pin end of the cables I will take standard square pin, breakable, male headers and add them to the free end of the wire. The solder is covered with a short piece of heat shrink which serves as an insulator and also a strain relief so that the wire is not stressed at the solder joint.

 

Here is what the bag of jumper cables has turned into:

 

   imageimage

 

With the new alligator patch cables in hand I set up the experiment that had inspired me to make them.

 

image

 

The flexibility of the cables make it easy to set up and position. My old cables were constantly applying torque to the circuit board in one direction or another making it difficult to get things to stay where I wanted them. The net out of pocket cost of this project was under $3.

 

John

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +8
    Hi John, They look great! I have soldered the alligator clips to the wire that comes with them in the past, but it really is poor quality wire. Do you find this approach for the pin end: For the pin end…
  • dougw
    dougw over 7 years ago +7
    Great idea John. One thing I find frustrating is how slippery some of those sleeves are on the alligator clips. It is hard to get your fingers squeezing in the right direction on some of them. I have some…
  • Gough Lui
    Gough Lui over 7 years ago +6
    Doing some searching on element14 - it seems it is possible to buy such wire in the Hook-Up wire section. One just has to be careful to filter by gauge and strand counts to find something decently flexible…
  • dougw
    dougw over 7 years ago in reply to jw0752

    Maybe if you melt the boot to the wire insulation, it won't twist as much....

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago

    If anyone is looking for some of this wire just ask your dentist to save his old failed power optic handpiece and cavitron hoses for you.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to dougw

    Hi Douglas,

     

    Yes the slippery plastic remains a problem in search of a solution. I too have been frustrated with the way they want to slip off or to the side when I am trying to position them.  I will think about it but if someone already has a fix, make my day.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago

    Great idea John.

    One thing I find frustrating is how slippery some of those sleeves are on the alligator clips. It is hard to get your fingers squeezing in the right direction on some of them. I have some ideas, but never got around to solving it, so if you have a solution be sure to let us know....

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
<