Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Shop Tips - Plate Glass
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 11 May 2015 1:27 AM Date Created
  • Views 1253 views
  • Likes 7 likes
  • Comments 10 comments
  • shop
  • solder
  • vise
  • glue
  • tools
  • glass_plate
Related
Recommended

Shop Tips - Plate Glass

jw0752
jw0752
11 May 2015

One of the useful multi-task items in my shop it a 31cm x 25cm piece of plate glass. This particular piece of glass was obtained used from a glass shop. The edges have been beveled and the corners rounded. I have glued 4 rubber feet at the corners to support it and keep if from slipping on my bench.

 

       imageimage

 

One of the uses that the glass gets regularly is to be a solid support for the vacuum vise. When working on or disassembling a circuit board the glass allows the vise to clamp solidly. As components are soldered or desoldered the glass provides a place where solder can fall without damage.

 

      imageimage

 

One of my habits while soldering is to shake the excess solder from the tip as needed to prevent an accumulation of rosin depleted alloy. The glass provides an excellent target. The large heat sink provided by the glass solidifies the cast off solder almost instantly. When completed that glass is cleaned of solder splatter and excess rosin using a razor scraper and a little flux solvent.

 

    imageimageimage

 

The uses for the glass continued with gluing and particularly with the application of Hot Glue. There is always over run and drips from the hot gun. The glass provides a safe place to place the gun and just like the cast off solder the glue drips are quickly cooled on the glass's surface. Clean up is easy with the razor scraper. Even spilled epoxy and super glue can be cleaned from the glass surface. When not in use the glass can be stored on a shelf under your vise or glue gun or even put on a book shelf between a couple of books for protection.

 

 

John

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago +1
    Excellent recycling use. Mark
  • Problemchild
    Problemchild over 11 years ago +1
    Same here, nice and simple... By recovering all that solder you could make little lead soldiers
  • DAB
    DAB over 11 years ago +1
    Great idea John, I like simple solutions to problems. DAB
Parents
  • dtozer
    dtozer over 11 years ago

    Looks like you know Windows pretty well, plate glass.

    How used in your case?

    Regards

    David Tozer CET

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to dtozer

    Hi David Tozer CET,

    Thanks for checking out the blog. I did not understand your question :   "How used in your case?"  but I will try.

    Interpretation #1: The glass was old and came from a broken store front window, I think. Hence it was "used".

    Interpretation #2: I "use" the plate glass primarily as a base for my vacuum vise, occasionally for gluing, and frequently for a solder shake off target.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 11 years ago in reply to dtozer

    Hi David Tozer CET,

    Thanks for checking out the blog. I did not understand your question :   "How used in your case?"  but I will try.

    Interpretation #1: The glass was old and came from a broken store front window, I think. Hence it was "used".

    Interpretation #2: I "use" the plate glass primarily as a base for my vacuum vise, occasionally for gluing, and frequently for a solder shake off target.

    John