Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Shop Tips  -  Power to the Bread Board
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 20 May 2015 3:17 PM Date Created
  • Views 2369 views
  • Likes 12 likes
  • Comments 13 comments
  • pomona_test_wire
  • stem
  • power_cords
  • stem_academy
  • bread_board
Related
Recommended

Shop Tips  -  Power to the Bread Board

jw0752
jw0752
20 May 2015

Previous Shop Tips:

http://www.element14.com/community/people/jw0752/blog/2015/05/11/shop-tips--plate-glass

 

http://www.element14.com/community/people/jw0752/blog/2015/05/16/shop-tips--mind-the-wires

 

 

 

 

Power to the Bread Board:

Until retirement, a couple years ago, I did very little bread boarding of circuits. While my job kept me immersed in the very specific niche of electronics that pertains to Dental Equipment servicing almost no free time was available to experiment or explore further. One of the small problems that was encountered, as I began to bread board, was how to best deliver power to the board. At first I hooked up the banana jacks that came with the bread board kit but, quickly, these were found to be clumsy and not very flexible. I tried alligator clipping to components or to bare wires sticking up from the board. In both of these scenarios the wire or component was often pulled from the board.

 

image

 

image

 

image

 

It was decided that the best solution would be to make up some power supply wires specific for the needs of my shop. The power supplies in my shop all use the standard banana jack / plug for their output connection. So I ordered some good quality test lead wire and some banana plugs.

 

Here is a link to the wire that I chose. It is available in Red and Black, has a 10kV silicone rubber insulation and the wire core is 18 AWG consisting of 192 (41 GA) copper conductors. The feel of the wire is soft and very flexible like a long piece of spaghetti.

 

http://www.newark.com/pomona/6733-2/test-lead-wire-50ft-18awg-copper/dp/63H2515

image

 

 

While it was a little pricey it is better to have a little initial $ pain and not regret every time the wire gets used. The extra wire will come in handy and some of my buddies will want a cord or two also when they see how nice this wire is.

 

Here is the procedure that was followed to make up the bread board power cord that I wanted.

 

image

 

Wires are cut and tagged so resistance can be noted

 

image

 

Banana Plugs are attached to one end of the cords.

 

image

 

On the bread board end of the wire a "Y" is soldered into place.

 

image

 

The "Y" Assemblies.

 

image

 

Wire ends of the "Ys" are completed by adding proper sized pins for the bread board and insulating with shrink tubing.

 

image

 

Completed cords with ID and Resistance labels.

 

Here are some of the examples of why I find this arrangement very useful for my bread board experiments:image

 

If I feel that my circuit will require higher current I double up the wires on each rail.

 

image

 

If higher currents aren't an issue it is really nice to be able to pull V+ and V- both from the upper and lower power rails.

 

 

Occasionally while conducting an experiment it is necessary to have a separate voltage source. While it is perfectly acceptable to build up a small regulator or converter or even just a resistive divider, I have found that a small battery pack with bread board wires is often easier and quicker. Here are my battery packs for bread board experiments.

 

image

 

These are simple tools and modifications but they continue to repay the effort of making them by simplifying hookup and minimizing the problem of having to jury rig hookups and patches to bread board experiments.

 

John

  • Sign in to reply

Top Comments

  • fvan
    fvan over 11 years ago +5
    Nicely done, John! I'm doing something similar using a female barrel jack adapter with screw terminals, in which I can fasten a couple of jumper wires
  • DAB
    DAB over 11 years ago +2
    Good blog John. I have to say, you keep your wires in very good shape with labels and nice heat shrink tubing. My lab is considerably more messy. Keep up the good work, DAB
  • mcb1
    mcb1 over 11 years ago +2
    Great idea. I have one of these (well similar with the jacks) but because of the size, it's not often used. I might have to make some of your leads ...much more friendly on smaller boards. Mark
  • jw0752
    jw0752 over 11 years ago in reply to mcb1

    In my opinion the best part of a blog is when someone comes back and challenges or shares additional ideas. E-14 is a valuable learning environment. I have picked up a lot of great ideas and learning resources from my interactions here. Everyday brings something new to the table.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to jw0752

    No you have to run wires, like yours.

     

    The board is too large for most of my projects so it sits unused.

    It was purchased in the days when it was quite expensive and is not worth throwing away.

     

    fvan  power lead has given me an idea to make up some leads that go to screw terminals ...interfacing to that large wire just doesn't work on breadboards.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to mcb1

    Hi Mark,

    Does the bread board you pictured tie into the rails or do you have to run your own wires from the posts to the rails? The ones I had like this all required power to come into the binding post from a banana plug and then it was necessary to run a separate wire to where ever. I'm not sure why I didn't like it but I took the binding posts off and used them on other projects. Thanks for checking out my blog.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to DAB

    Thanks Donald,

    Glad you liked it.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to fvan

    Hi Frederick,

    This is a very nice adapter idea. That would have application in the signal area as well. Thanks for checking out my blog and posting the picture.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>